AM261x MCU+ SDK  26.00.00

Detailed Description

This is DKEK type which holds the label and context for derivation. This also holds the 256 derived KEK value which is returned by TIFS.

Parameters
label_lengthlength of label.
context_lengthlength of context
label_and_contextholds the label and context as an array
dkekholds the derived key as returned by TIFS.

Data Fields

uint8_t label_length
 
uint8_t context_length
 
uint8_t label_and_context [LABEL_AND_CONTEXT_LEN_MAX]
 
uint32_t dkek [8]
 

Field Documentation

◆ label_length

uint8_t DKEK_t::label_length

label length.

◆ context_length

uint8_t DKEK_t::context_length

context length.

◆ label_and_context

uint8_t DKEK_t::label_and_context[LABEL_AND_CONTEXT_LEN_MAX]

label_and_context array

◆ dkek

uint32_t DKEK_t::dkek[8]

derived KEK.