This is bank swap request structure passed to HSM core via SIPC as argument, these parameters are required by the service handler. Valid only for F29x family of devices.
- Parameters
-
| c29CpuId | C29 CPU for which flash banks are to be swapped |
| syncFlag | Synchronisation flag, HSM waits for this flag to be set to a specific value within a given time period, post which HSM swaps the flash banks |
| timeout | Timeout period for which HSM is supposed to wait |
| c29CpuBankSwapVal | C29 CPU bankswap register value read before making swap request to HSM, used by C29 CPU only |