AM261x MCU+ SDK  26.00.00
pinmux/am261x/pinmux.h File Reference

Introduction

PINMUX Driver API/interface file.

This file contains pad configure register offsets and bit-field value macros for different configurations,

BIT[20] INVERT Invert input (0 = Non Inverted / 1 = Inverted) BIT[19:18] QUAL SEL Select the input qualifier type (00 : SYNC, 01 : 3 SAMPLE, 10 : 6 SAMPLE, 11 : ASYNC) BIT[17:16] GPIO SEL Select the CPU ownership for GPIO pin (00 : GPIO0, 01 : GPIO1, 10 : GPIO2, 11 : GPIO3) BIT[10] SLEWRATE Set slew rate (0 = High / 1 = Low) BIT[9] PULLTYPESEL Set the iternal resistor pull direction high or low (if enabled) BIT[8] PULLUDEN Internal resistor disable (0 = enabled / 1 = disabled) BIT[7:4] OVERRIDE Override the default input and output driver from IP BIT[3:0] MUXMODE select the desired function on the given pin

Go to the source code of this file.

Data Structures

struct  Pinmux_PerCfg_t
 Structure defining the pin configuration parameters. More...
 

Macros

#define PINMUX_END   (-1)
 Macro to mark end of pinmux config array. More...
 
#define PIN_MODE(mode)   ((uint32_t) mode)
 Pin mode - it is at 0th bit. No shift requried. More...
 
#define PIN_FORCE_INPUT_ENABLE   (((uint32_t) 0x1U) << 4U)
 Override IP default to enable input. More...
 
#define PIN_FORCE_INPUT_DISABLE   (((uint32_t) 0x3U) << 4U)
 Override IP default to disable input. More...
 
#define PIN_FORCE_OUTPUT_ENABLE   (((uint32_t) 0x1U) << 6U)
 Override IP default to enable output. More...
 
#define PIN_FORCE_OUTPUT_DISABLE   (((uint32_t) 0x3U) << 6U)
 Override IP default to disable output. More...
 
#define PIN_PULL_DISABLE   (((uint32_t) 0x1U) << 8U)
 Resistor enable. More...
 
#define PIN_PULL_UP   (((uint32_t) 0x1U) << 9U)
 Pull Up. More...
 
#define PIN_PULL_DOWN   (((uint32_t) 0x0U) << 9U)
 Pull Down. More...
 
#define PIN_SLEW_RATE_HIGH   (((uint32_t) 0x0U) << 10U)
 Slew Rate High. More...
 
#define PIN_SLEW_RATE_LOW   (((uint32_t) 0x1U) << 10U)
 Slew Rate Low. More...
 
#define PIN_GPIO_R5SS0_0   (((uint32_t) 0x0U) << 16U)
 GPIO Pin CPU ownership - R5SS0_0. More...
 
#define PIN_GPIO_R5SS0_1   (((uint32_t) 0x1U) << 16U)
 GPIO Pin CPU ownership - R5SS0_1. More...
 
#define PIN_GPIO_R5SS1_0   (((uint32_t) 0x2U) << 16U)
 GPIO Pin CPU ownership - R5SS1_0. More...
 
#define PIN_GPIO_R5SS1_1   (((uint32_t) 0x3U) << 16U)
 GPIO Pin CPU ownership - R5SS1_1. More...
 
#define PIN_QUAL_GRP_MAX_INDEX   (17U)
 Maximum possible index for GPIO Qual group. More...
 
#define PIN_QUAL_GROUP_CFG_START   (CSL_IOMUX_QUAL_GRP_0_CFG_REG)
 Qual Group config register offset in control module. More...
 
#define PIN_QUAL_SYNC   (((uint32_t) 0x0U) << 18U)
 Pin Qualifier - SYNC. More...
 
#define PIN_QUAL_3SAMPLE   (((uint32_t) 0x1U) << 18U)
 Pin Qualifier - 3 SAMPLE. More...
 
#define PIN_QUAL_6SAMPLE   (((uint32_t) 0x2U) << 18U)
 Pin Qualifier - 6 SAMPLE. More...
 
#define PIN_QUAL_ASYNC   (((uint32_t) 0x3U) << 18U)
 Pin Qualifier - ASYNC. More...
 
#define PIN_INVERT   (((uint32_t) 0x1U) << 20U)
 Pin Invert. More...
 
#define PIN_NON_INVERT   (((uint32_t) 0x0U) << 20U)
 Pin Non Invert. More...
 
Pinmux Domain ID

#define PINMUX_DOMAIN_ID_MAIN   (0U)
 
Pad config register offset in control module

#define PIN_GPIO0   (0x00000000U)
 
#define PIN_GPIO1   (0x00000004U)
 
#define PIN_GPIO2   (0x00000008U)
 
#define PIN_GPIO3   (0x0000000CU)
 
#define PIN_GPIO4   (0x00000010U)
 
#define PIN_GPIO5   (0x00000014U)
 
#define PIN_GPIO6   (0x00000018U)
 
#define PIN_GPIO7   (0x0000001CU)
 
#define PIN_GPIO8   (0x00000020U)
 
#define PIN_GPIO9   (0x00000024U)
 
#define PIN_GPIO10   (0x00000028U)
 
#define PIN_GPIO11   (0x0000002CU)
 
#define PIN_GPIO12   (0x00000030U)
 
#define PIN_GPIO13   (0x00000034U)
 
#define PIN_GPIO14   (0x00000038U)
 
#define PIN_GPIO15   (0x0000003CU)
 
#define PIN_GPIO16   (0x00000040U)
 
#define PIN_GPIO17   (0x00000044U)
 
#define PIN_GPIO18   (0x00000048U)
 
#define PIN_GPIO19   (0x0000004CU)
 
#define PIN_GPIO20   (0x00000050U)
 
#define PIN_GPIO21   (0x00000054U)
 
#define PIN_GPIO22   (0x00000058U)
 
#define PIN_GPIO23   (0x0000005CU)
 
#define PIN_GPIO24   (0x00000060U)
 
#define PIN_GPIO25   (0x00000064U)
 
#define PIN_GPIO26   (0x00000068U)
 
#define PIN_GPIO27   (0x0000006CU)
 
#define PIN_GPIO28   (0x00000070U)
 
#define PIN_GPIO29   (0x00000074U)
 
#define PIN_GPIO30   (0x00000078U)
 
#define PIN_GPIO31   (0x0000007CU)
 
#define PIN_GPIO32   (0x00000080U)
 
#define PIN_GPIO33   (0x00000084U)
 
#define PIN_GPIO34   (0x00000088U)
 
#define PIN_GPIO35   (0x0000008CU)
 
#define PIN_GPIO36   (0x00000090U)
 
#define PIN_GPIO37   (0x00000094U)
 
#define PIN_GPIO38   (0x00000098U)
 
#define PIN_GPIO39   (0x0000009CU)
 
#define PIN_GPIO40   (0x000000A0U)
 
#define PIN_GPIO41   (0x000000A4U)
 
#define PIN_GPIO42   (0x000000A8U)
 
#define PIN_GPIO43   (0x000000ACU)
 
#define PIN_GPIO44   (0x000000B0U)
 
#define PIN_GPIO45   (0x000000B4U)
 
#define PIN_GPIO46   (0x000000B8U)
 
#define PIN_GPIO47   (0x000000BCU)
 
#define PIN_GPIO48   (0x000000C0U)
 
#define PIN_GPIO49   (0x000000C4U)
 
#define PIN_GPIO50   (0x000000C8U)
 
#define PIN_GPIO51   (0x000000CCU)
 
#define PIN_GPIO52   (0x000000D0U)
 
#define PIN_GPIO53   (0x000000D4U)
 
#define PIN_GPIO54   (0x000000D8U)
 
#define PIN_GPIO55   (0x000000DCU)
 
#define PIN_GPIO56   (0x000000E0U)
 
#define PIN_GPIO57   (0x000000E4U)
 
#define PIN_GPIO58   (0x000000E8U)
 
#define PIN_GPIO59   (0x000000ECU)
 
#define PIN_GPIO60   (0x000000F0U)
 
#define PIN_GPIO61   (0x000000F4U)
 
#define PIN_GPIO62   (0x000000F8U)
 
#define PIN_GPIO63   (0x000000FCU)
 
#define PIN_GPIO64   (0x00000100U)
 
#define PIN_GPIO65   (0x00000104U)
 
#define PIN_GPIO66   (0x00000108U)
 
#define PIN_GPIO67   (0x0000010CU)
 
#define PIN_GPIO68   (0x00000110U)
 
#define PIN_GPIO69   (0x00000114U)
 
#define PIN_GPIO70   (0x00000118U)
 
#define PIN_GPIO71   (0x0000011CU)
 
#define PIN_GPIO72   (0x00000120U)
 
#define PIN_GPIO73   (0x00000124U)
 
#define PIN_GPIO74   (0x00000128U)
 
#define PIN_GPIO75   (0x0000012CU)
 
#define PIN_GPIO76   (0x00000130U)
 
#define PIN_GPIO77   (0x00000134U)
 
#define PIN_GPIO78   (0x00000138U)
 
#define PIN_GPIO79   (0x0000013CU)
 
#define PIN_GPIO80   (0x00000140U)
 
#define PIN_GPIO81   (0x00000144U)
 
#define PIN_GPIO82   (0x00000148U)
 
#define PIN_GPIO83   (0x0000014CU)
 
#define PIN_GPIO84   (0x00000150U)
 
#define PIN_GPIO85   (0x00000154U)
 
#define PIN_GPIO86   (0x00000158U)
 
#define PIN_GPIO87   (0x0000015CU)
 
#define PIN_GPIO88   (0x00000160U)
 
#define PIN_GPIO89   (0x00000164U)
 
#define PIN_GPIO90   (0x00000168U)
 
#define PIN_GPIO91   (0x0000016CU)
 
#define PIN_GPIO92   (0x00000170U)
 
#define PIN_GPIO93   (0x00000174U)
 
#define PIN_GPIO94   (0x00000178U)
 
#define PIN_GPIO95   (0x0000017CU)
 
#define PIN_GPIO96   (0x00000180U)
 
#define PIN_GPIO97   (0x00000184U)
 
#define PIN_GPIO98   (0x00000188U)
 
#define PIN_GPIO99   (0x0000018CU)
 
#define PIN_GPIO100   (0x00000190U)
 
#define PIN_GPIO101   (0x00000194U)
 
#define PIN_GPIO102   (0x00000198U)
 
#define PIN_GPIO103   (0x0000019CU)
 
#define PIN_GPIO104   (0x000001A0U)
 
#define PIN_GPIO105   (0x000001A4U)
 
#define PIN_GPIO106   (0x000001A8U)
 
#define PIN_GPIO107   (0x000001ACU)
 
#define PIN_GPIO108   (0x000001B0U)
 
#define PIN_GPIO109   (0x000001B4U)
 
#define PIN_GPIO110   (0x000001B8U)
 
#define PIN_GPIO111   (0x000001BCU)
 
#define PIN_GPIO112   (0x000001C0U)
 
#define PIN_GPIO113   (0x000001C4U)
 
#define PIN_GPIO114   (0x000001C8U)
 
#define PIN_GPIO115   (0x000001CCU)
 
#define PIN_GPIO116   (0x000001D0U)
 
#define PIN_GPIO117   (0x000001D4U)
 
#define PIN_GPIO118   (0x000001D8U)
 
#define PIN_GPIO119   (0x000001DCU)
 
#define PIN_GPIO120   (0x000001E0U)
 
#define PIN_GPIO121   (0x000001E4U)
 
#define PIN_GPIO122   (0x000001E8U)
 
#define PIN_GPIO123   (0x000001ECU)
 
#define PIN_GPIO124   (0x000001F0U)
 
#define PIN_GPIO125   (0x000001F4U)
 
#define PIN_GPIO126   (0x000001F8U)
 
#define PIN_GPIO127   (0x000001FCU)
 
#define PIN_GPIO128   (0x00000200U)
 
#define PIN_GPIO129   (0x00000204U)
 
#define PIN_GPIO130   (0x00000208U)
 
#define PIN_GPIO131   (0x0000020CU)
 
#define PIN_GPIO132   (0x00000210U)
 
#define PIN_GPIO133   (0x00000214U)
 
#define PIN_GPIO134   (0x00000218U)
 
#define PIN_GPIO135   (0x0000021CU)
 
#define PIN_GPIO136   (0x00000220U)
 
#define PIN_GPIO137   (0x00000224U)
 
#define PIN_GPIO138   (0x00000228U)
 
#define PIN_GPIO139   (0x0000022CU)
 
#define PIN_GPIO140   (0x00000230U)
 
#define PIN_WARMRSTn   (0x00000234U)
 
#define PIN_SAFETY_ERRORn   (0x00000238U)
 
#define PIN_TDI   (0x0000023CU)
 
#define PIN_TDO   (0x00000240U)
 
#define PIN_TMS   (0x00000244U)
 
#define PIN_TCK   (0x00000248U)
 
#define PIN_OSPI0_CLKLB   (0x0000024CU)
 
#define PIN_OSPI1_CLKLB   (0x00000250U)
 
#define PIN_PORz   (0x00000254U)
 
#define PIN_XTAL_XI   (0x00000258U)
 
#define PIN_XTAL_XO   (0x0000025CU)
 
#define PIN_ADC0_AIN0   (0x00000260U)
 
#define PIN_ADC0_AIN1   (0x00000264U)
 
#define PIN_ADC0_AIN2   (0x00000268U)
 
#define PIN_ADC0_AIN3   (0x0000026CU)
 
#define PIN_ADC0_AIN4   (0x00000270U)
 
#define PIN_ADC0_AIN5   (0x00000274U)
 
#define PIN_ADC0_AIN6   (0x00000278U)
 
#define PIN_ADC1_AIN0   (0x0000027CU)
 
#define PIN_ADC1_AIN1   (0x00000280U)
 
#define PIN_ADC1_AIN2   (0x00000284U)
 
#define PIN_ADC1_AIN3   (0x00000288U)
 
#define PIN_ADC1_AIN4   (0x0000028CU)
 
#define PIN_ADC1_AIN5   (0x00000290U)
 
#define PIN_ADC1_AIN6   (0x00000294U)
 
#define PIN_ADC2_AIN0   (0x00000298U)
 
#define PIN_ADC2_AIN1   (0x0000029CU)
 
#define PIN_ADC2_AIN2   (0x000002A0U)
 
#define PIN_ADC2_AIN3   (0x000002A4U)
 
#define PIN_ADC2_AIN4   (0x000002A8U)
 
#define PIN_ADC2_AIN5   (0x000002ACU)
 
#define PIN_ADC2_AIN6   (0x000002B0U)
 
#define PIN_ADC3_AIN0   (0x000002B4U)
 
#define PIN_ADC3_AIN1   (0x000002B8U)
 
#define PIN_ADC3_AIN2   (0x000002BCU)
 
#define PIN_ADC3_AIN3   (0x000002C0U)
 
#define PIN_ADC3_AIN4   (0x000002C4U)
 
#define PIN_ADC3_AIN5   (0x000002C8U)
 
#define PIN_ADC4_AIN0   (0x000002CCU)
 
#define PIN_ADC4_AIN1   (0x000002D0U)
 
#define PIN_ADC4_AIN2   (0x000002D4U)
 
#define PIN_ADC4_AIN3   (0x000002D8U)
 
#define PIN_ADC4_AIN4   (0x000002DCU)
 
#define PIN_ADC4_AIN5   (0x000002E0U)
 
#define PIN_ADC_VREFHISRC0   (0x000002E4U)
 
#define PIN_ADC_VREFLOSRC0   (0x000002E8U)
 
#define PIN_ADC_VREFHI0   (0x000002ECU)
 
#define PIN_ADC_VREFLO0   (0x000002F0U)
 
#define PIN_ADC_VREFHI1   (0x000002F4U)
 
#define PIN_ADC_VREFLO1   (0x000002F8U)
 
#define PIN_ADC_VREFHI2   (0x000002FCU)
 
#define PIN_ADC_VREFLO2   (0x00000300U)
 
#define PIN_ADC_VREFHISRC1   (0x00000304U)
 
#define PIN_ADC_VREFLOSRC1   (0x00000308U)
 
#define PIN_ADC_VREFHI3   (0x0000030CU)
 
#define PIN_ADC_VREFLO3   (0x00000310U)
 
#define PIN_ADC_VREFHI4   (0x00000314U)
 
#define PIN_ADC_VREFLO4   (0x00000318U)
 
#define PIN_ADC_CAL0   (0x0000031CU)
 
#define PIN_ADC_CAL1   (0x00000320U)
 
#define PIN_DAC_VREF0   (0x00000324U)
 
#define PIN_DAC_VREF1   (0x00000328U)
 
#define PIN_DAC_OUT   (0x0000032CU)
 
#define PIN_TEMPCAL   (0x00000330U)
 
#define PIN_VSYS_MON   (0x00000334U)
 
#define PIN_ATESTV0   (0x00000338U)
 
#define PIN_ATESTV1   (0x0000033CU)
 
#define PIN_PMUBYPASS   (0x00000340U)
 
#define PIN_USB0_CE   (0x00000344U)
 
#define PIN_SDADC0_DP   (0x00000348U)
 
#define PIN_SDADC0_DM   (0x0000034CU)
 
#define PIN_ADC_CAL2   (0x00000350U)
 
#define PIN_ADC_R0_AIN0   (0x00000354U)
 
#define PIN_ADC_R0_AIN1   (0x00000358U)
 
#define PIN_ADC_R0_AIN2   (0x0000035CU)
 
#define PIN_ADC_R0_AIN3   (0x00000360U)
 
#define PIN_ADC_VREFLO5   (0x00000364U)
 
#define PIN_ADC_VREFHI5   (0x00000368U)
 
#define PIN_ADC_VREFLO6   (0x0000036CU)
 
#define PIN_ADC_VREFHI6   (0x00000370U)
 
#define PIN_ADC_R1_AIN0   (0x00000374U)
 
#define PIN_ADC_R1_AIN1   (0x00000378U)
 
#define PIN_ADC_R1_AIN2   (0x0000037CU)
 
#define PIN_ADC_R1_AIN3   (0x00000380U)
 
#define PIN_ADC_CAL3   (0x00000384U)
 

Functions

void Pinmux_config (const Pinmux_PerCfg_t *pinmuxCfg, uint32_t domainId)
 This API configures the pinmux based on the domain. More...
 
void Pinmux_qualPeriodConfig (uint32_t qualGroupIndex, uint8_t qualPeriod)
 This API configures the Qualification period for a specific GPIO Pin group. More...
 
void Pinmux_enableUserMode (void)
 This API enables user mode access to the IOMUX register space. More...
 
void Pinmux_disableUserMode (void)
 This API disables user mode access to the IOMUX register space. More...