AM261x MCU+ SDK  26.00.00

Introduction

This module contains APIs to program and use the pinmux module.

Files

file  pinmux/am261x/pinmux.h
 PINMUX Driver API/interface file.
 

Data Structures

struct  Pinmux_PerCfg_t
 Structure defining the pin configuration parameters. More...
 

Functions

void Pinmux_config (const Pinmux_PerCfg_t *pinmuxCfg, uint32_t domainId)
 This API configures the pinmux based on the domain. More...
 
void Pinmux_qualPeriodConfig (uint32_t qualGroupIndex, uint8_t qualPeriod)
 This API configures the Qualification period for a specific GPIO Pin group. More...
 
void Pinmux_enableUserMode (void)
 This API enables user mode access to the IOMUX register space. More...
 
void Pinmux_disableUserMode (void)
 This API disables user mode access to the IOMUX register space. More...
 

Macros

#define PINMUX_END   (-1)
 Macro to mark end of pinmux config array. More...
 
#define PIN_MODE(mode)   ((uint32_t) mode)
 Pin mode - it is at 0th bit. No shift requried. More...
 
#define PIN_FORCE_INPUT_ENABLE   (((uint32_t) 0x1U) << 4U)
 Override IP default to enable input. More...
 
#define PIN_FORCE_INPUT_DISABLE   (((uint32_t) 0x3U) << 4U)
 Override IP default to disable input. More...
 
#define PIN_FORCE_OUTPUT_ENABLE   (((uint32_t) 0x1U) << 6U)
 Override IP default to enable output. More...
 
#define PIN_FORCE_OUTPUT_DISABLE   (((uint32_t) 0x3U) << 6U)
 Override IP default to disable output. More...
 
#define PIN_PULL_DISABLE   (((uint32_t) 0x1U) << 8U)
 Resistor enable. More...
 
#define PIN_PULL_UP   (((uint32_t) 0x1U) << 9U)
 Pull Up. More...
 
#define PIN_PULL_DOWN   (((uint32_t) 0x0U) << 9U)
 Pull Down. More...
 
#define PIN_SLEW_RATE_HIGH   (((uint32_t) 0x0U) << 10U)
 Slew Rate High. More...
 
#define PIN_SLEW_RATE_LOW   (((uint32_t) 0x1U) << 10U)
 Slew Rate Low. More...
 
#define PIN_GPIO_R5SS0_0   (((uint32_t) 0x0U) << 16U)
 GPIO Pin CPU ownership - R5SS0_0. More...
 
#define PIN_GPIO_R5SS0_1   (((uint32_t) 0x1U) << 16U)
 GPIO Pin CPU ownership - R5SS0_1. More...
 
#define PIN_GPIO_R5SS1_0   (((uint32_t) 0x2U) << 16U)
 GPIO Pin CPU ownership - R5SS1_0. More...
 
#define PIN_GPIO_R5SS1_1   (((uint32_t) 0x3U) << 16U)
 GPIO Pin CPU ownership - R5SS1_1. More...
 
#define PIN_QUAL_GRP_MAX_INDEX   (17U)
 Maximum possible index for GPIO Qual group. More...
 
#define PIN_QUAL_GROUP_CFG_START   (CSL_IOMUX_QUAL_GRP_0_CFG_REG)
 Qual Group config register offset in control module. More...
 
#define PIN_QUAL_SYNC   (((uint32_t) 0x0U) << 18U)
 Pin Qualifier - SYNC. More...
 
#define PIN_QUAL_3SAMPLE   (((uint32_t) 0x1U) << 18U)
 Pin Qualifier - 3 SAMPLE. More...
 
#define PIN_QUAL_6SAMPLE   (((uint32_t) 0x2U) << 18U)
 Pin Qualifier - 6 SAMPLE. More...
 
#define PIN_QUAL_ASYNC   (((uint32_t) 0x3U) << 18U)
 Pin Qualifier - ASYNC. More...
 
#define PIN_INVERT   (((uint32_t) 0x1U) << 20U)
 Pin Invert. More...
 
#define PIN_NON_INVERT   (((uint32_t) 0x0U) << 20U)
 Pin Non Invert. More...
 

Pinmux Domain ID

#define PINMUX_DOMAIN_ID_MAIN   (0U)
 

Pad config register offset in control module

#define PIN_GPIO0   (0x00000000U)
 
#define PIN_GPIO1   (0x00000004U)
 
#define PIN_GPIO2   (0x00000008U)
 
#define PIN_GPIO3   (0x0000000CU)
 
#define PIN_GPIO4   (0x00000010U)
 
#define PIN_GPIO5   (0x00000014U)
 
#define PIN_GPIO6   (0x00000018U)
 
#define PIN_GPIO7   (0x0000001CU)
 
#define PIN_GPIO8   (0x00000020U)
 
#define PIN_GPIO9   (0x00000024U)
 
#define PIN_GPIO10   (0x00000028U)
 
#define PIN_GPIO11   (0x0000002CU)
 
#define PIN_GPIO12   (0x00000030U)
 
#define PIN_GPIO13   (0x00000034U)
 
#define PIN_GPIO14   (0x00000038U)
 
#define PIN_GPIO15   (0x0000003CU)
 
#define PIN_GPIO16   (0x00000040U)
 
#define PIN_GPIO17   (0x00000044U)
 
#define PIN_GPIO18   (0x00000048U)
 
#define PIN_GPIO19   (0x0000004CU)
 
#define PIN_GPIO20   (0x00000050U)
 
#define PIN_GPIO21   (0x00000054U)
 
#define PIN_GPIO22   (0x00000058U)
 
#define PIN_GPIO23   (0x0000005CU)
 
#define PIN_GPIO24   (0x00000060U)
 
#define PIN_GPIO25   (0x00000064U)
 
#define PIN_GPIO26   (0x00000068U)
 
#define PIN_GPIO27   (0x0000006CU)
 
#define PIN_GPIO28   (0x00000070U)
 
#define PIN_GPIO29   (0x00000074U)
 
#define PIN_GPIO30   (0x00000078U)
 
#define PIN_GPIO31   (0x0000007CU)
 
#define PIN_GPIO32   (0x00000080U)
 
#define PIN_GPIO33   (0x00000084U)
 
#define PIN_GPIO34   (0x00000088U)
 
#define PIN_GPIO35   (0x0000008CU)
 
#define PIN_GPIO36   (0x00000090U)
 
#define PIN_GPIO37   (0x00000094U)
 
#define PIN_GPIO38   (0x00000098U)
 
#define PIN_GPIO39   (0x0000009CU)
 
#define PIN_GPIO40   (0x000000A0U)
 
#define PIN_GPIO41   (0x000000A4U)
 
#define PIN_GPIO42   (0x000000A8U)
 
#define PIN_GPIO43   (0x000000ACU)
 
#define PIN_GPIO44   (0x000000B0U)
 
#define PIN_GPIO45   (0x000000B4U)
 
#define PIN_GPIO46   (0x000000B8U)
 
#define PIN_GPIO47   (0x000000BCU)
 
#define PIN_GPIO48   (0x000000C0U)
 
#define PIN_GPIO49   (0x000000C4U)
 
#define PIN_GPIO50   (0x000000C8U)
 
#define PIN_GPIO51   (0x000000CCU)
 
#define PIN_GPIO52   (0x000000D0U)
 
#define PIN_GPIO53   (0x000000D4U)
 
#define PIN_GPIO54   (0x000000D8U)
 
#define PIN_GPIO55   (0x000000DCU)
 
#define PIN_GPIO56   (0x000000E0U)
 
#define PIN_GPIO57   (0x000000E4U)
 
#define PIN_GPIO58   (0x000000E8U)
 
#define PIN_GPIO59   (0x000000ECU)
 
#define PIN_GPIO60   (0x000000F0U)
 
#define PIN_GPIO61   (0x000000F4U)
 
#define PIN_GPIO62   (0x000000F8U)
 
#define PIN_GPIO63   (0x000000FCU)
 
#define PIN_GPIO64   (0x00000100U)
 
#define PIN_GPIO65   (0x00000104U)
 
#define PIN_GPIO66   (0x00000108U)
 
#define PIN_GPIO67   (0x0000010CU)
 
#define PIN_GPIO68   (0x00000110U)
 
#define PIN_GPIO69   (0x00000114U)
 
#define PIN_GPIO70   (0x00000118U)
 
#define PIN_GPIO71   (0x0000011CU)
 
#define PIN_GPIO72   (0x00000120U)
 
#define PIN_GPIO73   (0x00000124U)
 
#define PIN_GPIO74   (0x00000128U)
 
#define PIN_GPIO75   (0x0000012CU)
 
#define PIN_GPIO76   (0x00000130U)
 
#define PIN_GPIO77   (0x00000134U)
 
#define PIN_GPIO78   (0x00000138U)
 
#define PIN_GPIO79   (0x0000013CU)
 
#define PIN_GPIO80   (0x00000140U)
 
#define PIN_GPIO81   (0x00000144U)
 
#define PIN_GPIO82   (0x00000148U)
 
#define PIN_GPIO83   (0x0000014CU)
 
#define PIN_GPIO84   (0x00000150U)
 
#define PIN_GPIO85   (0x00000154U)
 
#define PIN_GPIO86   (0x00000158U)
 
#define PIN_GPIO87   (0x0000015CU)
 
#define PIN_GPIO88   (0x00000160U)
 
#define PIN_GPIO89   (0x00000164U)
 
#define PIN_GPIO90   (0x00000168U)
 
#define PIN_GPIO91   (0x0000016CU)
 
#define PIN_GPIO92   (0x00000170U)
 
#define PIN_GPIO93   (0x00000174U)
 
#define PIN_GPIO94   (0x00000178U)
 
#define PIN_GPIO95   (0x0000017CU)
 
#define PIN_GPIO96   (0x00000180U)
 
#define PIN_GPIO97   (0x00000184U)
 
#define PIN_GPIO98   (0x00000188U)
 
#define PIN_GPIO99   (0x0000018CU)
 
#define PIN_GPIO100   (0x00000190U)
 
#define PIN_GPIO101   (0x00000194U)
 
#define PIN_GPIO102   (0x00000198U)
 
#define PIN_GPIO103   (0x0000019CU)
 
#define PIN_GPIO104   (0x000001A0U)
 
#define PIN_GPIO105   (0x000001A4U)
 
#define PIN_GPIO106   (0x000001A8U)
 
#define PIN_GPIO107   (0x000001ACU)
 
#define PIN_GPIO108   (0x000001B0U)
 
#define PIN_GPIO109   (0x000001B4U)
 
#define PIN_GPIO110   (0x000001B8U)
 
#define PIN_GPIO111   (0x000001BCU)
 
#define PIN_GPIO112   (0x000001C0U)
 
#define PIN_GPIO113   (0x000001C4U)
 
#define PIN_GPIO114   (0x000001C8U)
 
#define PIN_GPIO115   (0x000001CCU)
 
#define PIN_GPIO116   (0x000001D0U)
 
#define PIN_GPIO117   (0x000001D4U)
 
#define PIN_GPIO118   (0x000001D8U)
 
#define PIN_GPIO119   (0x000001DCU)
 
#define PIN_GPIO120   (0x000001E0U)
 
#define PIN_GPIO121   (0x000001E4U)
 
#define PIN_GPIO122   (0x000001E8U)
 
#define PIN_GPIO123   (0x000001ECU)
 
#define PIN_GPIO124   (0x000001F0U)
 
#define PIN_GPIO125   (0x000001F4U)
 
#define PIN_GPIO126   (0x000001F8U)
 
#define PIN_GPIO127   (0x000001FCU)
 
#define PIN_GPIO128   (0x00000200U)
 
#define PIN_GPIO129   (0x00000204U)
 
#define PIN_GPIO130   (0x00000208U)
 
#define PIN_GPIO131   (0x0000020CU)
 
#define PIN_GPIO132   (0x00000210U)
 
#define PIN_GPIO133   (0x00000214U)
 
#define PIN_GPIO134   (0x00000218U)
 
#define PIN_GPIO135   (0x0000021CU)
 
#define PIN_GPIO136   (0x00000220U)
 
#define PIN_GPIO137   (0x00000224U)
 
#define PIN_GPIO138   (0x00000228U)
 
#define PIN_GPIO139   (0x0000022CU)
 
#define PIN_GPIO140   (0x00000230U)
 
#define PIN_WARMRSTn   (0x00000234U)
 
#define PIN_SAFETY_ERRORn   (0x00000238U)
 
#define PIN_TDI   (0x0000023CU)
 
#define PIN_TDO   (0x00000240U)
 
#define PIN_TMS   (0x00000244U)
 
#define PIN_TCK   (0x00000248U)
 
#define PIN_OSPI0_CLKLB   (0x0000024CU)
 
#define PIN_OSPI1_CLKLB   (0x00000250U)
 
#define PIN_PORz   (0x00000254U)
 
#define PIN_XTAL_XI   (0x00000258U)
 
#define PIN_XTAL_XO   (0x0000025CU)
 
#define PIN_ADC0_AIN0   (0x00000260U)
 
#define PIN_ADC0_AIN1   (0x00000264U)
 
#define PIN_ADC0_AIN2   (0x00000268U)
 
#define PIN_ADC0_AIN3   (0x0000026CU)
 
#define PIN_ADC0_AIN4   (0x00000270U)
 
#define PIN_ADC0_AIN5   (0x00000274U)
 
#define PIN_ADC0_AIN6   (0x00000278U)
 
#define PIN_ADC1_AIN0   (0x0000027CU)
 
#define PIN_ADC1_AIN1   (0x00000280U)
 
#define PIN_ADC1_AIN2   (0x00000284U)
 
#define PIN_ADC1_AIN3   (0x00000288U)
 
#define PIN_ADC1_AIN4   (0x0000028CU)
 
#define PIN_ADC1_AIN5   (0x00000290U)
 
#define PIN_ADC1_AIN6   (0x00000294U)
 
#define PIN_ADC2_AIN0   (0x00000298U)
 
#define PIN_ADC2_AIN1   (0x0000029CU)
 
#define PIN_ADC2_AIN2   (0x000002A0U)
 
#define PIN_ADC2_AIN3   (0x000002A4U)
 
#define PIN_ADC2_AIN4   (0x000002A8U)
 
#define PIN_ADC2_AIN5   (0x000002ACU)
 
#define PIN_ADC2_AIN6   (0x000002B0U)
 
#define PIN_ADC3_AIN0   (0x000002B4U)
 
#define PIN_ADC3_AIN1   (0x000002B8U)
 
#define PIN_ADC3_AIN2   (0x000002BCU)
 
#define PIN_ADC3_AIN3   (0x000002C0U)
 
#define PIN_ADC3_AIN4   (0x000002C4U)
 
#define PIN_ADC3_AIN5   (0x000002C8U)
 
#define PIN_ADC4_AIN0   (0x000002CCU)
 
#define PIN_ADC4_AIN1   (0x000002D0U)
 
#define PIN_ADC4_AIN2   (0x000002D4U)
 
#define PIN_ADC4_AIN3   (0x000002D8U)
 
#define PIN_ADC4_AIN4   (0x000002DCU)
 
#define PIN_ADC4_AIN5   (0x000002E0U)
 
#define PIN_ADC_VREFHISRC0   (0x000002E4U)
 
#define PIN_ADC_VREFLOSRC0   (0x000002E8U)
 
#define PIN_ADC_VREFHI0   (0x000002ECU)
 
#define PIN_ADC_VREFLO0   (0x000002F0U)
 
#define PIN_ADC_VREFHI1   (0x000002F4U)
 
#define PIN_ADC_VREFLO1   (0x000002F8U)
 
#define PIN_ADC_VREFHI2   (0x000002FCU)
 
#define PIN_ADC_VREFLO2   (0x00000300U)
 
#define PIN_ADC_VREFHISRC1   (0x00000304U)
 
#define PIN_ADC_VREFLOSRC1   (0x00000308U)
 
#define PIN_ADC_VREFHI3   (0x0000030CU)
 
#define PIN_ADC_VREFLO3   (0x00000310U)
 
#define PIN_ADC_VREFHI4   (0x00000314U)
 
#define PIN_ADC_VREFLO4   (0x00000318U)
 
#define PIN_ADC_CAL0   (0x0000031CU)
 
#define PIN_ADC_CAL1   (0x00000320U)
 
#define PIN_DAC_VREF0   (0x00000324U)
 
#define PIN_DAC_VREF1   (0x00000328U)
 
#define PIN_DAC_OUT   (0x0000032CU)
 
#define PIN_TEMPCAL   (0x00000330U)
 
#define PIN_VSYS_MON   (0x00000334U)
 
#define PIN_ATESTV0   (0x00000338U)
 
#define PIN_ATESTV1   (0x0000033CU)
 
#define PIN_PMUBYPASS   (0x00000340U)
 
#define PIN_USB0_CE   (0x00000344U)
 
#define PIN_SDADC0_DP   (0x00000348U)
 
#define PIN_SDADC0_DM   (0x0000034CU)
 
#define PIN_ADC_CAL2   (0x00000350U)
 
#define PIN_ADC_R0_AIN0   (0x00000354U)
 
#define PIN_ADC_R0_AIN1   (0x00000358U)
 
#define PIN_ADC_R0_AIN2   (0x0000035CU)
 
#define PIN_ADC_R0_AIN3   (0x00000360U)
 
#define PIN_ADC_VREFLO5   (0x00000364U)
 
#define PIN_ADC_VREFHI5   (0x00000368U)
 
#define PIN_ADC_VREFLO6   (0x0000036CU)
 
#define PIN_ADC_VREFHI6   (0x00000370U)
 
#define PIN_ADC_R1_AIN0   (0x00000374U)
 
#define PIN_ADC_R1_AIN1   (0x00000378U)
 
#define PIN_ADC_R1_AIN2   (0x0000037CU)
 
#define PIN_ADC_R1_AIN3   (0x00000380U)
 
#define PIN_ADC_CAL3   (0x00000384U)
 

Macro Definition Documentation

◆ PINMUX_DOMAIN_ID_MAIN

#define PINMUX_DOMAIN_ID_MAIN   (0U)

◆ PINMUX_END

#define PINMUX_END   (-1)

Macro to mark end of pinmux config array.

◆ PIN_MODE

#define PIN_MODE (   mode)    ((uint32_t) mode)

Pin mode - it is at 0th bit. No shift requried.

◆ PIN_FORCE_INPUT_ENABLE

#define PIN_FORCE_INPUT_ENABLE   (((uint32_t) 0x1U) << 4U)

Override IP default to enable input.

◆ PIN_FORCE_INPUT_DISABLE

#define PIN_FORCE_INPUT_DISABLE   (((uint32_t) 0x3U) << 4U)

Override IP default to disable input.

◆ PIN_FORCE_OUTPUT_ENABLE

#define PIN_FORCE_OUTPUT_ENABLE   (((uint32_t) 0x1U) << 6U)

Override IP default to enable output.

◆ PIN_FORCE_OUTPUT_DISABLE

#define PIN_FORCE_OUTPUT_DISABLE   (((uint32_t) 0x3U) << 6U)

Override IP default to disable output.

◆ PIN_PULL_DISABLE

#define PIN_PULL_DISABLE   (((uint32_t) 0x1U) << 8U)

Resistor enable.

◆ PIN_PULL_UP

#define PIN_PULL_UP   (((uint32_t) 0x1U) << 9U)

Pull Up.

◆ PIN_PULL_DOWN

#define PIN_PULL_DOWN   (((uint32_t) 0x0U) << 9U)

Pull Down.

◆ PIN_SLEW_RATE_HIGH

#define PIN_SLEW_RATE_HIGH   (((uint32_t) 0x0U) << 10U)

Slew Rate High.

◆ PIN_SLEW_RATE_LOW

#define PIN_SLEW_RATE_LOW   (((uint32_t) 0x1U) << 10U)

Slew Rate Low.

◆ PIN_GPIO_R5SS0_0

#define PIN_GPIO_R5SS0_0   (((uint32_t) 0x0U) << 16U)

GPIO Pin CPU ownership - R5SS0_0.

◆ PIN_GPIO_R5SS0_1

#define PIN_GPIO_R5SS0_1   (((uint32_t) 0x1U) << 16U)

GPIO Pin CPU ownership - R5SS0_1.

◆ PIN_GPIO_R5SS1_0

#define PIN_GPIO_R5SS1_0   (((uint32_t) 0x2U) << 16U)

GPIO Pin CPU ownership - R5SS1_0.

◆ PIN_GPIO_R5SS1_1

#define PIN_GPIO_R5SS1_1   (((uint32_t) 0x3U) << 16U)

GPIO Pin CPU ownership - R5SS1_1.

◆ PIN_QUAL_GRP_MAX_INDEX

#define PIN_QUAL_GRP_MAX_INDEX   (17U)

Maximum possible index for GPIO Qual group.

◆ PIN_QUAL_GROUP_CFG_START

#define PIN_QUAL_GROUP_CFG_START   (CSL_IOMUX_QUAL_GRP_0_CFG_REG)

Qual Group config register offset in control module.

◆ PIN_QUAL_SYNC

#define PIN_QUAL_SYNC   (((uint32_t) 0x0U) << 18U)

Pin Qualifier - SYNC.

◆ PIN_QUAL_3SAMPLE

#define PIN_QUAL_3SAMPLE   (((uint32_t) 0x1U) << 18U)

Pin Qualifier - 3 SAMPLE.

◆ PIN_QUAL_6SAMPLE

#define PIN_QUAL_6SAMPLE   (((uint32_t) 0x2U) << 18U)

Pin Qualifier - 6 SAMPLE.

◆ PIN_QUAL_ASYNC

#define PIN_QUAL_ASYNC   (((uint32_t) 0x3U) << 18U)

Pin Qualifier - ASYNC.

◆ PIN_INVERT

#define PIN_INVERT   (((uint32_t) 0x1U) << 20U)

Pin Invert.

◆ PIN_NON_INVERT

#define PIN_NON_INVERT   (((uint32_t) 0x0U) << 20U)

Pin Non Invert.

◆ PIN_GPIO0

#define PIN_GPIO0   (0x00000000U)

◆ PIN_GPIO1

#define PIN_GPIO1   (0x00000004U)

◆ PIN_GPIO2

#define PIN_GPIO2   (0x00000008U)

◆ PIN_GPIO3

#define PIN_GPIO3   (0x0000000CU)

◆ PIN_GPIO4

#define PIN_GPIO4   (0x00000010U)

◆ PIN_GPIO5

#define PIN_GPIO5   (0x00000014U)

◆ PIN_GPIO6

#define PIN_GPIO6   (0x00000018U)

◆ PIN_GPIO7

#define PIN_GPIO7   (0x0000001CU)

◆ PIN_GPIO8

#define PIN_GPIO8   (0x00000020U)

◆ PIN_GPIO9

#define PIN_GPIO9   (0x00000024U)

◆ PIN_GPIO10

#define PIN_GPIO10   (0x00000028U)

◆ PIN_GPIO11

#define PIN_GPIO11   (0x0000002CU)

◆ PIN_GPIO12

#define PIN_GPIO12   (0x00000030U)

◆ PIN_GPIO13

#define PIN_GPIO13   (0x00000034U)

◆ PIN_GPIO14

#define PIN_GPIO14   (0x00000038U)

◆ PIN_GPIO15

#define PIN_GPIO15   (0x0000003CU)

◆ PIN_GPIO16

#define PIN_GPIO16   (0x00000040U)

◆ PIN_GPIO17

#define PIN_GPIO17   (0x00000044U)

◆ PIN_GPIO18

#define PIN_GPIO18   (0x00000048U)

◆ PIN_GPIO19

#define PIN_GPIO19   (0x0000004CU)

◆ PIN_GPIO20

#define PIN_GPIO20   (0x00000050U)

◆ PIN_GPIO21

#define PIN_GPIO21   (0x00000054U)

◆ PIN_GPIO22

#define PIN_GPIO22   (0x00000058U)

◆ PIN_GPIO23

#define PIN_GPIO23   (0x0000005CU)

◆ PIN_GPIO24

#define PIN_GPIO24   (0x00000060U)

◆ PIN_GPIO25

#define PIN_GPIO25   (0x00000064U)

◆ PIN_GPIO26

#define PIN_GPIO26   (0x00000068U)

◆ PIN_GPIO27

#define PIN_GPIO27   (0x0000006CU)

◆ PIN_GPIO28

#define PIN_GPIO28   (0x00000070U)

◆ PIN_GPIO29

#define PIN_GPIO29   (0x00000074U)

◆ PIN_GPIO30

#define PIN_GPIO30   (0x00000078U)

◆ PIN_GPIO31

#define PIN_GPIO31   (0x0000007CU)

◆ PIN_GPIO32

#define PIN_GPIO32   (0x00000080U)

◆ PIN_GPIO33

#define PIN_GPIO33   (0x00000084U)

◆ PIN_GPIO34

#define PIN_GPIO34   (0x00000088U)

◆ PIN_GPIO35

#define PIN_GPIO35   (0x0000008CU)

◆ PIN_GPIO36

#define PIN_GPIO36   (0x00000090U)

◆ PIN_GPIO37

#define PIN_GPIO37   (0x00000094U)

◆ PIN_GPIO38

#define PIN_GPIO38   (0x00000098U)

◆ PIN_GPIO39

#define PIN_GPIO39   (0x0000009CU)

◆ PIN_GPIO40

#define PIN_GPIO40   (0x000000A0U)

◆ PIN_GPIO41

#define PIN_GPIO41   (0x000000A4U)

◆ PIN_GPIO42

#define PIN_GPIO42   (0x000000A8U)

◆ PIN_GPIO43

#define PIN_GPIO43   (0x000000ACU)

◆ PIN_GPIO44

#define PIN_GPIO44   (0x000000B0U)

◆ PIN_GPIO45

#define PIN_GPIO45   (0x000000B4U)

◆ PIN_GPIO46

#define PIN_GPIO46   (0x000000B8U)

◆ PIN_GPIO47

#define PIN_GPIO47   (0x000000BCU)

◆ PIN_GPIO48

#define PIN_GPIO48   (0x000000C0U)

◆ PIN_GPIO49

#define PIN_GPIO49   (0x000000C4U)

◆ PIN_GPIO50

#define PIN_GPIO50   (0x000000C8U)

◆ PIN_GPIO51

#define PIN_GPIO51   (0x000000CCU)

◆ PIN_GPIO52

#define PIN_GPIO52   (0x000000D0U)

◆ PIN_GPIO53

#define PIN_GPIO53   (0x000000D4U)

◆ PIN_GPIO54

#define PIN_GPIO54   (0x000000D8U)

◆ PIN_GPIO55

#define PIN_GPIO55   (0x000000DCU)

◆ PIN_GPIO56

#define PIN_GPIO56   (0x000000E0U)

◆ PIN_GPIO57

#define PIN_GPIO57   (0x000000E4U)

◆ PIN_GPIO58

#define PIN_GPIO58   (0x000000E8U)

◆ PIN_GPIO59

#define PIN_GPIO59   (0x000000ECU)

◆ PIN_GPIO60

#define PIN_GPIO60   (0x000000F0U)

◆ PIN_GPIO61

#define PIN_GPIO61   (0x000000F4U)

◆ PIN_GPIO62

#define PIN_GPIO62   (0x000000F8U)

◆ PIN_GPIO63

#define PIN_GPIO63   (0x000000FCU)

◆ PIN_GPIO64

#define PIN_GPIO64   (0x00000100U)

◆ PIN_GPIO65

#define PIN_GPIO65   (0x00000104U)

◆ PIN_GPIO66

#define PIN_GPIO66   (0x00000108U)

◆ PIN_GPIO67

#define PIN_GPIO67   (0x0000010CU)

◆ PIN_GPIO68

#define PIN_GPIO68   (0x00000110U)

◆ PIN_GPIO69

#define PIN_GPIO69   (0x00000114U)

◆ PIN_GPIO70

#define PIN_GPIO70   (0x00000118U)

◆ PIN_GPIO71

#define PIN_GPIO71   (0x0000011CU)

◆ PIN_GPIO72

#define PIN_GPIO72   (0x00000120U)

◆ PIN_GPIO73

#define PIN_GPIO73   (0x00000124U)

◆ PIN_GPIO74

#define PIN_GPIO74   (0x00000128U)

◆ PIN_GPIO75

#define PIN_GPIO75   (0x0000012CU)

◆ PIN_GPIO76

#define PIN_GPIO76   (0x00000130U)

◆ PIN_GPIO77

#define PIN_GPIO77   (0x00000134U)

◆ PIN_GPIO78

#define PIN_GPIO78   (0x00000138U)

◆ PIN_GPIO79

#define PIN_GPIO79   (0x0000013CU)

◆ PIN_GPIO80

#define PIN_GPIO80   (0x00000140U)

◆ PIN_GPIO81

#define PIN_GPIO81   (0x00000144U)

◆ PIN_GPIO82

#define PIN_GPIO82   (0x00000148U)

◆ PIN_GPIO83

#define PIN_GPIO83   (0x0000014CU)

◆ PIN_GPIO84

#define PIN_GPIO84   (0x00000150U)

◆ PIN_GPIO85

#define PIN_GPIO85   (0x00000154U)

◆ PIN_GPIO86

#define PIN_GPIO86   (0x00000158U)

◆ PIN_GPIO87

#define PIN_GPIO87   (0x0000015CU)

◆ PIN_GPIO88

#define PIN_GPIO88   (0x00000160U)

◆ PIN_GPIO89

#define PIN_GPIO89   (0x00000164U)

◆ PIN_GPIO90

#define PIN_GPIO90   (0x00000168U)

◆ PIN_GPIO91

#define PIN_GPIO91   (0x0000016CU)

◆ PIN_GPIO92

#define PIN_GPIO92   (0x00000170U)

◆ PIN_GPIO93

#define PIN_GPIO93   (0x00000174U)

◆ PIN_GPIO94

#define PIN_GPIO94   (0x00000178U)

◆ PIN_GPIO95

#define PIN_GPIO95   (0x0000017CU)

◆ PIN_GPIO96

#define PIN_GPIO96   (0x00000180U)

◆ PIN_GPIO97

#define PIN_GPIO97   (0x00000184U)

◆ PIN_GPIO98

#define PIN_GPIO98   (0x00000188U)

◆ PIN_GPIO99

#define PIN_GPIO99   (0x0000018CU)

◆ PIN_GPIO100

#define PIN_GPIO100   (0x00000190U)

◆ PIN_GPIO101

#define PIN_GPIO101   (0x00000194U)

◆ PIN_GPIO102

#define PIN_GPIO102   (0x00000198U)

◆ PIN_GPIO103

#define PIN_GPIO103   (0x0000019CU)

◆ PIN_GPIO104

#define PIN_GPIO104   (0x000001A0U)

◆ PIN_GPIO105

#define PIN_GPIO105   (0x000001A4U)

◆ PIN_GPIO106

#define PIN_GPIO106   (0x000001A8U)

◆ PIN_GPIO107

#define PIN_GPIO107   (0x000001ACU)

◆ PIN_GPIO108

#define PIN_GPIO108   (0x000001B0U)

◆ PIN_GPIO109

#define PIN_GPIO109   (0x000001B4U)

◆ PIN_GPIO110

#define PIN_GPIO110   (0x000001B8U)

◆ PIN_GPIO111

#define PIN_GPIO111   (0x000001BCU)

◆ PIN_GPIO112

#define PIN_GPIO112   (0x000001C0U)

◆ PIN_GPIO113

#define PIN_GPIO113   (0x000001C4U)

◆ PIN_GPIO114

#define PIN_GPIO114   (0x000001C8U)

◆ PIN_GPIO115

#define PIN_GPIO115   (0x000001CCU)

◆ PIN_GPIO116

#define PIN_GPIO116   (0x000001D0U)

◆ PIN_GPIO117

#define PIN_GPIO117   (0x000001D4U)

◆ PIN_GPIO118

#define PIN_GPIO118   (0x000001D8U)

◆ PIN_GPIO119

#define PIN_GPIO119   (0x000001DCU)

◆ PIN_GPIO120

#define PIN_GPIO120   (0x000001E0U)

◆ PIN_GPIO121

#define PIN_GPIO121   (0x000001E4U)

◆ PIN_GPIO122

#define PIN_GPIO122   (0x000001E8U)

◆ PIN_GPIO123

#define PIN_GPIO123   (0x000001ECU)

◆ PIN_GPIO124

#define PIN_GPIO124   (0x000001F0U)

◆ PIN_GPIO125

#define PIN_GPIO125   (0x000001F4U)

◆ PIN_GPIO126

#define PIN_GPIO126   (0x000001F8U)

◆ PIN_GPIO127

#define PIN_GPIO127   (0x000001FCU)

◆ PIN_GPIO128

#define PIN_GPIO128   (0x00000200U)

◆ PIN_GPIO129

#define PIN_GPIO129   (0x00000204U)

◆ PIN_GPIO130

#define PIN_GPIO130   (0x00000208U)

◆ PIN_GPIO131

#define PIN_GPIO131   (0x0000020CU)

◆ PIN_GPIO132

#define PIN_GPIO132   (0x00000210U)

◆ PIN_GPIO133

#define PIN_GPIO133   (0x00000214U)

◆ PIN_GPIO134

#define PIN_GPIO134   (0x00000218U)

◆ PIN_GPIO135

#define PIN_GPIO135   (0x0000021CU)

◆ PIN_GPIO136

#define PIN_GPIO136   (0x00000220U)

◆ PIN_GPIO137

#define PIN_GPIO137   (0x00000224U)

◆ PIN_GPIO138

#define PIN_GPIO138   (0x00000228U)

◆ PIN_GPIO139

#define PIN_GPIO139   (0x0000022CU)

◆ PIN_GPIO140

#define PIN_GPIO140   (0x00000230U)

◆ PIN_WARMRSTn

#define PIN_WARMRSTn   (0x00000234U)

◆ PIN_SAFETY_ERRORn

#define PIN_SAFETY_ERRORn   (0x00000238U)

◆ PIN_TDI

#define PIN_TDI   (0x0000023CU)

◆ PIN_TDO

#define PIN_TDO   (0x00000240U)

◆ PIN_TMS

#define PIN_TMS   (0x00000244U)

◆ PIN_TCK

#define PIN_TCK   (0x00000248U)

◆ PIN_OSPI0_CLKLB

#define PIN_OSPI0_CLKLB   (0x0000024CU)

◆ PIN_OSPI1_CLKLB

#define PIN_OSPI1_CLKLB   (0x00000250U)

◆ PIN_PORz

#define PIN_PORz   (0x00000254U)

◆ PIN_XTAL_XI

#define PIN_XTAL_XI   (0x00000258U)

◆ PIN_XTAL_XO

#define PIN_XTAL_XO   (0x0000025CU)

◆ PIN_ADC0_AIN0

#define PIN_ADC0_AIN0   (0x00000260U)

◆ PIN_ADC0_AIN1

#define PIN_ADC0_AIN1   (0x00000264U)

◆ PIN_ADC0_AIN2

#define PIN_ADC0_AIN2   (0x00000268U)

◆ PIN_ADC0_AIN3

#define PIN_ADC0_AIN3   (0x0000026CU)

◆ PIN_ADC0_AIN4

#define PIN_ADC0_AIN4   (0x00000270U)

◆ PIN_ADC0_AIN5

#define PIN_ADC0_AIN5   (0x00000274U)

◆ PIN_ADC0_AIN6

#define PIN_ADC0_AIN6   (0x00000278U)

◆ PIN_ADC1_AIN0

#define PIN_ADC1_AIN0   (0x0000027CU)

◆ PIN_ADC1_AIN1

#define PIN_ADC1_AIN1   (0x00000280U)

◆ PIN_ADC1_AIN2

#define PIN_ADC1_AIN2   (0x00000284U)

◆ PIN_ADC1_AIN3

#define PIN_ADC1_AIN3   (0x00000288U)

◆ PIN_ADC1_AIN4

#define PIN_ADC1_AIN4   (0x0000028CU)

◆ PIN_ADC1_AIN5

#define PIN_ADC1_AIN5   (0x00000290U)

◆ PIN_ADC1_AIN6

#define PIN_ADC1_AIN6   (0x00000294U)

◆ PIN_ADC2_AIN0

#define PIN_ADC2_AIN0   (0x00000298U)

◆ PIN_ADC2_AIN1

#define PIN_ADC2_AIN1   (0x0000029CU)

◆ PIN_ADC2_AIN2

#define PIN_ADC2_AIN2   (0x000002A0U)

◆ PIN_ADC2_AIN3

#define PIN_ADC2_AIN3   (0x000002A4U)

◆ PIN_ADC2_AIN4

#define PIN_ADC2_AIN4   (0x000002A8U)

◆ PIN_ADC2_AIN5

#define PIN_ADC2_AIN5   (0x000002ACU)

◆ PIN_ADC2_AIN6

#define PIN_ADC2_AIN6   (0x000002B0U)

◆ PIN_ADC3_AIN0

#define PIN_ADC3_AIN0   (0x000002B4U)

◆ PIN_ADC3_AIN1

#define PIN_ADC3_AIN1   (0x000002B8U)

◆ PIN_ADC3_AIN2

#define PIN_ADC3_AIN2   (0x000002BCU)

◆ PIN_ADC3_AIN3

#define PIN_ADC3_AIN3   (0x000002C0U)

◆ PIN_ADC3_AIN4

#define PIN_ADC3_AIN4   (0x000002C4U)

◆ PIN_ADC3_AIN5

#define PIN_ADC3_AIN5   (0x000002C8U)

◆ PIN_ADC4_AIN0

#define PIN_ADC4_AIN0   (0x000002CCU)

◆ PIN_ADC4_AIN1

#define PIN_ADC4_AIN1   (0x000002D0U)

◆ PIN_ADC4_AIN2

#define PIN_ADC4_AIN2   (0x000002D4U)

◆ PIN_ADC4_AIN3

#define PIN_ADC4_AIN3   (0x000002D8U)

◆ PIN_ADC4_AIN4

#define PIN_ADC4_AIN4   (0x000002DCU)

◆ PIN_ADC4_AIN5

#define PIN_ADC4_AIN5   (0x000002E0U)

◆ PIN_ADC_VREFHISRC0

#define PIN_ADC_VREFHISRC0   (0x000002E4U)

◆ PIN_ADC_VREFLOSRC0

#define PIN_ADC_VREFLOSRC0   (0x000002E8U)

◆ PIN_ADC_VREFHI0

#define PIN_ADC_VREFHI0   (0x000002ECU)

◆ PIN_ADC_VREFLO0

#define PIN_ADC_VREFLO0   (0x000002F0U)

◆ PIN_ADC_VREFHI1

#define PIN_ADC_VREFHI1   (0x000002F4U)

◆ PIN_ADC_VREFLO1

#define PIN_ADC_VREFLO1   (0x000002F8U)

◆ PIN_ADC_VREFHI2

#define PIN_ADC_VREFHI2   (0x000002FCU)

◆ PIN_ADC_VREFLO2

#define PIN_ADC_VREFLO2   (0x00000300U)

◆ PIN_ADC_VREFHISRC1

#define PIN_ADC_VREFHISRC1   (0x00000304U)

◆ PIN_ADC_VREFLOSRC1

#define PIN_ADC_VREFLOSRC1   (0x00000308U)

◆ PIN_ADC_VREFHI3

#define PIN_ADC_VREFHI3   (0x0000030CU)

◆ PIN_ADC_VREFLO3

#define PIN_ADC_VREFLO3   (0x00000310U)

◆ PIN_ADC_VREFHI4

#define PIN_ADC_VREFHI4   (0x00000314U)

◆ PIN_ADC_VREFLO4

#define PIN_ADC_VREFLO4   (0x00000318U)

◆ PIN_ADC_CAL0

#define PIN_ADC_CAL0   (0x0000031CU)

◆ PIN_ADC_CAL1

#define PIN_ADC_CAL1   (0x00000320U)

◆ PIN_DAC_VREF0

#define PIN_DAC_VREF0   (0x00000324U)

◆ PIN_DAC_VREF1

#define PIN_DAC_VREF1   (0x00000328U)

◆ PIN_DAC_OUT

#define PIN_DAC_OUT   (0x0000032CU)

◆ PIN_TEMPCAL

#define PIN_TEMPCAL   (0x00000330U)

◆ PIN_VSYS_MON

#define PIN_VSYS_MON   (0x00000334U)

◆ PIN_ATESTV0

#define PIN_ATESTV0   (0x00000338U)

◆ PIN_ATESTV1

#define PIN_ATESTV1   (0x0000033CU)

◆ PIN_PMUBYPASS

#define PIN_PMUBYPASS   (0x00000340U)

◆ PIN_USB0_CE

#define PIN_USB0_CE   (0x00000344U)

◆ PIN_SDADC0_DP

#define PIN_SDADC0_DP   (0x00000348U)

◆ PIN_SDADC0_DM

#define PIN_SDADC0_DM   (0x0000034CU)

◆ PIN_ADC_CAL2

#define PIN_ADC_CAL2   (0x00000350U)

◆ PIN_ADC_R0_AIN0

#define PIN_ADC_R0_AIN0   (0x00000354U)

◆ PIN_ADC_R0_AIN1

#define PIN_ADC_R0_AIN1   (0x00000358U)

◆ PIN_ADC_R0_AIN2

#define PIN_ADC_R0_AIN2   (0x0000035CU)

◆ PIN_ADC_R0_AIN3

#define PIN_ADC_R0_AIN3   (0x00000360U)

◆ PIN_ADC_VREFLO5

#define PIN_ADC_VREFLO5   (0x00000364U)

◆ PIN_ADC_VREFHI5

#define PIN_ADC_VREFHI5   (0x00000368U)

◆ PIN_ADC_VREFLO6

#define PIN_ADC_VREFLO6   (0x0000036CU)

◆ PIN_ADC_VREFHI6

#define PIN_ADC_VREFHI6   (0x00000370U)

◆ PIN_ADC_R1_AIN0

#define PIN_ADC_R1_AIN0   (0x00000374U)

◆ PIN_ADC_R1_AIN1

#define PIN_ADC_R1_AIN1   (0x00000378U)

◆ PIN_ADC_R1_AIN2

#define PIN_ADC_R1_AIN2   (0x0000037CU)

◆ PIN_ADC_R1_AIN3

#define PIN_ADC_R1_AIN3   (0x00000380U)

◆ PIN_ADC_CAL3

#define PIN_ADC_CAL3   (0x00000384U)

Function Documentation

◆ Pinmux_config()

void Pinmux_config ( const Pinmux_PerCfg_t *  pinmuxCfg,
uint32_t  domainId 
)

This API configures the pinmux based on the domain.

Parameters
pinmuxCfgPointer to list of pinmux configuration array. This parameter cannot be NULL and the last entry should be initialized with PINMUX_END so that this function knows the end of configuration.
domainIdDomain ID to set pinmux configuration. Refer Pinmux_DomainId_t

◆ Pinmux_qualPeriodConfig()

void Pinmux_qualPeriodConfig ( uint32_t  qualGroupIndex,
uint8_t  qualPeriod 
)

This API configures the Qualification period for a specific GPIO Pin group.

Parameters
qualGroupIndexIndex of GPIO Pin group for which the Period is being configured. Range is from 0-17.
qualPeriodQual Period value for the Pin group.

◆ Pinmux_enableUserMode()

void Pinmux_enableUserMode ( void  )

This API enables user mode access to the IOMUX register space.

◆ Pinmux_disableUserMode()

void Pinmux_disableUserMode ( void  )

This API disables user mode access to the IOMUX register space.