AM261x MCU+ SDK  26.00.00
USB DFU Example

Introduction

  • This example demonstrates the use of TinyUSB DFU DEV Class driver. Its implements all the necessary callbacks that are required by TinyUSB DFU (Device Firmware Upgrade) DEV class driver.
  • When user issues DFU download command then the application receives the data in a static buffer via USB DFU. Once the manifest state is completed the application sends the received data back to UART0.
  • When user issues DFU Upload command it sends the Hello world from AM261x DFU! - Partition 0 string back to the HOST PC.
  • refer USB2.0 DFU specs to know more about USB 2.0 DFU class.
Note
The max buffer size is 4 KB thus, as far as this example is concerned user can send at max 4 KB of data.

Supported Combinations

Parameter Value
CPU + OS r5fss0-0_nortos
Toolchain ti-arm-clang
iar-arm
Boards am261x-lp, am261x-som
Example folder examples/usb/device/dfu

Steps to Run the Example

Build the example

HW Setup

AM261x-LP

  • To test the application, one can use a Windows/Linux PC as a USB host.
  • Connect the J10 on AM261x-LP to the USB host.

USB Micro B Device Connector

AM261X-SOM

  • To test the application, one can use a Windows/Linux PC as a USB host
  • Connect the J7 on AM261x SOM to the USB host

USB Micro B Device Connector

Run the example

  • Launch a CCS or IAR EW debug session and run the executable, see CCS Launch, Load and Run or IAR Launch, Load and Run
  • When the application is running. Observer DFU device detected on HOST PC.
  • Open cmd in windows and terminal in case of Linux. Run the following command to detect whether a DFU device has been enumerated or not.

    Windows

    dfu-util -l 
    

    Linux

    sudo dfu-util -l 
    
  • If the enumeration is successful the following should be displayed on console.

AM64x-AM243x DFU Device detected.

DFU Download

  • Open COM port in windows and /dev/ttyUSBx in Linux which opens console for UART0.
  • Once the DFU device is enumerated run the following command.

    Windows

    dfu-util -a 0 -i 0 -D test_data.txt
    

    Linux

    sudo dfu-util -a 0 -i 0 -D test_data.txt
    
  • The test_data.txt file contains a string data that is to be transferred.
  • Once the DFU transfer is completed following will be displayed on the terminal.

DFU Download command successful
  • Open UART0 serial port to observe the content of test_data.txt file displayed on same serial port.

Content of received file displayed on serial port.

DFU Upload

  • Run the following command to read the data from DFU device.

    Windows

    dfu-util -a 0 -i 0 -U upload_data.txt 
    

    Linux

    sudo dfu-util -a 0 -i 0 -U upload_data.txt
    
  • Once the DFU Upload transaction is successful , open upload_data.txt file to see the contents

Data sent by DFU device to DFU host.

See Also

USB