AM261x MCU+ SDK  26.00.00
EPWM Deadband

Introduction

Diagram featuring the DeadBand working in EPWM

Example Description

The Example sets up the following EPMWs to showcase the Deadband features, as follows,

  1. CONFIG_EPWM0 : Deadband disabled (Reference)
  2. CONFIG_EPWM1 : Deadband Active High
  3. CONFIG_EPWM2 : Deadband Active Low
  4. CONFIG_EPWM3 : Deadband Active High Complimentary
  5. CONFIG_EPWM4 : Deadband Active Low Complimentary
  6. CONFIG_EPWM5 : Deadband Output Swap i.e., (switch A and B outputs)
  7. CONFIG_EPWM6 : Deadband On Rising and Falling edges.
  8. SYNC_PWM : To sync all the PWMs and the ECAPs

The sequence of operations to obtain the deadband occur in the following manner,

  1. Input (EPWMx_A or EPWMx_B) is selected for operation
  2. Rising edge delay operation (if selected)
  3. Falling edge delay operation (if selected)
  4. Inversion of the RED / FED output (if selected)
  5. Output Swap (if selected)

Note :

  • All the EPWM in the example are synced with CONFIG_EPWM0 as its Counter reaches 0 and all EPMWs start counting up from 0 when sync pulse reaches.

EPWM DeadBand Example Block Diagram

External Connections

AM263X-CC or AM263PX-CC

When using AM263x-CC with TMDSHSECDOCK (HSEC180 controlCARD Baseboard Docking Station) Probe the following

  • CONFIG_EPWM0 output on HSEC PIN 49 (EPWM0_A)
  • CONFIG_EPWM0 output on HSEC PIN 51 (EPWM0_B)
  • CONFIG_EPWM1 output on HSEC PIN 53 (EPWM1_A)
  • CONFIG_EPWM1 output on HSEC PIN 55 (EPWM1_B)
  • CONFIG_EPWM2 output on HSEC PIN 50 (EPWM2_A)
  • CONFIG_EPWM2 output on HSEC PIN 52 (EPWM2_B)
  • CONFIG_EPWM3 output on HSEC PIN 54 (EPWM3_A)
  • CONFIG_EPWM3 output on HSEC PIN 56 (EPWM3_B)
  • CONFIG_EPWM4 output on HSEC PIN 153 (EPWM13_A)
  • CONFIG_EPWM4 output on HSEC PIN 154 (EPWM13_B)
  • CONFIG_EPWM5 output on HSEC PIN 159 (EPWM15_A)
  • CONFIG_EPWM5 output on HSEC PIN 160 (EPWM15_B)
  • CONFIG_EPWM6 output on HSEC PIN 57 (EPWM4_A)
  • CONFIG_EPWM6 output on HSEC PIN 59 (EPWM4_B) Early Access:AM263Px-CC E1 EPWM 15_A/15_B doesn't have a pinout so insted used EPWM 5_A/5_B ie: CONFIG_EPWM5 output on HSEC PIN 61 (EPWM5_A) and CONFIG_EPWM5 output on HSEC PIN 63 (EPWM5_B)

AM261X-SOM

When using AM261x-SOM with TMDSHSECDOCK (HSEC180 controlCARD Baseboard Docking Station) Probe the following

  • CONFIG_EPWM0 output on HSEC PIN 49 (EPWM0_A)
  • CONFIG_EPWM0 output on HSEC PIN 51 (EPWM0_B)
  • CONFIG_EPWM1 output on HSEC PIN 53 (EPWM1_A)
  • CONFIG_EPWM1 output on HSEC PIN 55 (EPWM1_B)
  • CONFIG_EPWM2 output on HSEC PIN 50 (EPWM2_A)
  • CONFIG_EPWM2 output on HSEC PIN 52 (EPWM2_B)
  • CONFIG_EPWM3 output on HSEC PIN 54 (EPWM3_A)
  • CONFIG_EPWM3 output on HSEC PIN 56 (EPWM3_B)
  • CONFIG_EPWM4 output on HSEC PIN 57 (EPWM4_A)
  • CONFIG_EPWM4 output on HSEC PIN 59 (EPWM4_B)
  • CONFIG_EPWM5 output on HSEC PIN 61 (EPWM5_A)
  • CONFIG_EPWM5 output on HSEC PIN 63 (EPWM5_B)
  • CONFIG_EPWM6 output on HSEC PIN 58 (EPWM6_A)
  • CONFIG_EPWM6 output on HSEC PIN 60 (EPWM6_B)

AM263X-LP or AM263PX-LP

Probe the following

  • CONFIG_EPWM0 output on PIN J2/4 11 (EPWM0_A)
  • CONFIG_EPWM0 output on PIN J6/8 59 (EPWM0_B)
  • CONFIG_EPWM1 output on PIN J2/4 37 (EPWM1_A)
  • CONFIG_EPWM1 output on PIN J2/4 38 (EPWM1_B)
  • CONFIG_EPWM2 output on PIN J2/4 39 (EPWM2_A)
  • CONFIG_EPWM2 output on PIN J2/4 40 (EPWM2_B)
  • CONFIG_EPWM3 output on PIN J6/8 77 (EPWM3_A)
  • CONFIG_EPWM3 output on PIN J6/8 78 (EPWM3_B)
  • CONFIG_EPWM4 output on PIN J6/8 79 (EPWM13_A)
  • CONFIG_EPWM4 output on PIN J6/8 80 (EPWM13_B)
  • CONFIG_EPWM5 output on PIN J2/4 34 (EPWM15_A)
  • CONFIG_EPWM5 output on PIN J5/7 45 (EPWM15_B)
  • CONFIG_EPWM6 output on PIN J2/4 35 (EPWM14_A)
  • CONFIG_EPWM6 output on PIN J2/4 36 (EPWM14_B)

AM261X-LP

Probe the following

  • CONFIG_EPWM0 output on PIN J6/8 76 (EPWM7_A)
  • CONFIG_EPWM0 output on PIN J6/8 75 (EPWM7_B)
  • CONFIG_EPWM1 output on PIN J5/7 69 (EPWM1_A)
  • CONFIG_EPWM1 output on PIN J5/7 63 (EPWM1_B)
  • CONFIG_EPWM2 output on PIN J2/4 40 (EPWM2_A)
  • CONFIG_EPWM2 output on PIN J2/4 39 (EPWM2_B)
  • CONFIG_EPWM3 output on PIN J2/4 38 (EPWM3_A)
  • CONFIG_EPWM3 output on PIN J2/4 37 (EPWM3_B)
  • CONFIG_EPWM4 output on PIN J2/4 36 (EPWM4_A)
  • CONFIG_EPWM4 output on PIN J2/4 35 (EPWM4_B)
  • CONFIG_EPWM5 output on PIN J6/8 80 (EPWM5_A)
  • CONFIG_EPWM5 output on PIN J2/4 13 (EPWM5_B)
  • CONFIG_EPWM6 output on PIN J6/8 78 (EPWM6_A)
  • CONFIG_EPWM6 output on PIN J6/8 77 (EPWM6_B)

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 nortos
Toolchain ti-arm-clang
Board am261x-som, am261x-lp
Example folder examples/drivers/epwm/epwm_deadband/

Steps to Run the Example

  • When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
  • When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)
  • Establish connections as mentioned in External Connections section
  • Launch a CCS debug session and run the executable, see CCS Launch, Load and Run

See Also

EPWM

Sample Output

Shown below is a sample output when the application is run,

EPWM DeadBand Test Started ...
EPWM DeadBand Example runs for 5 Secs
Rising Edge timestamp of Reference waveform : 503
Rising Edge timestamp of Deadband Active High output B : 503 (Same as Reference Rising Edge Timestamp)
Rising Edge timestamp of Deadband Active High output A : 903 (Reference Rising Edge Timestamp + Rising Edge Delay)
Falling Edge timestamp of Reference waveform : 3503
Falling Edge timestamp of Deadband Active High output A : 3503 (Same as Reference Falling Edge Timestamp)
Falling Edge timestamp of Deadband Active High output B : 3703 (Reference Falling Edge Timestamp + Falling Edge Delay)
Observed Rising Edege Delay : 400
Observed Falling Edege Delay : 200
EPWM DeadBand Test Passed!!
All tests have passed!!

EPWM DeadBand Example Sample Capture