AM243x MCU+ SDK  12.01.00

Introduction

This file contains the prototype of ASYMMETRIC CRYPTOGRAPHY driver APIs.

Go to the source code of this file.

Data Structures

struct  AsymCrypt_RSAPubkey
 RSA public key. All values are in biginteger format (size followed by word value array, least significant word first) More...
 
struct  AsymCrypt_RSAPrivkey
 RSA private key. All values are in biginteger format (size followed by word value array, least significant word first) More...
 
struct  AsymCrypt_ECPoint
 EC Point, also the public key. More...
 
struct  AsymCrypt_ECPrimeCurveP
 EC prime curve parameters. More...
 
struct  AsymCrypt_ECMontCurveP
 EC Montogomery curve parameters. More...
 
struct  AsymCrypt_ECDSASig
 ECDSA signature. More...
 
struct  AsymCrypt_EddsaPoint
 Point on Eddsa Elliptical Curve. More...
 
struct  AsymCrypt_EdCurveParam
 Structure to hold Edward Curve Eddsa parameters. More...
 
struct  AsymCrypt_EddsaSig
 Eddsa EDDSA signature. More...
 
struct  AsymCrypt_EddsaKey
 Eddsa EDDSA Private key - Public key pair in uint8 array form. More...
 
struct  AsymCrypt_SM2DSASig
 SM2DSA signature. More...
 

Macros

#define ASYM_CRYPT_RETURN_SUCCESS   (0xCEF6A572U)
 
#define ASYM_CRYPT_RETURN_FAILURE   (0xD20341DDU)
 
#define ASYM_CRYPT_CURVE_TYPE_EDDSA_25519   (0xBE2479A0U)
 
#define ASYM_CRYPT_CURVE_TYPE_EDDSA_448   (0x57138CAFU)
 
#define RSA_MAX_LENGTH   (130U)
 
#define ECDSA_MAX_LENGTH   (18U)
 
#define EC_PARAM_MAXLEN   (68U)
 
#define ASYM_CRYPT_LEN(bytelen)   (((bytelen) / 4U) + 1U)
 
#define RSA_KEY_E_MAXLEN   (8U)
 
#define RSA_KEY_N_MAXLEN   (520U)
 
#define RSA_KEY_PQ_MAXLEN   ((RSA_KEY_N_MAXLEN / 2U) + 4U)
 
#define RSA_SIG_MAXLEN   (RSA_KEY_N_MAXLEN)
 
#define EDDSA_MAX_KEY_LEN   (57U)
 
#define EDDSA_MAX_BIGINT_LEN   (ASYM_CRYPT_LEN(EDDSA_MAX_KEY_LEN - 1U))
 
#define EDDSA_ED25519_KEY_LEN   (32U)
 
#define EDDSA_ED448_KEY_LEN   (57U)
 
#define EDDSA_ED25519_HASH_LEN   (64U)
 
#define EDDSA_ED448_HASH_LEN   (114U)
 
#define DEVTYPE_HSSE   (0x0AU)
 device type HSSE More...
 

Typedefs

typedef uint32_t AsymCrypt_Return_t
 ASYM CRYPTO Driver Error code. More...
 
typedef uint32_t AsymCrypt_EdCurveType_t
 ASYM EDDSA Curve Type. More...
 
typedef void * AsymCrypt_Handle
 Handle to the AsymCrypt driver. More...
 
typedef AsymCrypt_Return_t(* AsymCrypt_ExecuteShaCallback) (uint8_t *in_addr, uint32_t length, uint8_t *sha_addr)
 This callback implemented to configure a SHA for EDDSA algorithms. More...
 

Functions

AsymCrypt_Handle AsymCrypt_open (uint32_t index)
 Function to Open AsymCrypt instance, enable AsymCrypt engine, Initialize clocks. More...
 
AsymCrypt_Return_t AsymCrypt_close (AsymCrypt_Handle handle)
 Function to close a AsymCrypt module specified by the AsymCrypt handle. More...
 
AsymCrypt_Return_t AsymCrypt_RSAPrivate (AsymCrypt_Handle handle, const uint32_t m[RSA_MAX_LENGTH], const struct AsymCrypt_RSAPrivkey *k, uint32_t result[RSA_MAX_LENGTH])
 This Function performs Decryption or Signing operations. More...
 
AsymCrypt_Return_t AsymCrypt_RSAPublic (AsymCrypt_Handle handle, const uint32_t m[RSA_MAX_LENGTH], const struct AsymCrypt_RSAPubkey *k, uint32_t result[RSA_MAX_LENGTH])
 This Function performs Encryption or Verification operations. More...
 
AsymCrypt_Return_t AsymCrypt_RSAKeyGenPrivate (AsymCrypt_Handle handle, struct AsymCrypt_RSAPrivkey *k, uint32_t keybitsize)
 This Function performs Encryption or Verification operations. More...
 
AsymCrypt_Return_t AsymCrypt_RSAKeyGenPublic (AsymCrypt_Handle handle, const struct AsymCrypt_RSAPrivkey *privKey, struct AsymCrypt_RSAPubkey *pubKey, uint32_t keybitsize)
 This Function performs Encryption or Verification operations. More...
 
AsymCrypt_Return_t AsymCrypt_ECDSASign (AsymCrypt_Handle handle, const struct AsymCrypt_ECPrimeCurveP *cp, const uint32_t priv[ECDSA_MAX_LENGTH], const uint32_t k[ECDSA_MAX_LENGTH], const uint32_t h[ECDSA_MAX_LENGTH], struct AsymCrypt_ECDSASig *sig, uint32_t curveId)
 ECDSA sign primitive function. More...
 
AsymCrypt_Return_t AsymCrypt_ECDSAVerify (AsymCrypt_Handle handle, const struct AsymCrypt_ECPrimeCurveP *cp, const struct AsymCrypt_ECPoint *pub, const struct AsymCrypt_ECDSASig *sig, const uint32_t h[ECDSA_MAX_LENGTH], uint32_t curveId)
 ECDSA verify primitive function. More...
 
AsymCrypt_Return_t AsymCrypt_ECDSAKeyGenPrivate (AsymCrypt_Handle handle, const struct AsymCrypt_ECPrimeCurveP *cp, uint32_t priv[ECDSA_MAX_LENGTH], uint32_t curveType)
 ECDSA KeyGen Private Key function. More...
 
AsymCrypt_Return_t AsymCrypt_ECDSAKeyGenPublic (AsymCrypt_Handle handle, const struct AsymCrypt_ECPrimeCurveP *cp, struct AsymCrypt_ECPoint *pub, const uint32_t priv[ECDSA_MAX_LENGTH], uint32_t curveType)
 ECDSA KeyGen Public Key function. More...
 
AsymCrypt_Return_t AsymCrypt_EddsaGetPubKey (AsymCrypt_Handle handle, AsymCrypt_ExecuteShaCallback shaCbFxn, uint8_t privKey[EDDSA_MAX_KEY_LEN], uint8_t pubKey[EDDSA_MAX_KEY_LEN], AsymCrypt_EdCurveType_t input_curve)
 ECDSA KeyGen Public Key function. More...
 
AsymCrypt_Return_t AsymCrypt_EddsaSign (AsymCrypt_Handle handle, AsymCrypt_ExecuteShaCallback shaCbFxn, const struct AsymCrypt_EddsaKey *key, const uint8_t *ptrData, const uint32_t dataSizeByte, struct AsymCrypt_EddsaSig *sig, AsymCrypt_EdCurveType_t input_curve)
 EDDSA Signing primitive function. More...
 
AsymCrypt_Return_t AsymCrypt_EddsaVerify (AsymCrypt_Handle handle, AsymCrypt_ExecuteShaCallback shaCbFxn, const uint8_t pubKey[EDDSA_MAX_KEY_LEN], const uint8_t *ptrData, const uint32_t dataSizeByte, const struct AsymCrypt_EddsaSig *sig, AsymCrypt_EdCurveType_t input_curve)
 ECDSA verify primitive function. More...
 
AsymCrypt_Return_t AsymCrypt_EcdhGenSharedSecret (AsymCrypt_Handle handle, const struct AsymCrypt_ECPrimeCurveP *cp, const uint32_t priv[ECDSA_MAX_LENGTH], const struct AsymCrypt_ECPoint *pubKey, struct AsymCrypt_ECPoint *ecShSecret, uint32_t curveType)
 ECDH shared secret generation function. More...
 
AsymCrypt_Return_t AsymCrypt_SM2DSASign (AsymCrypt_Handle handle, const uint32_t priv[ECDSA_MAX_LENGTH], const uint32_t k[ECDSA_MAX_LENGTH], const uint32_t h[ECDSA_MAX_LENGTH], struct AsymCrypt_SM2DSASig *sig)
 SM2DSA sign primitive function. More...
 
AsymCrypt_Return_t AsymCrypt_SM2DSAVerify (AsymCrypt_Handle handle, const struct AsymCrypt_ECPoint *pub, const struct AsymCrypt_SM2DSASig *sig, const uint32_t h[ECDSA_MAX_LENGTH])
 SM2DSA verify primitive function. More...
 
AsymCrypt_Return_t AsymCrypt_SM2DSAKeyGenPrivate (AsymCrypt_Handle handle, uint32_t priv[ECDSA_MAX_LENGTH])
 SM2DSA KeyGen Private Key function. More...
 
AsymCrypt_Return_t AsymCrypt_SM2DSAKeyGenPublic (AsymCrypt_Handle handle, struct AsymCrypt_ECPoint *pub, const uint32_t priv[ECDSA_MAX_LENGTH])
 SM2DSA KeyGen Public Key function. More...