hsrPrp_Config Structure storing the global variables
uint16_t hsrPrp_Config::redSeqNr |
uint16_t hsrPrp_Config::supSeqNr |
int* hsrPrp_Config::collision_pkt_dropped |
int* hsrPrp_Config::num_of_collision_occured |
ICSS_EMAC_Handle hsrPrp_Config::icssEmacHandle |
uint32_t hsrPrp_Config::redPruCheckTimerHostTableFlag |
uint32_t hsrPrp_Config::redPruCheckTimerNodeTableClear |
ClockP_Object hsrPrp_Config::redPruCheckTimer |
ClockP_Object hsrPrp_Config::redLifeCheckTimer |
RED_FRAME* hsrPrp_Config::redSupFrame |
TaskP_Object hsrPrp_Config::redSupTask |
TaskP_Object hsrPrp_Config::hsrPrpNodetableRefreshTask |
SemaphoreP_Object hsrPrp_Config::redLifeCheckSemaphore |
SemaphoreP_Object hsrPrp_Config::nodesTableSemaphore |
RED_INDEX_ARRAY_ENTRY* hsrPrp_Config::indexArrayBase |
RED_BIN_ARRAY_ENTRY* hsrPrp_Config::binArrayBase |
RED_NODE_TABLE_ENTRY* hsrPrp_Config::nodeTableBase |