Node Table Entry.
Data Fields | |
uint8_t | src [ETHER_ADDR_LEN] |
uint8_t | state |
uint8_t | status |
uint32_t | cntRxA |
uint32_t | cntRxB |
uint32_t | errRxA |
uint32_t | errRxB |
uint8_t | cntRxSupA |
uint8_t | cntRxSupB |
uint16_t | timeLasSeenS |
uint16_t | timeLasSeenA |
uint16_t | timeLasSeenB |
uint8_t RED_NODE_TABLE_ENTRY::src[ETHER_ADDR_LEN] |
Source Address (MAC address of the node)
uint8_t RED_NODE_TABLE_ENTRY::state |
Valid (1) / Invalid (0)
uint8_t RED_NODE_TABLE_ENTRY::status |
Duplicate Discard [8:7] and Node Type [5:0]
uint32_t RED_NODE_TABLE_ENTRY::cntRxA |
Frames received on port A
uint32_t RED_NODE_TABLE_ENTRY::cntRxB |
Frames received on port B
uint32_t RED_NODE_TABLE_ENTRY::errRxA |
Erroneous frames received on port A
uint32_t RED_NODE_TABLE_ENTRY::errRxB |
Erroneous frames received on port B
uint8_t RED_NODE_TABLE_ENTRY::cntRxSupA |
Number of supervision frames received on port A
uint8_t RED_NODE_TABLE_ENTRY::cntRxSupB |
Number of supervision frames received on port B
uint16_t RED_NODE_TABLE_ENTRY::timeLasSeenS |
Time last seen of a supervision frame
uint16_t RED_NODE_TABLE_ENTRY::timeLasSeenA |
Time last seen of a frame received on port A
uint16_t RED_NODE_TABLE_ENTRY::timeLasSeenB |
Time last seen of a frame received on port B