uint32_t EI_API_ADP_getPortLogAnnounceInterval | ( | T * | pAdp_p, |
uint16_t * | pPortLogAnnounceInterval_p | ||
) |
Get the PortLogAnnounceInterval attribute of the Time Sync Object (Instance Attribute ID: 14).
Function that returns the PortLogAnnounceInterval member of the PortLogAnnounceIntervalCfg attribute for the EtherNet/IP adapter selected by parameter pAdp_p
in output parameter pPortLogAnnounceInterval
.
[in] | pAdp_p | Pointer to the adapter. |
[out] | pPortLogAnnounceInterval_p | uint16_t pointer to PortLogAnnounceInterval of the adapter Time Sync object specified by parameter pAdp_p . |
EI_API_ADP_eERR_OK | Success. |
EI_API_ADP_eERR_GENERAL | General error. |