uint32_t EI_API_ADP_setTimeSyncSupported | ( | T * | pAdp_p | ) |
Enable Time Sync Object support.
Enable Time Sync support. This function should only be called for applications that require EtherNet/IP Time Sync functionality.
[in] | pAdp_p | Pointer to the adapter. |
EI_API_ADP_eERR_OK | Success. |
EI_API_ADP_eERR_GENERAL | General error. |