uint32_t EI_API_ADP_getTimeSyncUserDescription | ( | T * | pAdp_p, |
char * | pUserDescription_p | ||
) |
Get the Description member of the UserDescription attribute of the Time Sync object (Instance Attribute ID: 23).
Function that returns the Description member of the UserDescription attribute for the adapter sleected by parameter pAdp_p
in output parameter pUserDescription_p
.
[in] | pAdp_p | Pointer to the adapter. |
[out] | pUserDescription_p | char pointer to UserDescription of the adapter Time Sync object specified by parameter pAdp_p . |
EI_API_ADP_eERR_OK | Success. |
EI_API_ADP_eERR_GENERAL | General error. |