uint32_t EI_API_ADP_getTimeSyncRevisionData | ( | T * | pAdp_p, |
char * | pRevisionData_p | ||
) |
Get the Revision member of the RevisionData attribute of the Time Sync object (Instance Attribute ID: 22).
Function that returns the Revision member of the RevisionData attribute for the adapter selected by parameter pAdp_p
in output parameter pRevisionData_p
.
[in] | pAdp_p | Pointer to the adapter. |
[out] | pRevisionData_p | char pointer to RevisionData of the adapter Time Sync object specified by parameter pAdp_p . |
EI_API_ADP_eERR_OK | Success. |
EI_API_ADP_eERR_GENERAL | General error. |