uint32_t EI_API_ADP_getDomainNumber | ( | T * | pAdp_p, |
uint8_t * | pDomainNumber_p | ||
) |
Get the DomainNumber attribute of the Time Sync Object (Instance Attribute ID: 18).
Function that returns the DomainNumber attribute in the Time Sync object of the EtherNet/IP adapter selected by parameter pAdp_p
in output parameter pDomainNumber_p
.
[in] | pAdp_p | Pointer to the adapter. |
[out] | pDomainNumber_p | uint8_t pointer to DomainNumber attribute. |
EI_API_ADP_eERR_OK | Success. |
EI_API_ADP_eERR_GENERAL | General error. |