uint32_t EI_API_ADP_getTimeSyncProductDescription | ( | T * | pAdp_p, |
char * | pProductDesc_p | ||
) |
Get the Description member of the ProductDescription attribute of the Time Sync Object (Instance Attribute ID: 21).
Function that returns the Description member of the ProductDescription attribute of the Time Sync Object for the adapter selected by parameter pAdp_p
in output parameter pProductDesc_p
.
[in] | pAdp_p | Pointer to the adapter. |
[out] | pProductDesc_p | char pointer to ProductDescription. |
EI_API_ADP_eERR_OK | Success. |
EI_API_ADP_eERR_GENERAL | General error. |