uint32_t EI_API_ADP_setIntfConfig | ( | T * | adp, |
uint8_t | intfId, | ||
EI_API_ADP_UIntfConf_t | intfConfig | ||
) |
Set the adapter Ethernet interface configuration (Instance Attribute ID: 6).
This function can be used to set the current adapter Ethernet interface configuration.
[in] | adp | Pointer to the adapter. |
[in] | intfId | Interface ID. |
intfConfig | New interface configuration. |
EI_API_ADP_OK | Success. |
EI_API_ADP_ERROR | General error. |