uint32_t EI_API_ADP_getIntfConfig | ( | T * | pAdp_p, |
uint8_t | intfId_p, | ||
EI_API_ADP_UIntfConf_t * | pIntfConf_p | ||
) |
Get the current adapter configuration of interface with the specified ID (Instance Attribute ID: 6).
Function that returns the adapter configuration of interface with ID intfId_p
.
[in] | pAdp_p | Pointer to the adapter. |
[in] | intfId_p | Interface ID. |
[out] | pIntfConf_p | Pointer to a union of type EI_API_ADP_UIntfConf_t . |
EI_API_ADP_eERR_OK | Success. |
EI_API_ADP_eERR_GENERAL | General error. |