|
EtherNet/IP™ Adapter
1.04.10
User Reference Manual
|
|
◆ EI_API_ADP_pruicssStop()
void EI_API_ADP_pruicssStop |
( |
void |
| ) |
|
ETHIP_API void EI_API_ADP_pruicssStop(void)
Stops the PRU0 and PRU1 firmware on the PRU-ICSS block instance specified in EI_API_ADP_pruicssInit.
Definition: EI_API_ADP_main.c:246
Definition: EI_API_ADP.h:177
ETHIP_API void EI_API_ADP_pruicssStart(void)
Starts the PRU0 and PRU1 firmware on the PRU-ICSS block instance specified in EI_API_ADP_pruicssInit.
Definition: EI_API_ADP_main.c:201
uint8_t ai8uMacAddr[EIP_MAC_ADDR_LEN]
Definition: EI_API_ADP.h:178
ETHIP_API uint32_t EI_API_ADP_pruicssInit(EIP_SLoadParameter *ptPara_p)
Load and initialize the EtherNet/IP firmware in the PRU.
Definition: EI_API_ADP_main.c:107