Non IO-Link related functions.
Functions | |
IOL_FUNC_DECL void | IOLM_API_vSetPortCount (INT8U u8PortCnt_p) |
Set the number of ports. More... | |
IOL_FUNC_DECL IOL_EErrorInfo | IOLM_API_eInit (void) |
Initialize stack. More... | |
IOL_FUNC_DECL void | IOLM_API_vRun (void) |
Mainloop run. More... | |
IOL_FUNC_DECL IOL_EErrorInfo IOLM_API_eInit | ( | void | ) |
Initialize stack.
This function has to be called once before any other call. It initializes the stack and its internal variables. If it was successful the stack is ready for communication.
IOL_FUNC_DECL void IOLM_API_vRun | ( | void | ) |
Mainloop run.
This is the Mainloop function. It has to be called at least once during an IO-Link cycle to process acyclic data or prepare data for the cyclic communication.
IOL_FUNC_DECL void IOLM_API_vSetPortCount | ( | INT8U | u8PortCnt_p | ) |
Set the number of ports.
This function has to be called once before any other call. It initializes the number of ports for further initialization of the stack and its internal variables. If it was successful the stack is ready to be initialized by IOLM_API_eInit.
[in] | u8PortCnt_p | The number of ports. |