IO-Link Master Types.
IO-Link definitions for Master and Device.
Data Structures | |
struct | IOL_SDirectParam1 |
This structure stores the Direct Parameter Page 1. More... | |
struct | IOL_SEventEntry |
This structure defines a event buffer entry. More... | |
Macros | |
#define | NULL ((void*)0) |
#define | FALSE ((TBOOL)0) |
#define | TRUE ((TBOOL)1) |
Typedefs | |
typedef char | CHAR8 |
8 bit character data type | |
typedef uint8_t | TBOOL |
Boolean data type (at least 1 bit) | |
typedef int8_t | INT8S |
8 bit signed integer | |
typedef int16_t | INT16S |
16 bit signed integer | |
typedef int32_t | INT32S |
32 bit signed integer | |
typedef uint8_t | INT8U |
8 bit unsigned integer | |
typedef uint16_t | INT16U |
16 bit unsigned integer | |
typedef uint32_t | INT32U |
32 bit unsigned integer | |
typedef float | FLOAT32 |
32 bit float | |
typedef double | FLOAT64 |
64 bit float | |
Enumerations | |
enum | IOL_ETransferMode { IOL_eTransferMode_INACTIVE = 0, IOL_eTransferMode_COM1, IOL_eTransferMode_COM2, IOL_eTransferMode_COM3, IOL_eTransferMode_DI, IOL_eTransferMode_DO } |
This enumeration indicates the requested operation mode. More... | |
enum | IOL_EODLen { IOL_eODLen_1_Byte = 0, IOL_eODLen_2_Byte, IOL_eODLen_8_Byte, IOL_eODLen_32_Byte } |
This enumeration indicates the number of OD bytes in M-sequence. | |
enum | IOL_ETransferStatus { IOL_eTransferStatus_OK, IOL_eTransferStatus_PARITY_ERROR, IOL_eTransferStatus_FRAMING_ERROR, IOL_eTransferStatus_OVERRUN } |
This enumeration contains supplementary information on the transfer. status. More... | |
enum | IOL_EErrorInfo { IOL_eErrorInfo_NONE = 0, IOL_eErrorInfo_NO_COMM, IOL_eErrorInfo_STATE_CONFLICT, IOL_eErrorInfo_PARAMETER_CONFLICT, IOL_eErrorInfo_TIMING_CONFLICT, IOL_eErrorInfo_NO_DATA, IOL_eErrorInfo_VALUE_OUT_OF_RANGE, IOL_eErrorInfo_ISDU_TIMEOUT, IOL_eErrorInfo_ISDU_NOT_SUPPORTED, IOL_eErrorInfo_TIMEOUT } |
This enumeration contains error information. More... | |
enum | IOL_EComChannel { IOL_eComChannel_PROCESS = 0x00, IOL_eComChannel_PAGE = 0x20, IOL_eComChannel_DIAGNOSIS = 0x40, IOL_eComChannel_ISDU = 0x60 } |
This enumeration indicates the communication channel for the access to the user data. | |
enum | IOL_EDirection { IOL_eDirection_WRITE = 0x00, IOL_eDirection_READ = 0x80 } |
This enumeration contains ISDU transport direction. More... | |
enum | IOL_EDLMode { IOL_eDLMode_INACTIVE = 0, IOL_eDLMode_STARTUP, IOL_eDLMode_PREOPERATE, IOL_eDLMode_OPERATE, IOL_eDLMode_UNPAIRING } |
This enumeration indicates the requested mode of the Master's DL on an individual port. More... | |
enum | IOL_EDLRealMode { IOL_eDLRealMode_INACTIVE = 0, IOL_eDLRealMode_COM1, IOL_eDLRealMode_COM2, IOL_eDLRealMode_COM3, IOL_eDLRealMode_COMLOST, IOL_eDLRealMode_ESTABCOM, IOL_eDLRealMode_ACTIVE, IOL_eDLRealMode_STARTUP, IOL_eDLRealMode_PREOPERATE, IOL_eDLRealMode_OPERATE, IOL_eDLRealMode_INVALID } |
This enumeration indicates the status of the DL-mode handler. More... | |
enum | IOL_EMSequence { IOL_eMSequence_TYPE_0 = 0, IOL_eMSequence_TYPE_1 = 0x40, IOL_eMSequence_TYPE_2 = 0x80, IOL_eMSequence_TYPE_MASK = 0xC0 } |
This enumeration contains the M-sequence types. More... | |
enum | IOL_EPDInStatus { IOL_ePDInStatus_VALID = 0, IOL_ePDInStatus_INVALID = 0x40 } |
This enumeration indicates the qualifier status of the Process Data (PD). More... | |
enum | IOL_EPDOutStatus { IOL_ePDOutStatus_PDOUTVALID = 0, IOL_ePDOutStatus_PDOUTINVALID, IOL_ePDOutStatus_RTFAULT } |
This enumeration indicates the qualifier status of the Process Data (PD). More... | |
enum | IOL_EMHInfo { IOL_eMHInfo_COMLOST = 0, IOL_eMHInfo_ILLEGAL_MESSAGETYPE, IOL_eMHInfo_CHECKSUM_MISMATCH } |
This enumeration contains the exception indication of the message handler. More... | |
enum | IOL_ETargetMode { IOL_eTargetMode_INACTIVE = 0, IOL_eTargetMode_DI, IOL_eTargetMode_DO, IOL_eTargetMode_CFGCOM, IOL_eTargetMode_AUTOCOM, IOL_eTargetMode_COM1, IOL_eTargetMode_COM2, IOL_eTargetMode_COM3, IOL_eTargetMode_OSSDE, IOL_eTargetMode_SAFETYCOM, IOL_eTargetMode_MIXEDSAFETYCOM } |
This enumeration indicates the requested operational mode of the port. More... | |
enum | IOL_EIQMode { IOL_eIQMode_INACTIVE = 0, IOL_eIQMode_IN, IOL_eIQMode_OUT } |
This enumeration indicates the requested IQ mode of the port. More... | |
enum | IOL_EBaudrate { IOL_eBaudrate_AUTO = 0, IOL_eBaudrate_COM1, IOL_eBaudrate_COM2, IOL_eBaudrate_COM3 } |
This enumeration indicates the transmission rate. More... | |
enum | IOL_EPortMode { IOL_ePortMode_INACTIVE = 0, IOL_ePortMode_DI, IOL_ePortMode_DO, IOL_ePortMode_COMREADY, IOL_ePortMode_READY_TO_OPERATE, IOL_ePortMode_SM_OPERATE, IOL_ePortMode_COMLOST, IOL_ePortMode_REVISION_FAULT, IOL_ePortMode_COMP_FAULT, IOL_ePortMode_SERNUM_FAULT, IOL_ePortMode_DS_FAULT, IOL_ePortMode_CYCTIME_FAULT, IOL_ePortMode_PORTPOWEROFF } |
This enumeration indicates changes or faults of the local communication mode. More... | |
enum | IOL_EDeviceMode { IOL_eDeviceMode_INACTIVE = 0, IOL_eDeviceMode_IDLE, IOL_eDeviceMode_SIO, IOL_eDeviceMode_ESTABCOM, IOL_eDeviceMode_COMx, IOL_eDeviceMode_STARTUP, IOL_eDeviceMode_IDENT_STARTUP, IOL_eDeviceMode_IDENT_CHANGE, IOL_eDeviceMode_PREOPERATE, IOL_eDeviceMode_OPERATE, IOL_eDeviceMode_PAIRING, IOL_eDeviceMode_TIMEOUT, IOL_eDeviceMode_TEMPORARY, IOL_eDeviceMode_PERMANENT, IOL_eDeviceMode_PAIRED, IOL_eDeviceMode_UNPAIRED, IOL_eDeviceMode_UNPAIRING } |
This enumeration indicates changes of communication states to the Device application. More... | |
enum | IOL_EIService { IOL_eIService_NO_SERVICE = 0, IOL_eIService_WR_REQ_8B_IDX, IOL_eIService_WR_REQ_8B_IDX_SIDX, IOL_eIService_WR_REQ_16B_IDX_SIDX, IOL_eIService_WR_RES_NOK, IOL_eIService_WR_RES_OK, IOL_eIService_RESERVED_1, IOL_eIService_RESERVED_2, IOL_eIService_RESERVED_3, IOL_eIService_RD_REQ_8B_IDX, IOL_eIService_RD_REQ_8B_IDX_SIDX, IOL_eIService_RD_REQ_16B_IDX_SIDX, IOL_eIService_RD_RES_NOK, IOL_eIService_RD_RES_OK, IOL_eIService_RESERVED_4, IOL_eIService_RESERVED_5 } |
This enumeration defines the I-Services of the ISDU. | |
enum | IOL_EDirectParam { IOL_eDirectParam_MasterCommand = 0, IOL_eDirectParam_MasterCycleTime, IOL_eDirectParam_MinCycleTime, IOL_eDirectParam_MSequenceCapability, IOL_eDirectParam_RevisionID, IOL_eDirectParam_ProcessDataIn, IOL_eDirectParam_ProcessDataOut, IOL_eDirectParam_VendorID1, IOL_eDirectParam_VendorID2, IOL_eDirectParam_DeviceID1, IOL_eDirectParam_DeviceID2, IOL_eDirectParam_DeviceID3, IOL_eDirectParam_FunctionID1, IOL_eDirectParam_FunctionID2, IOL_eDirectParam_Reserved, IOL_eDirectParam_SystemCommand, IOL_eDirectParam_MAX } |
This enumeration is a index list of the Direct Parameter Page 1. | |
enum | IOL_EMasterCommand { IOL_eMasterCommand_Fallback = 0x5A, IOL_eMasterCommand_Inactive = 0x5C, IOL_eMasterCommand_PreDLink = 0x5D, IOL_eMasterCommand_FullDLink = 0x5E, IOL_eMasterCommand_Unpairing = 0x5F, IOL_eMasterCommand_MasterIdent = 0x95, IOL_eMasterCommand_DeviceIdent = 0x96, IOL_eMasterCommand_DeviceStartup = 0x97, IOL_eMasterCommand_ProcessDataOutputOperate = 0x98, IOL_eMasterCommand_DeviceOperate = 0x99, IOL_eMasterCommand_DevicePreoperate = 0x9A, IOL_eMasterCommand_Jump_0 = 0xF0, IOL_eMasterCommand_Jump_1 = 0xF1, IOL_eMasterCommand_Jump_2 = 0xF2, IOL_eMasterCommand_Jump_3 = 0xF3, IOL_eMasterCommand_Jump_4 = 0xF4, IOL_eMasterCommand_Jump_5 = 0xF5, IOL_eMasterCommand_Jump_6 = 0xF6, IOL_eMasterCommand_Jump_7 = 0xF7, IOL_eMasterCommand_Jump_8 = 0xF8, IOL_eMasterCommand_Jump_9 = 0xF9, IOL_eMasterCommand_Jump_10 = 0xFA, IOL_eMasterCommand_Jump_11 = 0xFB, IOL_eMasterCommand_Jump_12 = 0xFC, IOL_eMasterCommand_Jump_13 = 0xFD, IOL_eMasterCommand_Jump_14 = 0xFE, IOL_eMasterCommand_WakeUp = 0xFF } |
This enumeration indicates the Master Commands. | |
enum | IOL_EISDUIndex { IOL_eISDUIndex_DirectParam1 = 0, IOL_eISDUIndex_DirectParam2 = 1, IOL_eISDUIndex_SystemCommand = 2, IOL_eISDUIndex_DataStorage = 3, IOL_eISDUIndex_DeviceAccessLocks = 12, IOL_eISDUIndex_ProfileCharacteristic = 13, IOL_eISDUIndex_PDInputDescriptor = 14, IOL_eISDUIndex_PDOutputDescriptor = 15, IOL_eISDUIndex_VendorName = 16, IOL_eISDUIndex_VendorText = 17, IOL_eISDUIndex_ProductName = 18, IOL_eISDUIndex_ProductID = 19, IOL_eISDUIndex_ProductText = 20, IOL_eISDUIndex_SerialNumber = 21, IOL_eISDUIndex_HardwareRevision = 22, IOL_eISDUIndex_FirmwareRevision = 23, IOL_eISDUIndex_AppSpecificTag = 24, IOL_eISDUIndex_ErrorCount = 32, IOL_eISDUIndex_DeviceStatus = 36, IOL_eISDUIndex_DetailedDeviceStatus = 37, IOL_eISDUIndex_ProcessDataInput = 40, IOL_eISDUIndex_ProcessDataOutput = 41, IOL_eISDUIndex_WirelessSystemMgmnt = 0x5001, IOL_eISDUIndex_WirelessSystemCfg = 0x5002, IOL_eISDUIndex_LinkQuality = 0x5003, IOL_eISDUIndex_WBridgeInfo = 0x5004, IOL_eISDUIndex_WirelessRadioInfo = 0x5005, IOL_eISDUIndex_AdaptiveHopTable = 0x5006 } |
This enumeration indicates the predefined index values for ISDU. | |
enum | IOL_EErrorType { IOL_eErrorType_NONE = 0, IOL_eErrorType_APP_DEV = 0x8000, IOL_eErrorType_IDX_NOTAVAIL = 0x8011, IOL_eErrorType_SUBIDX_NOTAVAIL = 0x8012, IOL_eErrorType_SERV_NOTAVAIL = 0x8020, IOL_eErrorType_SERV_NOTAVAIL_LOCCTRL = 0x8021, IOL_eErrorType_SERV_NOTAVAIL_DEVCTRL = 0x8022, IOL_eErrorType_IDX_NOT_WRITEABLE = 0x8023, IOL_eErrorType_PAR_VALOUTOFRNG = 0x8030, IOL_eErrorType_PAR_VALGTLIM = 0x8031, IOL_eErrorType_PAR_VALLTLIM = 0x8032, IOL_eErrorType_VAL_LENOVRRUN = 0x8033, IOL_eErrorType_VAL_LENUNDRUN = 0x8034, IOL_eErrorType_FUNC_NOTAVAIL = 0x8035, IOL_eErrorType_FUNC_UNAVAILTEMP = 0x8036, IOL_eErrorType_PAR_SETINVALID = 0x8040, IOL_eErrorType_PAR_SETINCONSIST = 0x8041, IOL_eErrorType_APP_DEVNOTRDY = 0x8082, IOL_eErrorType_UNSPECIFIC = 0x8100, IOL_eErrorType_VENDOR_SPECIFIC_BEGIN = 0x8101, IOL_eErrorType_VENDOR_SPECIFIC_END = 0x81FF, IOL_eErrorType_COM_ERR = 0x1000, IOL_eErrorType_I_SERVICE_TIMEOUT = 0x1100, IOL_eErrorType_M_ISDU_CHECKSUM = 0x5600, IOL_eErrorType_M_ISDU_ILLEGAL = 0x5700, IOL_eErrorType_ARGBLOCK_NOT_SUPPORTED = 0x4001, IOL_eErrorType_ARGBLOCK_ID_NOT_SUPPORTED = 0x4002, IOL_eErrorType_DEVICE_NOT_ACCESSIBLE = 0x4003, IOL_eErrorType_SERVICE_NOT_SUPPORTED = 0x4004, IOL_eErrorType_CMD_NOT_SUPPORTED = 0x4005, IOL_eErrorType_PORT_NUM_INVALID = 0x4011, IOL_eErrorType_ARGBLOCK_LENGTH_INVALID = 0x4034, IOL_eErrorType_SERVICE_TEMP_UNAVAILABLE = 0x4036, IOL_eErrorType_PORT_CONFIG_INCONSISTENT = 0x4041 } |
This enumeration indicates the permissible ISDU ErrorTypes resulting from the Device application. More... | |
enum | IOL_EECode { IOL_eECode_NO_MALFUNCTION = 0x0000, IOL_eECode_GENERAL_MALFUNCTION = 0x1000, IOL_eECode_TEMP_FAULT = 0x4000, IOL_eECode_TEMP_OVERRUN = 0x4210, IOL_eECode_TEMP_UNDERRUN = 0x4220, IOL_eECode_HW_FAULT = 0x5000, IOL_eECode_COMP_MALFUNCTION = 0x5010, IOL_eECode_MEM_LOSS = 0x5011, IOL_eECode_BATTERIES_LOW = 0x5012, IOL_eECode_SUPPLY_FAULT = 0x5100, IOL_eECode_FUSE_OPEN = 0x5101, IOL_eECode_SUPPLY_OVERRUN = 0x5110, IOL_eECode_SUPPLY_UNDERRUN = 0x5111, IOL_eECode_SEC_SUPPLY_FAULT = 0x5112, IOL_eECode_SW_FAULT = 0x6000, IOL_eECode_PARAM_ERROR = 0x6320, IOL_eECode_PARAM_MISSING = 0x6321, IOL_eECode_PARAM_CHANGED = 0x6350, IOL_eECode_WIRE_BREAK = 0x7700, IOL_eECode_WIRE_BREAK_D1 = 0x7701, IOL_eECode_WIRE_BREAK_D2 = 0x7702, IOL_eECode_WIRE_BREAK_D3 = 0x7703, IOL_eECode_WIRE_BREAK_D4 = 0x7704, IOL_eECode_WIRE_BREAK_D5 = 0x7705, IOL_eECode_WIRE_BREAK_D6 = 0x7706, IOL_eECode_WIRE_BREAK_D7 = 0x7707, IOL_eECode_WIRE_BREAK_D8 = 0x7708, IOL_eECode_WIRE_BREAK_D9 = 0x7709, IOL_eECode_WIRE_BREAK_D10 = 0x770A, IOL_eECode_WIRE_BREAK_D11 = 0x770B, IOL_eECode_WIRE_BREAK_D12 = 0x770C, IOL_eECode_WIRE_BREAK_D13 = 0x770D, IOL_eECode_WIRE_BREAK_D14 = 0x770E, IOL_eECode_WIRE_BREAK_D15 = 0x770F, IOL_eECode_SHORT_CIRCUIT = 0x7710, IOL_eECode_GROUND_FAULT = 0x7711, IOL_eECode_APP_FAULT = 0x8C00, IOL_eECode_SIM_ACTIVE = 0x8C01, IOL_eECode_PD_OVERRUN = 0x8C10, IOL_eECode_MEASUREMENT_OVERRUN = 0x8C20, IOL_eECode_PD_UNDERRUN = 0x8C30, IOL_eECode_MAINT_CLEANING = 0x8C40, IOL_eECode_MAINT_REFILL = 0x8C41, IOL_eECode_MAINT_EXCHANGE = 0x8C42, IOL_eECode_EVENT = 0xFF31, IOL_eECode_DS_UPLOAD_REQ = 0xFF91, IOL_eECode_IOLW_RETRY_ERROR_R = 0xFFB0 } |
This enumeration lists the specified EventCode identifiers and their definitions. The EventCodes are created by the technology specific Device application (instance = APP). More... | |
enum | IOL_EEPortCode { IOL_eEPortCode_NoDevice = 0x1800, IOL_eEPortCode_StartupParamError = 0x1801, IOL_eEPortCode_IncorrectVendorId = 0x1802, IOL_eEPortCode_IncorrectDeviceId = 0x1803, IOL_eEPortCode_ShortCircuit = 0x1804, IOL_eEPortCode_PhyOvertemperatur = 0x1805, IOL_eEPortCode_ShortCircuitLP = 0x1806, IOL_eEPortCode_OvercurrentAtLp = 0x1807, IOL_eEPortCode_DeviceEventOverflow = 0x1808, IOL_eEPortCode_BackupMemOutOfRange = 0x1809, IOL_eEPortCode_BackupIdentityFault = 0x180A, IOL_eEPortCode_BackupUnspecificError = 0x180B, IOL_eEPortCode_BackupUploadFault = 0x180C, IOL_eEPortCode_BackupDownloadFault = 0x180D, IOL_eEPortCode_P24MissingUndervoltage = 0x180E, IOL_eEPortCode_ShortCircuitP24 = 0x180F, IOL_eEPortCode_ShortCircuitIQ = 0x1810, IOL_eEPortCode_ShortCircuitAtCQ = 0x1811, IOL_eEPortCode_OvercurrentIQ = 0x1812, IOL_eEPortCode_OvercurrentCQ = 0x1813, IOL_eEPortCode_EvalExpired = 0x1F00, IOL_eEPortCode_InvalidCycleTime = 0x6000, IOL_eEPortCode_RevisionFault = 0x6001, IOL_eEPortCode_ISDUBatchFailed = 0x6002, IOL_eEPortCode_NEW_SLAVE = 0xFF21, IOL_eEPortCode_DEV_COM_LOST = 0xFF22, IOL_eEPortCode_DS_IDENT_MISMATCH = 0xFF23, IOL_eEPortCode_DS_BUFFER_OVERFLOW = 0xFF24, IOL_eEPortCode_DS_ACCESS_DENIED = 0xFF25, IOL_eEPortCode_PortStatusChanged = 0xFF26, IOL_eEPortCode_DataStorageComplete = 0xFF27, IOL_eEPortCode_IncorectEventSignalling = 0xFF31, IOL_eEPortCode_IOLW_RETRY_ERROR_L = 0x3000, IOL_eEPortCode_IOLW_IMA_TIMEOUT = 0x3001 } |
This enumeration lists the specified EventCode identifiers and their definitions. The EventCodes are created by the technology specific Device application (instance = APP). More... | |
enum | IOL_EEInstance { IOL_eEInstance_UNKNOWN = 0, IOL_eEInstance_PHY, IOL_eEInstance_DL, IOL_eEInstance_AL, IOL_eEInstance_APPLICATION, IOL_eEInstance_RESERVED_4, IOL_eEInstance_RESERVED_5, IOL_eEInstance_RESERVED_6 } |
This enumeration indicates the particular source (instance) of an event thus refining its evaluation on the receiver side. More... | |
enum | IOL_EESource { IOL_eESource_DEVICE = 0, IOL_eESource_MASTER } |
This enumeration indicates the source of the event. More... | |
enum | IOL_EEType { IOL_eEEType_RESERVED = 0, IOL_eEEType_NOTIFICATION, IOL_eEEType_WARNING, IOL_eEEType_ERROR } |
This enumeration indicates the event category. More... | |
enum | IOL_EEMode { IOL_eEEMode_RESERVED = 0, IOL_eEEMode_SINGLE_SHOT, IOL_eEEMode_DISAPPEARS, IOL_eEEMode_APPEARS } |
This enumeration indicates the event mode. More... | |
enum | IOL_EDSCommand { IOL_eDSCommand_Reserved = 0, IOL_eDSCommand_UploadStart, IOL_eDSCommand_UploadEnd, IOL_eDSCommand_DownloadStart, IOL_eDSCommand_DownloadEnd, IOL_eDSCommand_Break } |
This enumeration indicates the DS commands. | |
enum | IOL_ESystemCommand { IOL_eSystemCommand_Reserved = 0, IOL_eSystemCommand_UploadStart, IOL_eSystemCommand_UploadEnd, IOL_eSystemCommand_DownloadStart, IOL_eSystemCommand_DownloadEnd, IOL_eSystemCommand_DownloadEndStore, IOL_eSystemCommand_Break, IOL_eSystemCommand_DeviceReset = 128, IOL_eSystemCommand_ApplicationReset = 129, IOL_eSystemCommand_RestoreFactorySettings = 130, IOL_eSystemCommand_BackToBox = 131 } |
This enumeration indicates the predefined system commands. | |
enum | IOL_ESlotType { IOL_eSlotType_SSLOT = 0, IOL_eSlotType_DSLOT = 1 } |
Physical layer slot types. | |
enum IOL_EBaudrate |
This enumeration indicates the transmission rate.
Enumerator | |
---|---|
IOL_eBaudrate_AUTO | Master accepts transmission rate found during IOL_eDLRealMode_ESTABCOM "ESTABLISHCOM". |
IOL_eBaudrate_COM1 | Transmission rate of COM1 (4,8 kbit/s). |
IOL_eBaudrate_COM2 | Transmission rate of COM2 (38,4 kbit/s). |
IOL_eBaudrate_COM3 | Transmission rate of COM3 (230,4 kbit/s). |
enum IOL_EDeviceMode |
This enumeration indicates changes of communication states to the Device application.
enum IOL_EDirection |
enum IOL_EDLMode |
This enumeration indicates the requested mode of the Master's DL on an individual port.
enum IOL_EDLRealMode |
This enumeration indicates the status of the DL-mode handler.
enum IOL_EECode |
This enumeration lists the specified EventCode identifiers and their definitions. The EventCodes are created by the technology specific Device application (instance = APP).
enum IOL_EEInstance |
This enumeration indicates the particular source (instance) of an event thus refining its evaluation on the receiver side.
enum IOL_EEMode |
enum IOL_EEPortCode |
This enumeration lists the specified EventCode identifiers and their definitions. The EventCodes are created by the technology specific Device application (instance = APP).
enum IOL_EErrorInfo |
This enumeration contains error information.
enum IOL_EErrorType |
This enumeration indicates the permissible ISDU ErrorTypes resulting from the Device application.
enum IOL_EESource |
enum IOL_EEType |
enum IOL_EIQMode |
enum IOL_EMHInfo |
enum IOL_EMSequence |
This enumeration contains the M-sequence types.
TYPE_1_1 forces interleave mode of process and On-request Data transmission, see 7.3.4.2 of IO-Link Specification v1.1.2.
enum IOL_EPDInStatus |
enum IOL_EPDOutStatus |
This enumeration indicates the qualifier status of the Process Data (PD).
enum IOL_EPortMode |
This enumeration indicates changes or faults of the local communication mode.
enum IOL_ETargetMode |
This enumeration indicates the requested operational mode of the port.
enum IOL_ETransferMode |
This enumeration indicates the requested operation mode.
enum IOL_ETransferStatus |
This enumeration contains supplementary information on the transfer. status.