#include <api/EI_API.h>
EI_API_ADP_T* pEI_API_ADP = NULL;
uint32_t errCode;
uint8_t numInterfaces = 1;
uint8_t macAddr[] = { 0x00, 0x00, 0x00, 0x00, 0x00, 0x00 };
ETHIP_API T * EI_API_ADP_new(uint8_t numInterfaces_p)
Create a new EtherNet/IP adapter.
Definition: EI_API_ADP_main.c:232
ETHIP_API uint32_t EI_API_ADP_setEnipAcdAddr(T *pAdp_p, const EI_API_ADP_SParam_t *pEnipAcdAddr_p)
Set the address conflict detection MAC address (Instance Attribute ID: 11).
Definition: EI_API_ADP_main.c:3189
Definition: EI_API_ADP.h:113