uint32_t EI_API_ADP_getEnipAcdAddr | ( | T * | pAdp_p, |
EI_API_ADP_SParam_t * | pEnipAcdAddr_p | ||
) |
Get the adapter address conflict detection MAC address (Instance Attribute ID: 11).
Function that returns the current Address Conflict Detection (ACD) MAC address inside a structure of type EI_API_ADP_SParam_t
[in] | pAdp_p | Pointer to the adapter. |
[out] | pEnipAcdAddr_p | Pointer to the Ethernet Address Conflict Detection MAC address packed within a EI_API_ADP_SParam_t type. |
EI_API_ADP_eERR_OK | Success. |
EI_API_ADP_eERR_GENERAL | General error. |