EtherCAT Slave  1.04.03

◆ EC_API_SLV_setProductName()

uint32_t EC_API_SLV_setProductName ( EC_API_SLV_SHandle_t pEcSlaveApi_p,
char *  pProductName_p 
)

Set device product name.

Set a product name for the device. Required by the Object Dictionary

Parameters
[in]pEcSlaveApi_pThe pointer to the EtherCAT API instance.
[in]pProductName_pproduct name.
Returns
uint32_t Returns the API error code.
Example
#include <ecSlvApi.h>
// required variables
uint32_t retVal = 0;
EC_API_SLV_SHandle_t* S_ecSlvApiHdl;
// the Call
retVal = EC_API_SLV_setProductName(S_ecSlvApiHdl, "KUNBUS AM3359 EtherCAT");
See also
EC_API_SLV_setVendorId, EC_API_SLV_setProductCode, EC_API_SLV_setRevisionNumber, EC_API_SLV_getProductName
EC_API_SLV_setProductName
uint32_t EC_API_SLV_setProductName(EC_API_SLV_SHandle_t *pEcSlaveApi_p, char *pProductName_p)
Set device product name.
Definition: ecSlvApi_ParamStub.c:276
EC_API_SLV_SHandle_t
struct EC_API_SLV_SHandle EC_API_SLV_SHandle_t
EC_API_SLV_SHandle_t describes the EtherCAT Slave API.
Definition: ecSlvApi.h:134