uint32_t EC_API_SLV_setVendorId | ( | EC_API_SLV_SHandle_t * | pEcSlaveApi_p, |
uint32_t | vendorId_p | ||
) |
Set device vendor ID. Used by the EEPROM and Object Dictionary.
Set a vendor ID. Required for device identification. It is used by the SII interface and the Object Dictionary
[in] | pEcSlaveApi_p | The pointer to the EtherCAT API instance. |
[in] | vendorId_p | vendor identification number. |