MCSPI configuration parameters for the channel.
MCSPI channel parameters used with the MCSPI_chConfig() call. Default values for these parameters are set using MCSPI_ChConfig_init().
If NULL is passed for the parameters, MCSPI_chConfig() uses default parameters.
Data Fields | |
uint32_t | chNum |
uint32_t | frameFormat |
uint32_t | bitRate |
uint32_t | csPolarity |
uint32_t | dataSize |
uint32_t | trMode |
uint32_t | inputSelect |
uint32_t | dpe0 |
uint32_t | dpe1 |
uint32_t | slvCsSelect |
uint32_t | startBitEnable |
uint32_t | startBitPolarity |
uint32_t | csIdleTime |
uint32_t | defaultTxData |
uint32_t MCSPI_ChConfig::chNum |
Channel number. Refer MCSPI_ChannelId
uint32_t MCSPI_ChConfig::frameFormat |
MCSPI frame format. Refer MCSPI_FrameFormat
uint32_t MCSPI_ChConfig::bitRate |
MCSPI bit rate in Hz
uint32_t MCSPI_ChConfig::csPolarity |
Polarity of the chip select signal. Refer MCSPI_CsPolarity
uint32_t MCSPI_ChConfig::dataSize |
MCSPI data frame size in bits - valid values: 4 bits to 32 bits
The dataSize value determines the element types of txBuf and rxBuf. If the dataSize is from 4 to 8 bits, the driver assumes the data buffers are of type uint8_t (unsigned char). If the dataSize is from 8 to 16 bits, the driver assumes the data buffers are of type uint16_t (unsigned short). If the dataSize is greater than 16 bits, the driver assumes the data buffers are uint32_t (unsigned long).
uint32_t MCSPI_ChConfig::trMode |
Channel transmit/receive mode. Refer MCSPI_TrMode
uint32_t MCSPI_ChConfig::inputSelect |
Input Select - D0 or D1. Refer MCSPI_InputSelect
uint32_t MCSPI_ChConfig::dpe0 |
Transmission enable/disable for D0. Refer MCSPI_TxEnable
uint32_t MCSPI_ChConfig::dpe1 |
Transmission enable/disable for D1. Refer MCSPI_TxEnable
uint32_t MCSPI_ChConfig::slvCsSelect |
MCSPI slave select signal detection. Applicable for Channel 0 and in slave mode only. Refer MCSPI_SlvCsSelect
uint32_t MCSPI_ChConfig::startBitEnable |
Start bit D/CX added before SPI transfer. Polarity is defined by start bit level (below)
uint32_t MCSPI_ChConfig::startBitPolarity |
Start-bit polarity used when startBitEnable is TRUE Refer MCSPI_SbPolarity
uint32_t MCSPI_ChConfig::csIdleTime |
Chip select time control. Refer MCSPI_CsIdleTime. This is applicable only in master mode
uint32_t MCSPI_ChConfig::defaultTxData |
Default TX data to use when NULL pointer is provided for TX buffer. The actual data that is transmitted depends on the dataSize field