This module contains APIs to program and use the MCSPI module. The APIs can be used by other drivers to get access to MCSPI and also by application to initiate data transfer operation.
Files | |
file | mcspi/v0/mcspi.h |
MCSPI Driver API/interface file. | |
Data Structures | |
struct | MCSPI_Transaction |
Data structure used with MCSPI_transfer() More... | |
struct | MCSPI_OpenParams |
MCSPI Parameters. More... | |
struct | MCSPI_ChConfig |
MCSPI configuration parameters for the channel. More... | |
struct | MCSPI_Attrs |
MCSPI instance attributes - used during init time. More... | |
struct | MCSPI_ChObject |
MCSPI channel object. More... | |
struct | MCSPI_Object |
MCSPI driver object. More... | |
struct | MCSPI_Config |
MCSPI global configuration array. More... | |
Functions | |
void | MCSPI_init (void) |
This function initializes the MCSPI module. More... | |
void | MCSPI_deinit (void) |
This function de-initializes the MCSPI module. More... | |
MCSPI_Handle | MCSPI_open (uint32_t index, const MCSPI_OpenParams *openPrms) |
This function opens a given MCSPI peripheral. More... | |
void | MCSPI_close (MCSPI_Handle handle) |
Function to close a MCSPI peripheral specified by the MCSPI handle. More... | |
int32_t | MCSPI_chConfig (MCSPI_Handle handle, const MCSPI_ChConfig *chCfg) |
Function to configure a MCSPI channel. More... | |
int32_t | MCSPI_transfer (MCSPI_Handle handle, MCSPI_Transaction *transaction) |
Function to perform MCSPI transactions. More... | |
int32_t | MCSPI_transferCancel (MCSPI_Handle handle) |
Function to cancel MCSPI transactions on channel of a SPI peripheral specified by the MCSPI handle. More... | |
static void | MCSPI_OpenParams_init (MCSPI_OpenParams *openPrms) |
Function to initialize the MCSPI_OpenParams struct to its defaults. More... | |
static void | MCSPI_ChConfig_init (MCSPI_ChConfig *chConfig) |
Function to initialize the MCSPI_ChConfig struct to its defaults. More... | |
uint32_t | MCSPI_getBaseAddr (MCSPI_Handle handle) |
Function to get base address of MCSPI instance of a particular handle. More... | |
int32_t | MCSPI_reConfigFifo (MCSPI_Handle handle, uint32_t chNum, uint32_t numWordsRxTx) |
Function to re-configure Effective FIFO Words. More... | |
static uint32_t | MCSPI_getBufWidthShift (uint32_t dataSize) |
This API will return the buffer width in bytes based on dataSize. More... | |
static uint32_t | MCSPI_readChStatusReg (uint32_t baseAddr, uint32_t chNum) |
This API will return the status of the McSPI channel currently in use. More... | |
static uint32_t | MCSPI_readChCtrlReg (uint32_t baseAddr, uint32_t chNum) |
This API returns Channel control register value. More... | |
static void | MCSPI_writeChCtrlReg (uint32_t baseAddr, uint32_t chNum, uint32_t regVal) |
This API sets Channel control register value. More... | |
static uint32_t | MCSPI_readChConf (uint32_t baseAddr, uint32_t chNum) |
This API returns Channel Config register value. More... | |
static void | MCSPI_writeChConfReg (uint32_t baseAddr, uint32_t chNum, uint32_t regVal) |
This API sets Channel Config register value. More... | |
static void | MCSPI_writeTxDataReg (uint32_t baseAddr, uint32_t txData, uint32_t chNum) |
This API will put the data on to the McSPI Channel transmit register. More... | |
static void | MCSPI_enableTxFIFO (uint32_t baseAddr, uint32_t chNum, uint32_t enableFlag) |
This API will enable/disable the Tx FIFOs of McSPI peripheral. More... | |
static void | MCSPI_enableRxFIFO (uint32_t baseAddr, uint32_t chNum, uint32_t enableFlag) |
This API will enable/disable the Rx FIFOs of McSPI peripheral. More... | |
static uint32_t | MCSPI_readRxDataReg (uint32_t baseAddr, uint32_t chNum) |
This API will return the data present in the MCSPI_RX register. More... | |
Typedefs | |
typedef void * | MCSPI_Handle |
A handle that is returned from a MCSPI_open() call. More... | |
typedef void(* | MCSPI_CallbackFxn) (MCSPI_Handle handle, MCSPI_Transaction *transaction) |
The definition of a callback function used by the SPI driver when used in MCSPI_TRANSFER_MODE_CALLBACK. More... | |
Macros | |
#define | MCSPI_MAX_NUM_CHANNELS (4U) |
Max number of channels/Chip Select (CS) supported. More... | |
#define | MCSPI_FIFO_LENGTH (64U) |
Total length of FIFO for both TX/RX. More... | |
#define | MCSPI_RX_FIFO_ENABLE |
McSPI peripheral Rx FIFO is enabled. More... | |
#define | MCSPI_RX_FIFO_DISABLE |
McSPI peripheral Rx FIFO is disabled. More... | |
#define | MCSPI_TX_FIFO_ENABLE |
McSPI peripheral Tx FIFO is enabled. More... | |
#define | MCSPI_TX_FIFO_DISABLE |
McSPI peripheral Tx FIFO is disabled. More... | |
#define | MCSPI_REG_OFFSET (0x14U) |
McSPI Register Offset for MCSPI_CHxCONF, MCSPI_CHxSTAT, MCSPI_CHxCTRL, MCSPI_TXx and MCSPI_RXx register set. More... | |
#define | MCSPI_CHCONF(x) |
Base address of McSPI_CHCONF(x) More... | |
#define | MCSPI_CHSTAT(x) |
Base address of McSPI_CHSTAT(x) More... | |
#define | MCSPI_CHCTRL(x) |
Base address of McSPI_CHCTRL(x) More... | |
#define | MCSPI_CHTX(x) |
Base address of McSPI_CHTX(x) More... | |
#define | MCSPI_CHRX(x) |
Base address of McSPI_CHRX(x) More... | |
#define | MCSPI_CLKD_MASK (0x0FU) |
#define | MCSPI_IRQSTATUS_CLEAR_ALL |
Bit mask to clear all status bits. More... | |
Channel Id | |
Values used to determine the channel number used for McSPI communication. This determines which Chip Select (CS) line to use | |
#define | MCSPI_CHANNEL_0 (0U) |
#define | MCSPI_CHANNEL_1 (1U) |
#define | MCSPI_CHANNEL_2 (2U) |
#define | MCSPI_CHANNEL_3 (3U) |
Transfer Status Code | |
Status codes that are set by the MCSPI driver | |
#define | MCSPI_TRANSFER_COMPLETED (0U) |
#define | MCSPI_TRANSFER_STARTED (1U) |
#define | MCSPI_TRANSFER_CANCELLED (2U) |
#define | MCSPI_TRANSFER_FAILED (3U) |
#define | MCSPI_TRANSFER_CSN_DEASSERT (4U) |
#define | MCSPI_TRANSFER_TIMEOUT (5U) |
Transfer Mode | |
This determines whether the driver operates synchronously or asynchronously In MCSPI_TRANSFER_MODE_BLOCKING mode MCSPI_transfer() blocks code execution until the transaction has completed In MCSPI_TRANSFER_MODE_CALLBACK MCSPI_transfer() does not block code execution and instead calls a MCSPI_CallbackFxn callback function when the transaction has completed | |
#define | MCSPI_TRANSFER_MODE_BLOCKING (0U) |
MCSPI_transfer() blocks execution. This mode can only be used when called within a Task context More... | |
#define | MCSPI_TRANSFER_MODE_CALLBACK (1U) |
MCSPI_transfer() does not block code execution and will call a MCSPI_CallbackFxn. This mode can be used in a Task, Swi, or Hwi context More... | |
Modes of Operation | |
Definitions for various MCSPI modes of operation The MCSPI driver operates in both master and SPI slave modes. Logically, the implementation is identical, however the difference between these two modes is driven by hardware. The default mode is MCSPI_MS_MODE_MASTER, but can be set to slave mode by setting MCSPI_OpenParams.msMode to MCSPI_MS_MODE_SLAVE in the parameters passed to MCSPI_open(). | |
#define | MCSPI_MS_MODE_MASTER (CSL_MCSPI_MODULCTRL_MS_MASTER) |
The module generates the clock and CS. More... | |
#define | MCSPI_MS_MODE_SLAVE (CSL_MCSPI_MODULCTRL_MS_SLAVE) |
The module receives the clock and CS. More... | |
Frame Format | |
Definitions for various SPI data frame formats POL0 = SPICLK is held low during the INACTIVE state POL1 = SPICLK is held high during the INACTIVE state PHA0 = Data are latched on odd-numbered edges of SPICLK PHA1 = Data are latched on even-numbered edges of SPICLK | |
#define | MCSPI_FF_POL0_PHA0 (0U) |
#define | MCSPI_FF_POL0_PHA1 (1U) |
#define | MCSPI_FF_POL1_PHA0 (2U) |
#define | MCSPI_FF_POL1_PHA1 (3U) |
Chip-select Polarity | |
Type for SPI Chip Select Polarity and Clock Idle Level | |
#define | MCSPI_CS_POL_HIGH (CSL_MCSPI_CH0CONF_EPOL_ACTIVEHIGH) |
SPIEN (CS) is held high during the ACTIVE state. More... | |
#define | MCSPI_CS_POL_LOW (CSL_MCSPI_CH0CONF_EPOL_ACTIVELOW) |
SPIEN (CS) is held low during the ACTIVE state. More... | |
Transmit-Receive Modes | |
#define | MCSPI_TR_MODE_TX_RX (CSL_MCSPI_CH0CONF_TRM_TRANSRECEI) |
#define | MCSPI_TR_MODE_RX_ONLY (CSL_MCSPI_CH0CONF_TRM_RECEIVONLY) |
#define | MCSPI_TR_MODE_TX_ONLY (CSL_MCSPI_CH0CONF_TRM_TRANSONLY) |
Input Select | |
#define | MCSPI_IS_D0 (CSL_MCSPI_CH0CONF_IS_LINE0) |
Data line 0 (SPIDAT[0]) selected for reception. More... | |
#define | MCSPI_IS_D1 (CSL_MCSPI_CH0CONF_IS_LINE1) |
Data line 1 (SPIDAT[1]) selected for reception. More... | |
Transmission Enable for Data Line | |
#define | MCSPI_DPE_ENABLE (CSL_MCSPI_CH0CONF_DPE0_ENABLED) |
Data line selected for transmission. More... | |
#define | MCSPI_DPE_DISABLE (CSL_MCSPI_CH0CONF_DPE0_DISABLED) |
No transmission on Data Line. More... | |
Slave Chip-select Signal Select | |
#define | MCSPI_SLV_CS_SELECT_0 (CSL_MCSPI_CH0CONF_SPIENSLV_SPIEN0) |
#define | MCSPI_SLV_CS_SELECT_1 (CSL_MCSPI_CH0CONF_SPIENSLV_SPIEN1) |
#define | MCSPI_SLV_CS_SELECT_2 (CSL_MCSPI_CH0CONF_SPIENSLV_SPIEN2) |
#define | MCSPI_SLV_CS_SELECT_3 (CSL_MCSPI_CH0CONF_SPIENSLV_SPIEN3) |
Start-bit Polarity | |
#define | MCSPI_SB_POL_HIGH (CSL_MCSPI_CH0CONF_SBPOL_HIGHLEVEL) |
SStart-bit polarity is held to 1 during MCSPI transfer. More... | |
#define | MCSPI_SB_POL_LOW (CSL_MCSPI_CH0CONF_SBPOL_LOWLEVEL) |
Start-bit polarity is held to 0 during MCSPI transfer. More... | |
Chip-select Idle Time | |
Values used to configure the chip select time control (TCS) | |
#define | MCSPI_TCS0_0_CLK (CSL_MCSPI_CH0CONF_TCS0_ZEROCYCLEDLY) |
0.5 clock cycles delay More... | |
#define | MCSPI_TCS0_1_CLK (CSL_MCSPI_CH0CONF_TCS0_ONECYCLEDLY) |
1.5 clock cycles delay More... | |
#define | MCSPI_TCS0_2_CLK (CSL_MCSPI_CH0CONF_TCS0_TWOCYCLEDLY) |
2.5 clock cycles delay More... | |
#define | MCSPI_TCS0_3_CLK (CSL_MCSPI_CH0CONF_TCS0_THREECYCLEDLY) |
3.5 clock cycles delay More... | |
Channel Mode | |
#define | MCSPI_CH_MODE_SINGLE (CSL_MCSPI_MODULCTRL_SINGLE_SINGLE) |
Only one channel will be used in master mode. This should be used when CS is used in forced enable mode. More... | |
#define | MCSPI_CH_MODE_MULTI (CSL_MCSPI_MODULCTRL_SINGLE_MULTI) |
More than one channel will be used in master mode. More... | |
Pin Mode | |
#define | MCSPI_PINMODE_3PIN (CSL_MCSPI_MODULCTRL_PIN34_3PINMODE) |
SPIEN (CS) is not used. In this mode all related options to chip-select have no meaning. More... | |
#define | MCSPI_PINMODE_4PIN (CSL_MCSPI_MODULCTRL_PIN34_4PINMODE) |
Init Delay | |
Values used to enable initial delay for first transfer | |
#define | MCSPI_INITDLY_0 (CSL_MCSPI_MODULCTRL_INITDLY_NODELAY) |
No delay. More... | |
#define | MCSPI_INITDLY_4 (CSL_MCSPI_MODULCTRL_INITDLY_4CLKDLY) |
4 SPI bus clock delays More... | |
#define | MCSPI_INITDLY_8 (CSL_MCSPI_MODULCTRL_INITDLY_8CLKDLY) |
8 SPI bus clock delays More... | |
#define | MCSPI_INITDLY_16 (CSL_MCSPI_MODULCTRL_INITDLY_16CLKDLY) |
16 SPI bus clock delays More... | |
#define | MCSPI_INITDLY_32 (CSL_MCSPI_MODULCTRL_INITDLY_32CLKDLY) |
32 SPI bus clock delays More... | |
#define MCSPI_CHANNEL_0 (0U) |
#define MCSPI_CHANNEL_1 (1U) |
#define MCSPI_CHANNEL_2 (2U) |
#define MCSPI_CHANNEL_3 (3U) |
#define MCSPI_MAX_NUM_CHANNELS (4U) |
Max number of channels/Chip Select (CS) supported.
#define MCSPI_TRANSFER_COMPLETED (0U) |
#define MCSPI_TRANSFER_STARTED (1U) |
#define MCSPI_TRANSFER_CANCELLED (2U) |
#define MCSPI_TRANSFER_FAILED (3U) |
#define MCSPI_TRANSFER_CSN_DEASSERT (4U) |
#define MCSPI_TRANSFER_TIMEOUT (5U) |
#define MCSPI_TRANSFER_MODE_BLOCKING (0U) |
MCSPI_transfer() blocks execution. This mode can only be used when called within a Task context
#define MCSPI_TRANSFER_MODE_CALLBACK (1U) |
MCSPI_transfer() does not block code execution and will call a MCSPI_CallbackFxn. This mode can be used in a Task, Swi, or Hwi context
#define MCSPI_MS_MODE_MASTER (CSL_MCSPI_MODULCTRL_MS_MASTER) |
The module generates the clock and CS.
#define MCSPI_MS_MODE_SLAVE (CSL_MCSPI_MODULCTRL_MS_SLAVE) |
The module receives the clock and CS.
#define MCSPI_FF_POL0_PHA0 (0U) |
#define MCSPI_FF_POL0_PHA1 (1U) |
#define MCSPI_FF_POL1_PHA0 (2U) |
#define MCSPI_FF_POL1_PHA1 (3U) |
#define MCSPI_CS_POL_HIGH (CSL_MCSPI_CH0CONF_EPOL_ACTIVEHIGH) |
SPIEN (CS) is held high during the ACTIVE state.
#define MCSPI_CS_POL_LOW (CSL_MCSPI_CH0CONF_EPOL_ACTIVELOW) |
SPIEN (CS) is held low during the ACTIVE state.
#define MCSPI_TR_MODE_TX_RX (CSL_MCSPI_CH0CONF_TRM_TRANSRECEI) |
#define MCSPI_TR_MODE_RX_ONLY (CSL_MCSPI_CH0CONF_TRM_RECEIVONLY) |
#define MCSPI_TR_MODE_TX_ONLY (CSL_MCSPI_CH0CONF_TRM_TRANSONLY) |
#define MCSPI_IS_D0 (CSL_MCSPI_CH0CONF_IS_LINE0) |
Data line 0 (SPIDAT[0]) selected for reception.
#define MCSPI_IS_D1 (CSL_MCSPI_CH0CONF_IS_LINE1) |
Data line 1 (SPIDAT[1]) selected for reception.
#define MCSPI_DPE_ENABLE (CSL_MCSPI_CH0CONF_DPE0_ENABLED) |
Data line selected for transmission.
#define MCSPI_DPE_DISABLE (CSL_MCSPI_CH0CONF_DPE0_DISABLED) |
No transmission on Data Line.
#define MCSPI_SLV_CS_SELECT_0 (CSL_MCSPI_CH0CONF_SPIENSLV_SPIEN0) |
#define MCSPI_SLV_CS_SELECT_1 (CSL_MCSPI_CH0CONF_SPIENSLV_SPIEN1) |
#define MCSPI_SLV_CS_SELECT_2 (CSL_MCSPI_CH0CONF_SPIENSLV_SPIEN2) |
#define MCSPI_SLV_CS_SELECT_3 (CSL_MCSPI_CH0CONF_SPIENSLV_SPIEN3) |
#define MCSPI_SB_POL_HIGH (CSL_MCSPI_CH0CONF_SBPOL_HIGHLEVEL) |
SStart-bit polarity is held to 1 during MCSPI transfer.
#define MCSPI_SB_POL_LOW (CSL_MCSPI_CH0CONF_SBPOL_LOWLEVEL) |
Start-bit polarity is held to 0 during MCSPI transfer.
#define MCSPI_TCS0_0_CLK (CSL_MCSPI_CH0CONF_TCS0_ZEROCYCLEDLY) |
0.5 clock cycles delay
#define MCSPI_TCS0_1_CLK (CSL_MCSPI_CH0CONF_TCS0_ONECYCLEDLY) |
1.5 clock cycles delay
#define MCSPI_TCS0_2_CLK (CSL_MCSPI_CH0CONF_TCS0_TWOCYCLEDLY) |
2.5 clock cycles delay
#define MCSPI_TCS0_3_CLK (CSL_MCSPI_CH0CONF_TCS0_THREECYCLEDLY) |
3.5 clock cycles delay
#define MCSPI_CH_MODE_SINGLE (CSL_MCSPI_MODULCTRL_SINGLE_SINGLE) |
Only one channel will be used in master mode. This should be used when CS is used in forced enable mode.
#define MCSPI_CH_MODE_MULTI (CSL_MCSPI_MODULCTRL_SINGLE_MULTI) |
More than one channel will be used in master mode.
#define MCSPI_PINMODE_3PIN (CSL_MCSPI_MODULCTRL_PIN34_3PINMODE) |
SPIEN (CS) is not used. In this mode all related options to chip-select have no meaning.
#define MCSPI_PINMODE_4PIN (CSL_MCSPI_MODULCTRL_PIN34_4PINMODE) |
#define MCSPI_INITDLY_0 (CSL_MCSPI_MODULCTRL_INITDLY_NODELAY) |
No delay.
#define MCSPI_INITDLY_4 (CSL_MCSPI_MODULCTRL_INITDLY_4CLKDLY) |
4 SPI bus clock delays
#define MCSPI_INITDLY_8 (CSL_MCSPI_MODULCTRL_INITDLY_8CLKDLY) |
8 SPI bus clock delays
#define MCSPI_INITDLY_16 (CSL_MCSPI_MODULCTRL_INITDLY_16CLKDLY) |
16 SPI bus clock delays
#define MCSPI_INITDLY_32 (CSL_MCSPI_MODULCTRL_INITDLY_32CLKDLY) |
32 SPI bus clock delays
#define MCSPI_FIFO_LENGTH (64U) |
Total length of FIFO for both TX/RX.
#define MCSPI_RX_FIFO_ENABLE |
McSPI peripheral Rx FIFO is enabled.
#define MCSPI_RX_FIFO_DISABLE |
McSPI peripheral Rx FIFO is disabled.
#define MCSPI_TX_FIFO_ENABLE |
McSPI peripheral Tx FIFO is enabled.
#define MCSPI_TX_FIFO_DISABLE |
McSPI peripheral Tx FIFO is disabled.
#define MCSPI_REG_OFFSET (0x14U) |
McSPI Register Offset for MCSPI_CHxCONF, MCSPI_CHxSTAT, MCSPI_CHxCTRL, MCSPI_TXx and MCSPI_RXx register set.
#define MCSPI_CHCONF | ( | x | ) |
Base address of McSPI_CHCONF(x)
#define MCSPI_CHSTAT | ( | x | ) |
Base address of McSPI_CHSTAT(x)
#define MCSPI_CHCTRL | ( | x | ) |
Base address of McSPI_CHCTRL(x)
#define MCSPI_CHTX | ( | x | ) |
Base address of McSPI_CHTX(x)
#define MCSPI_CHRX | ( | x | ) |
Base address of McSPI_CHRX(x)
#define MCSPI_CLKD_MASK (0x0FU) |
#define MCSPI_IRQSTATUS_CLEAR_ALL |
Bit mask to clear all status bits.
typedef void* MCSPI_Handle |
A handle that is returned from a MCSPI_open() call.
typedef void(* MCSPI_CallbackFxn) (MCSPI_Handle handle, MCSPI_Transaction *transaction) |
The definition of a callback function used by the SPI driver when used in MCSPI_TRANSFER_MODE_CALLBACK.
MCSPI_Handle | MCSPI_Handle |
MCSPI_Transaction* | Pointer to a MCSPI_Transaction |
void MCSPI_init | ( | void | ) |
This function initializes the MCSPI module.
void MCSPI_deinit | ( | void | ) |
This function de-initializes the MCSPI module.
MCSPI_Handle MCSPI_open | ( | uint32_t | index, |
const MCSPI_OpenParams * | openPrms | ||
) |
This function opens a given MCSPI peripheral.
index | Index of config to use in the MCSPI_Config array |
openPrms | Pointer to open parameters. If NULL is passed, then default values will be used |
void MCSPI_close | ( | MCSPI_Handle | handle | ) |
Function to close a MCSPI peripheral specified by the MCSPI handle.
handle | MCSPI_Handle returned from MCSPI_open() |
int32_t MCSPI_chConfig | ( | MCSPI_Handle | handle, |
const MCSPI_ChConfig * | chCfg | ||
) |
Function to configure a MCSPI channel.
handle | MCSPI_Handle returned from MCSPI_open() |
chCfg | Pointer to MCSPI_ChConfig. This parameter can't be NULL |
int32_t MCSPI_transfer | ( | MCSPI_Handle | handle, |
MCSPI_Transaction * | transaction | ||
) |
Function to perform MCSPI transactions.
If the MCSPI is in MCSPI_MS_MODE_MASTER mode, it will immediately start the transaction. If the MCSPI is in MCSPI_MS_MODE_SLAVE mode, it prepares the driver for a transaction with a MCSPI master device. The device will then wait until the master begins the transfer.
In MCSPI_TRANSFER_MODE_BLOCKING, MCSPI_transfer() will block task execution until the transaction has completed or a timeout has occurred.
In MCSPI_TRANSFER_MODE_CALLBACK, MCSPI_transfer() does not block task execution, but calls a MCSPI_CallbackFxn once the transfer has finished. This makes MCSPI_transfer() safe to be used within a Task, software or hardware interrupt context.
From calling MCSPI_transfer() until transfer completion, the MCSPI_Transaction structure must stay persistent and must not be altered by application code. It is also forbidden to modify the content of the MCSPI_Transaction.txBuf during a transaction, even though the physical transfer might not have started yet. Doing this can result in data corruption. This is especially important for slave operations where MCSPI_transfer() might be called a long time before the actual data transfer begins.
handle | MCSPI_Handle returned from MCSPI_open() |
transaction | Pointer to a MCSPI_Transaction. All of the fields within transaction except MCSPI_Transaction.count and MCSPI_Transaction.status are WO (write-only) unless otherwise noted in the driver implementations. If a transaction timeout has occurred, MCSPI_Transaction.count will contain the number of frames that were transferred. Neither is it allowed to modify the transaction object nor the content of MCSPI_Transaction.txBuf until the transfer has completed |
int32_t MCSPI_transferCancel | ( | MCSPI_Handle | handle | ) |
Function to cancel MCSPI transactions on channel of a SPI peripheral specified by the MCSPI handle.
In MCSPI_TRANSFER_MODE_BLOCKING, MCSPI_transferCancel has no effect.
In MCSPI_TRANSFER_MODE_CALLBACK, MCSPI_transferCancel() will stop an MCSPI transfer if if one is in progress. If a transaction was in progress, its callback function will be called in context from which this API is called from. The MCSPI_CallbackFxn function can determine if the transaction was successful or not by reading the MCSPI_TransferStatus status value in the MCSPI_Transaction structure.
handle | MCSPI_Handle returned from MCSPI_open() |
|
inlinestatic |
Function to initialize the MCSPI_OpenParams struct to its defaults.
openPrms | Pointer to MCSPI_OpenParams structure for initialization |
|
inlinestatic |
Function to initialize the MCSPI_ChConfig struct to its defaults.
chConfig | Pointer to MCSPI_ChConfig structure for initialization |
uint32_t MCSPI_getBaseAddr | ( | MCSPI_Handle | handle | ) |
Function to get base address of MCSPI instance of a particular handle.
handle | MCSPI_Handle returned from MCSPI_open() |
int32_t MCSPI_reConfigFifo | ( | MCSPI_Handle | handle, |
uint32_t | chNum, | ||
uint32_t | numWordsRxTx | ||
) |
Function to re-configure Effective FIFO Words.
handle | MCSPI_Handle returned from MCSPI_open() |
chNum | Channel used for communication. |
numWordsRxTx | Number of words to transfer |
|
inlinestatic |
This API will return the buffer width in bytes based on dataSize.
dataSize | MCSPI data frame size in bits - valid values: 4 bits to 32 bits |
|
inlinestatic |
This API will return the status of the McSPI channel currently in use.
baseAddr | Memory Address of the McSPI instance used. |
chNum | Channel used for communication.'chNum' can take the following values.\n MCSPI_CHANNEL_n - Channel n is used for communication.\n |
|
inlinestatic |
This API returns Channel control register value.
baseAddr | Memory Address of the McSPI instance used. |
chNum | Channel number of the McSPI instance used. |
|
inlinestatic |
This API sets Channel control register value.
baseAddr | Memory Address of the McSPI instance used. |
chNum | Channel number of the McSPI instance used. |
regVal | register value to set in channel control register. |
|
inlinestatic |
This API returns Channel Config register value.
baseAddr | Memory Address of the McSPI instance used. |
chNum | Channel number of the McSPI instance used. |
|
inlinestatic |
This API sets Channel Config register value.
baseAddr | Memory Address of the McSPI instance used. |
chNum | Channel number of the McSPI instance used. |
regVal | register value to set in channel Config register. |
|
inlinestatic |
This API will put the data on to the McSPI Channel transmit register.
baseAddr | Memory Address of the McSPI instance used. |
txData | 32 bit data sent by the user which is put on to the MCSPI_TX register. |
chNum | Channel number of the McSPI instance used.'chNum' can take the following values.\n MCSPI_CHANNEL_n - Channel n is used for communication.\n For chNum n can range from 0-3.\n |
|
inlinestatic |
This API will enable/disable the Tx FIFOs of McSPI peripheral.
baseAddr | Memory Address of the McSPI instance used. |
chNum | Channel number of the McSPI instance used. |
enableFlag | Flag to enable/diable FIFO transmit mode. 'enableFlag' can take the following values.\n MCSPI_TX_FIFO_ENABLE - Enables the receiver FIFO of McSPI.\n MCSPI_TX_FIFO_DISABLE - Disables the receiver FIFO of McSPI.\n 'chNum' can take the following values.\n MCSPI_CHANNEL_n - Channel n is used for communication.\n For chNum n can range from 0-3.\n |
|
inlinestatic |
This API will enable/disable the Rx FIFOs of McSPI peripheral.
baseAddr | Memory Address of the McSPI instance used. |
chNum | Channel number of the McSPI instance used. |
enableFlag | Flag to enable/diable FIFO receive mode. 'enableFlag' can take the following values.\n MCSPI_RX_FIFO_ENABLE - Enables the receiver FIFO of McSPI.\n MCSPI_RX_FIFO_DISABLE - Disables the receiver FIFO of McSPI.\n 'chNum' can take the following values.\n MCSPI_CHANNEL_n - Channel n is used for communication.\n For chNum n can range from 0-3.\n |
|
inlinestatic |
This API will return the data present in the MCSPI_RX register.
baseAddr | Memory Address of the McSPI instance used. |
chNum | Channel number of the McSPI instance used. 'chNum' can take the following values.\n MCSPI_CHANNEL_n - Channel n is used for communication.\n For chNum n can range from 0-3.\n |
|
extern |
Externally defined driver configuration array.
|
extern |
Externally defined driver configuration array size.