MMCSD Driver API/interface file.
Go to the source code of this file.
Data Structures | |
struct | MMCSD_Params |
MMCSD instance attributes - used during init time. More... | |
struct | MMCSD_Transaction |
MMCSD transaction. More... | |
struct | MMCSD_Attrs |
MMCSD instance attributes - used during init time. More... | |
struct | MMCSD_Object |
MMCSD driver object. More... | |
struct | MMCSD_Config |
Typedefs | |
typedef void * | MMCSD_Handle |
Functions | |
void | MMCSD_init (void) |
This function initializes the MMCSD module. More... | |
void | MMCSD_deinit (void) |
This function de-initializes the MMCSD module. More... | |
void | MMCSD_Params_init (MMCSD_Params *mmcsdParams) |
Initialize data structure with defaults. More... | |
MMCSD_Handle | MMCSD_open (uint32_t index, const MMCSD_Params *openParams) |
This function opens a given MMCSD peripheral. More... | |
void | MMCSD_close (MMCSD_Handle handle) |
Function to close a MMCSD peripheral specified by the MMCSD handle. More... | |
MMCSD_Handle | MMCSD_getHandle (uint32_t index) |
This function returns the handle of an open MMCSD Instance from the instance index. More... | |
int32_t | MMCSD_read (MMCSD_Handle handle, uint8_t *buf, uint32_t startBlk, uint32_t numBlks) |
Function to perform block reads from the MMC/SD media. More... | |
int32_t | MMCSD_write (MMCSD_Handle handle, uint8_t *buf, uint32_t startBlk, uint32_t numBlks) |
Function to perform block writes to the MMC/SD media. More... | |
int32_t | MMCSD_ioctl (MMCSD_Handle handle, uint32_t cmd, void *arg) |
Function performs implementation specific features on a given MMCSD_Handle. More... | |
uint32_t | MMCSD_getBlockSize (MMCSD_Handle handle) |
This function returns the block size of the MMC/SD media connected to the MMCSD controller. More... | |
Variables | |
MMCSD_Config | gMmcsdConfig [] |
Externally defined driver configuration array. More... | |
uint32_t | gMmcsdConfigNum |
Externally defined driver configuration array size. More... | |