Go to the source code of this file.
Data Structures | |
struct | LED_Params |
Parameters passed during LED_open() More... | |
struct | LED_Fxns |
Driver implementation callbacks. More... | |
struct | LED_Attrs |
LED device attributes, these are filled by SysCfg based on the device that is selected. More... | |
struct | LED_Config |
LED driver configuration, these are filled by SysCfg based on the device that is selected. More... | |
struct | LED_Object |
LED driver object - not to be used by application. More... | |
Typedefs | |
typedef void * | LED_Handle |
Handle to the LED driver returned by LED_open() More... | |
typedef struct LED_Config_s | LED_Config |
Forward declaration of LED_Config. More... | |
typedef struct LED_Params_s | LED_Params |
Forward declaration of LED_Params. More... | |
LED driver implementation callbacks | |
typedef int32_t(* | LED_OpenFxn) (LED_Config *config, const LED_Params *params) |
Driver implementation to open a specific LED driver. More... | |
typedef void(* | LED_CloseFxn) (LED_Config *config) |
Driver implementation to close a specific LED driver. More... | |
typedef int32_t(* | LED_OnFxn) (LED_Config *config, uint32_t index) |
Driver implementation to power on an LED using a specific LED driver. More... | |
typedef int32_t(* | LED_OffFxn) (LED_Config *config, uint32_t index) |
Driver implementation to power off an LED using a specific LED driver. More... | |
typedef int32_t(* | LED_SetMaskFxn) (LED_Config *config, uint32_t mask) |
Driver implementation to set group mask using a specific LED driver. More... | |
Functions | |
void | LED_Params_init (LED_Params *params) |
Set default parameters in the LED_Params structure. More... | |
LED_Handle | LED_open (uint32_t instanceId, const LED_Params *params) |
Open LED driver. More... | |
void | LED_close (LED_Handle handle) |
Open LED driver. More... | |
int32_t | LED_on (LED_Handle handle, uint32_t index) |
API to power on the LED. More... | |
int32_t | LED_off (LED_Handle handle, uint32_t index) |
API to power off the LED. More... | |
int32_t | LED_setMask (LED_Handle handle, uint32_t mask) |
API to set the group mask incase of I2C controlled LED having more than one LED connected to the controller. More... | |
const LED_Attrs * | LED_getAttrs (uint32_t instanceId) |
Return LED attributes. More... | |