This module contains APIs to program and use I2C or GPIO based LED module on the board.
See LED for more details.
◆ LED_Handle
◆ LED_Config
◆ LED_Params
◆ LED_OpenFxn
Driver implementation to open a specific LED driver.
Typically this callback is hidden from the end application and is implemented when a new type of LED device needs to be implemented.
- Parameters
-
config | [IN] LED configuration for the specific LED device |
params | [IN] User controllable parameters when opening the LED device |
- Returns
- SystemP_SUCCESS on success, else failure
◆ LED_CloseFxn
Driver implementation to close a specific LED driver.
Typically this callback is hidden from the end application and is implemented when a new type of LED device needs to be implemented.
- Parameters
-
config | [IN] LED configuration for the specific LED device |
- Returns
- SystemP_SUCCESS on success, else failure
◆ LED_OnFxn
Driver implementation to power on an LED using a specific LED driver.
Typically this callback is hidden from the end application and is implemented when a new type of LED device needs to be implemented.
- Parameters
-
config | [IN] LED configuration for the specific LED device |
index | [IN] Index to the LED group which needs to be turned on |
- Returns
- SystemP_SUCCESS on success, else failure
◆ LED_OffFxn
Driver implementation to power off an LED using a specific LED driver.
Typically this callback is hidden from the end application and is implemented when a new type of LED device needs to be implemented.
- Parameters
-
config | [IN] LED configuration for the specific LED device |
index | [IN] Index to the LED group which needs to be turned off |
- Returns
- SystemP_SUCCESS on success, else failure
◆ LED_SetMaskFxn
typedef int32_t(* LED_SetMaskFxn) (LED_Config *config, uint32_t mask) |
Driver implementation to set group mask using a specific LED driver.
Typically this callback is hidden from the end application and is implemented when a new type of LED device needs to be implemented.
- Parameters
-
config | [IN] LED configuration for the specific LED device |
mask | [IN] Bit Mask to set at one go |
- Returns
- SystemP_SUCCESS on success, else failure
◆ LED_Params_init()
Set default parameters in the LED_Params structure.
Call this API to set defaults and then override the fields as needed before calling LED_open.
- Parameters
-
params | [OUT] Initialized parameters |
◆ LED_open()
Open LED driver.
Make sure the SOC peripheral driver is open'ed before calling this API. Drivers_open function generated by SysCfg opens the underlying SOC peripheral driver, e.g I2C.
Global variables LED_Config gLedConfig[]
and uint32_t gLedConfigNum
is instantiated by SysCfg to describe the LED configuration based on user selection in SysCfg.
- Parameters
-
instanceId | [IN] Index within LED_Config gLedConfig[] denoting the LED driver to open |
params | [IN] Open parameters |
- Returns
- Handle to LED driver which should be used in subsequent API call Else returns NULL in case of failure
◆ LED_close()
Open LED driver.
- Parameters
-
handle | [IN] LED driver handle from LED_open |
◆ LED_on()
int32_t LED_on |
( |
LED_Handle |
handle, |
|
|
uint32_t |
index |
|
) |
| |
API to power on the LED.
- Parameters
-
handle | [IN] LED driver handle from LED_open |
index | [IN] Index to the LED group which needs to be turned on. In case of GPIO controlled LED, set this to 0. |
- Returns
- SystemP_SUCCESS on success, else failure
◆ LED_off()
int32_t LED_off |
( |
LED_Handle |
handle, |
|
|
uint32_t |
index |
|
) |
| |
API to power off the LED.
- Parameters
-
handle | [IN] LED driver handle from LED_open |
index | [IN] Index to the LED group which needs to be turned off. In case of GPIO controlled LED, set this to 0. |
- Returns
- SystemP_SUCCESS on success, else failure
◆ LED_setMask()
int32_t LED_setMask |
( |
LED_Handle |
handle, |
|
|
uint32_t |
mask |
|
) |
| |
API to set the group mask incase of I2C controlled LED having more than one LED connected to the controller.
- Parameters
-
handle | [IN] LED driver handle from LED_open |
mask | [IN] Bit Mask to set at one go. Only bits upto the number of LED present in a group will be used by this function. Set bit to 0 for OFF. Set bit to 1 for ON. |
- Returns
- SystemP_SUCCESS on success, else failure
◆ LED_getAttrs()
const LED_Attrs* LED_getAttrs |
( |
uint32_t |
instanceId | ) |
|
Return LED attributes.
- Parameters
-
instanceId | [IN] LED instance ID |
- Returns
- LED_Attrs, else NULL if instanceId is invalid