![]() |
0.01.00
|
This file includes the OpenThread API for TMF Proxy feature. More...
#include <openthread/types.h>Go to the source code of this file.
Typedefs | |
| typedef void(* | otTmfProxyStreamHandler) (otMessage *aMessage, uint16_t aLocator, uint16_t aPort, void *aContext) |
| This function pointer is called when a TMF packet for host is received. More... | |
Functions | |
| otError | otTmfProxyStart (otInstance *aInstance, otTmfProxyStreamHandler aHandler, void *aContext) |
| Start the TMF proxy. More... | |
| otError | otTmfProxyStop (otInstance *aInstance) |
| Stop the TMF proxy. More... | |
| otError | otTmfProxySend (otInstance *aInstance, otMessage *aMessage, uint16_t aLocator, uint16_t aPort) |
| Send packet through TMF proxy. More... | |
| bool | otTmfProxyIsEnabled (otInstance *aInstance) |
| Get the TMF proxy status (enabled/disabled) More... | |
This file includes the OpenThread API for TMF Proxy feature.