![]() |
0.01.00
|
This is the complete list of members for ot::ThreadExtMacAddressTlv, including all inherited members.
| Get(const Message &aMessage, uint8_t aType, uint16_t aMaxLength, Tlv &aTlv) | ot::Tlv | static |
| GetLength(void) const | ot::Tlv | inline |
| GetMacAddr(void) const | ot::ThreadExtMacAddressTlv | inline |
| GetNext(void) | ot::Tlv | inline |
| GetNext(void) const | ot::Tlv | inline |
| GetOffset(const Message &aMessage, uint8_t aType, uint16_t &aOffset) | ot::Tlv | static |
| GetSize(void) const | ot::Tlv | inline |
| GetTlv(const Message &aMessage, Type aType, uint16_t aMaxLength, Tlv &aTlv) | ot::ThreadTlv | inlinestatic |
| GetType(void) const | ot::ThreadTlv | inline |
| GetValue(void) | ot::Tlv | inline |
| GetValue(void) const | ot::Tlv | inline |
| GetValueOffset(const Message &aMesasge, uint8_t aType, uint16_t &aOffset, uint16_t &aLength) | ot::Tlv | static |
| Init(void) | ot::ThreadExtMacAddressTlv | inline |
| IsValid(void) const | ot::ThreadExtMacAddressTlv | inline |
| kExtendedLength enum value | ot::Tlv | protected |
| kExtMacAddress enum value | ot::ThreadTlv | |
| kLastTransactionTime enum value | ot::ThreadTlv | |
| kMeshLocalEid enum value | ot::ThreadTlv | |
| kNDData enum value | ot::ThreadTlv | |
| kNDOption enum value | ot::ThreadTlv | |
| kRloc16 enum value | ot::ThreadTlv | |
| kRouterMask enum value | ot::ThreadTlv | |
| kStatus enum value | ot::ThreadTlv | |
| kTarget enum value | ot::ThreadTlv | |
| kThreadNetworkData enum value | ot::ThreadTlv | |
| SetLength(uint8_t aLength) | ot::Tlv | inline |
| SetMacAddr(const Mac::ExtAddress &aAddress) | ot::ThreadExtMacAddressTlv | inline |
| SetType(Type aType) | ot::ThreadTlv | inline |
| ot::Tlv::SetType(uint8_t aType) | ot::Tlv | inline |
| Tlv(void) | ot::Tlv | inline |
| Type enum name | ot::ThreadTlv |