This module includes functions that control the Thread stack's execution.
More...
This module includes functions that control the Thread stack's execution.
§ otNcpDelegateAllowPeekPoke
| typedef bool(* otNcpDelegateAllowPeekPoke) (uint32_t aAddress, uint16_t aCount) |
Defines delegate (function pointer) type to control behavior of peek/poke operation.
This delegate function is called to decide whether to allow peek or poke of a specific memory region. It is used if NCP support for peek/poke commands is enabled.
- Parameters
-
| [in] | aAddress | Start address of memory region. |
| [in] | aCount | Number of bytes to peek or poke. |
- Returns
- TRUE to allow peek/poke of the given memory region, FALSE otherwise.
§ otNcpHandlerJoinLegacyNode
| typedef void(* otNcpHandlerJoinLegacyNode) (const otExtAddress *aExtAddress) |
Defines handler (function pointer) type for initiating joining process.
- Parameters
-
| [in] | aExtAddress | A pointer to the extended address for the node to join or NULL if desired to join any neighboring node. |
Invoked to initiate a legacy join procedure to any or a specific node.
§ otNcpHandlerSetLegacyUlaPrefix
| typedef void(* otNcpHandlerSetLegacyUlaPrefix) (const uint8_t *aUlaPrefix) |
Defines handler (function pointer) type for setting the legacy ULA prefix.
- Parameters
-
| [in] | aUlaPrefix | A pointer to buffer containing the legacy ULA prefix. |
Invoked to set the legacy ULA prefix.
§ otNcpHandlerStartLegacy
| typedef void(* otNcpHandlerStartLegacy) (void) |
Defines handler (function pointer) type for starting legacy network.
Invoked to start the legacy network.
§ otNcpHandlerStopLegacy
| typedef void(* otNcpHandlerStopLegacy) (void) |
Defines handler (function pointer) type for stopping legacy network.
Invoked to stop the legacy network.
§ otNcpHandleDidReceiveNewLegacyUlaPrefix()
| void otNcpHandleDidReceiveNewLegacyUlaPrefix |
( |
const uint8_t * |
aUlaPrefix | ) |
|
This callback is invoked by the legacy stack to notify that the legacy ULA prefix has changed.
param[in] aUlaPrefix A pointer to the received ULA prefix.
§ otNcpHandleLegacyNodeDidJoin()
| void otNcpHandleLegacyNodeDidJoin |
( |
const otExtAddress * |
aExtAddr | ) |
|
This callback is invoked by the legacy stack to notify that a new legacy node did join the network.
- Parameters
-
| [in] | aExtAddr | A pointer to the extended address of the joined node. |
§ otNcpInit()
Initialize the NCP.
- Parameters
-
| [in] | aInstance | The OpenThread instance structure. |
§ otNcpPlatLogv()
Callback to write the OpenThread Log to the NCP Spinel Tunnel.
- Parameters
-
| [in] | aLogLevel | The log level. |
| [in] | aLogRegion | The log region. |
| [in] | aFormat | A pointer to the format string. |
| [in] | ap | va_list matching aFormat. |
§ otNcpRegisterLegacyHandlers()
This method registers a set of legacy handlers with NCP.
The set of handlers provided by the struct aHandlers are used by NCP code to start/stop legacy network. The aHandlers can be NULL to disable legacy support on NCP. Individual handlers in the given handlers struct can also be NULL.
- Parameters
-
| [in] | aHandlers | A pointer to a handler struct. |
§ otNcpRegisterPeekPokeDelagates()
This method registers peek/poke delegate functions with NCP module.
The delegate functions are called by NCP module to decide whether to allow peek or poke of a specific memory region. If the delegate pointer is set to NULL, it allows peek/poke operation for any address.
- Parameters
-
| [in] | aAllowPeekDelegate | Delegate function pointer for peek operation. |
| [in] | aAllowPokeDelegate | Delegate function pointer for poke operation. |
- Return values
-
| OT_ERROR_NONE | Successfully registered delegate functions. |
| OT_ERROR_DISABLED_FEATURE | Peek/Poke feature is disabled (by a build-time configuration option). |
§ otNcpStreamWrite()
| otError otNcpStreamWrite |
( |
int |
aStreamId, |
|
|
const uint8_t * |
aDataPtr, |
|
|
int |
aDataLen |
|
) |
| |
Send data to the host via a specific stream.
This function attempts to send the given data to the host using the given aStreamId. This is useful for reporting error messages, implementing debug/diagnostic consoles, and potentially other types of datastreams.
The write either is accepted in its entirety or rejected. Partial writes are not attempted.
- Parameters
-
| [in] | aStreamId | A numeric identifier for the stream to write to. If set to '0', will default to the debug stream. |
| [in] | aDataPtr | A pointer to the data to send on the stream. If aDataLen is non-zero, this param MUST NOT be NULL. |
| [in] | aDataLen | The number of bytes of data from aDataPtr to send. |
- Return values
-
| OT_ERROR_NONE | The data was queued for delivery to the host. |
| OT_ERROR_BUSY | There are not enough resources to complete this request. This is usually a temporary condition. |
| OT_ERROR_INVALID_ARGS | The given aStreamId was invalid. |