![]() |
0.01.00
|
This file defines the top-level functions for the OpenThread library. More...
#include <openthread/crypto.h>#include <openthread/dataset.h>#include <openthread/instance.h>#include <openthread/ip6.h>#include <openthread/link.h>#include <openthread/message.h>#include <openthread/netdata.h>#include <openthread/tasklet.h>#include <openthread/thread.h>#include <openthread/types.h>Go to the source code of this file.
Functions | |
| OTAPI const char *OTCALL | otGetVersionString (void) |
| Get the OpenThread version string. More... | |
| OTAPI const char *OTCALL | otThreadErrorToString (otError aError) |
| This function converts an otError enum into a string. More... | |
This file defines the top-level functions for the OpenThread library.
Get the OpenThread version string.
PLATFORM_VERSION_ATTR_PREFIX and PLATFORM_VERSION_ATTR_SUFFIX are intended to be used to specify compiler directives to indicate what linker section the platform version string should be stored.
This is useful for specifying an exact locaiton of where the version string will be located so that it can be easily retrieved from the raw firmware image.
If PLATFORM_VERSION_ATTR_PREFIX is unspecified, the keyword static is used instead.
If both are unspecified, the location of the string in the firmware image will be undefined and may change.