0.01.00
crypto.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2016, The OpenThread Authors.
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions are met:
7  * 1. Redistributions of source code must retain the above copyright
8  * notice, this list of conditions and the following disclaimer.
9  * 2. Redistributions in binary form must reproduce the above copyright
10  * notice, this list of conditions and the following disclaimer in the
11  * documentation and/or other materials provided with the distribution.
12  * 3. Neither the name of the copyright holder nor the
13  * names of its contributors may be used to endorse or promote products
14  * derived from this software without specific prior written permission.
15  *
16  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
17  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE
18  * IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE
19  * ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT HOLDER OR CONTRIBUTORS BE
20  * LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR
21  * CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF
22  * SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS
23  * INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN
24  * CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE)
25  * ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE
26  * POSSIBILITY OF SUCH DAMAGE.
27  */
28 
35 #ifndef OPENTHREAD_CRYPTO_H_
36 #define OPENTHREAD_CRYPTO_H_
37 
38 #include <stdbool.h>
39 #include <stdint.h>
40 
41 #ifdef __cplusplus
42 extern "C" {
43 #endif
44 
55 #define OT_CRYPTO_HMAC_SHA_HASH_SIZE 32
56 
57 
68  const uint8_t *aKey, uint16_t aKeyLength,
69  const uint8_t *aBuf, uint16_t aBufLength,
70  uint8_t *aHash);
71 
92 void otCryptoAesCcm(
93  const uint8_t *aKey, uint16_t aKeyLength,
94  uint8_t aTagLength,
95  const void *aNonce, uint8_t aNonceLength,
96  const void *aHeader, uint32_t aHeaderLength,
97  void *aPlainText, void *aCipherText, uint32_t aLength, bool aEncrypt,
98  void *aTag);
99 
105 #ifdef __cplusplus
106 } // extern "C"
107 #endif
108 
109 #endif // OPENTHREAD_CRYPTO_H_
void otCryptoAesCcm(const uint8_t *aKey, uint16_t aKeyLength, uint8_t aTagLength, const void *aNonce, uint8_t aNonceLength, const void *aHeader, uint32_t aHeaderLength, void *aPlainText, void *aCipherText, uint32_t aLength, bool aEncrypt, void *aTag)
This method performs AES CCM computation.
Definition: crypto_api.cpp:58
void otCryptoHmacSha256(const uint8_t *aKey, uint16_t aKeyLength, const uint8_t *aBuf, uint16_t aBufLength, uint8_t *aHash)
This function performs HMAC computation.
Definition: crypto_api.cpp:44