This module includes cryptographic functions.
More...
|
| void | otCryptoHmacSha256 (const uint8_t *aKey, uint16_t aKeyLength, const uint8_t *aBuf, uint16_t aBufLength, uint8_t *aHash) |
| | This function performs HMAC computation. More...
|
| |
| void | otCryptoAesCcm (const uint8_t *aKey, uint16_t aKeyLength, uint8_t aTagLength, const void *aNonce, uint8_t aNonceLength, const void *aHeader, uint32_t aHeaderLength, void *aPlainText, void *aCipherText, uint32_t aLength, bool aEncrypt, void *aTag) |
| | This method performs AES CCM computation. More...
|
| |
This module includes cryptographic functions.
§ otCryptoAesCcm()
| void otCryptoAesCcm |
( |
const uint8_t * |
aKey, |
|
|
uint16_t |
aKeyLength, |
|
|
uint8_t |
aTagLength, |
|
|
const void * |
aNonce, |
|
|
uint8_t |
aNonceLength, |
|
|
const void * |
aHeader, |
|
|
uint32_t |
aHeaderLength, |
|
|
void * |
aPlainText, |
|
|
void * |
aCipherText, |
|
|
uint32_t |
aLength, |
|
|
bool |
aEncrypt, |
|
|
void * |
aTag |
|
) |
| |
This method performs AES CCM computation.
- Parameters
-
| [in] | aKey | A pointer to the key. |
| [in] | aKeyLength | Length of the key in bytes. |
| [in] | aTagLength | Length of tag in bytes. |
| [in] | aNonce | A pointer to the nonce. |
| [in] | aNonceLength | Length of nonce in bytes. |
| [in] | aHeader | A pointer to the header. |
| [in] | aHeaderLength | Length of header in bytes. |
| [in,out] | aPlainText | A pointer to the plaintext. |
| [in,out] | aCipherText | A pointer to the ciphertext. |
| [in] | aLength | Plaintext length in bytes. |
| [in] | aEncrypt | true on encrypt and false on decrypt. |
| [out] | aTag | A pointer to the tag. |
§ otCryptoHmacSha256()
| void otCryptoHmacSha256 |
( |
const uint8_t * |
aKey, |
|
|
uint16_t |
aKeyLength, |
|
|
const uint8_t * |
aBuf, |
|
|
uint16_t |
aBufLength, |
|
|
uint8_t * |
aHash |
|
) |
| |
This function performs HMAC computation.
- Parameters
-
| [in] | aKey | A pointer to the key. |
| [in] | aKeyLength | The key length in bytes. |
| [in] | aBuf | A pointer to the input buffer. |
| [in] | aBufLength | The length of aBuf in bytes. |
| [out] | aHash | A pointer to the output hash buffer. |