![]() |
0.01.00
|
This class is used to represent a tasklet. More...
#include <src/core/common/tasklet.hpp>
Public Types | |
| typedef void(* | Handler) (Tasklet &aTasklet) |
| This function pointer is called when the tasklet is run. More... | |
Public Member Functions | |
| Tasklet (otInstance &aInstance, Handler aHandler, void *aContext) | |
| This constructor creates a tasklet instance. More... | |
| otError | Post (void) |
| This method puts the tasklet on the run queue. | |
Public Member Functions inherited from ot::InstanceLocator | |
| otInstance & | GetInstance (void) const |
| This method returns a reference to the parent otInstance structure. More... | |
| Ip6::Ip6 & | GetIp6 (void) const |
| This method returns a reference to the Ip6. More... | |
| ThreadNetif & | GetNetif (void) const |
| This method returns a reference to the thread network interface. More... | |
Friends | |
| class | TaskletScheduler |
Additional Inherited Members | |
Protected Member Functions inherited from ot::InstanceLocator | |
| InstanceLocator (otInstance &aInstance) | |
| This constructor initializes the object. More... | |
Protected Member Functions inherited from ot::Context | |
| Context (void *aContext) | |
| This constructor initializes the context object. More... | |
This class is used to represent a tasklet.
| typedef void(* ot::Tasklet::Handler) (Tasklet &aTasklet) |
This function pointer is called when the tasklet is run.
| [in] | aTasklet | A reference to the tasklet being run. |
| ot::Tasklet::Tasklet | ( | otInstance & | aInstance, |
| Handler | aHandler, | ||
| void * | aContext | ||
| ) |
This constructor creates a tasklet instance.
| [in] | aInstance | A reference to the instance object. |
| [in] | aHandler | A pointer to a function that is called when the tasklet is run. |
| [in] | aContext | A pointer to arbitrary context information. |