0.01.00
alarm-micro.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2016, The OpenThread Authors.
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions are met:
7  * 1. Redistributions of source code must retain the above copyright
8  * notice, this list of conditions and the following disclaimer.
9  * 2. Redistributions in binary form must reproduce the above copyright
10  * notice, this list of conditions and the following disclaimer in the
11  * documentation and/or other materials provided with the distribution.
12  * 3. Neither the name of the copyright holder nor the
13  * names of its contributors may be used to endorse or promote products
14  * derived from this software without specific prior written permission.
15  *
16  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
17  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE
18  * IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE
19  * ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT HOLDER OR CONTRIBUTORS BE
20  * LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR
21  * CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF
22  * SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS
23  * INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN
24  * CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE)
25  * ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE
26  * POSSIBILITY OF SUCH DAMAGE.
27  */
28 
35 #ifndef ALARM_MICRO_H_
36 #define ALARM_MICRO_H_
37 
38 #include <stdint.h>
39 
40 #include <openthread/types.h>
41 
42 #ifdef __cplusplus
43 extern "C" {
44 #endif
45 
61 void otPlatAlarmMicroStartAt(otInstance *aInstance, uint32_t aT0, uint32_t aDt);
62 
69 void otPlatAlarmMicroStop(otInstance *aInstance);
70 
77 uint32_t otPlatAlarmMicroGetNow(void);
78 
84 extern void otPlatAlarmMicroFired(otInstance *aInstance);
85 
91 #ifdef __cplusplus
92 } // extern "C"
93 #endif
94 
95 #endif // ALARM_MICRO_H_
This type represents all the static / global variables used by OpenThread allocated in one place...
Definition: openthread-instance.h:59
This file defines the types and structures used in the OpenThread library API.
void otPlatAlarmMicroFired(otInstance *aInstance)
Signal that the alarm has fired.
uint32_t otPlatAlarmMicroGetNow(void)
Get the current time.
void otPlatAlarmMicroStop(otInstance *aInstance)
Stop the alarm.
void otPlatAlarmMicroStartAt(otInstance *aInstance, uint32_t aT0, uint32_t aDt)
Set the alarm to fire at aDt microseconds after aT0.