![]() |
0.01.00
|
This class implements handling Energy Scan Requests. More...
#include <src/core/thread/energy_scan_server.hpp>
Public Member Functions | |
| EnergyScanServer (otInstance &aInstance) | |
| This constructor initializes the object. | |
Public Member Functions inherited from ot::InstanceLocator | |
| otInstance & | GetInstance (void) const |
| This method returns a reference to the parent otInstance structure. More... | |
| Ip6::Ip6 & | GetIp6 (void) const |
| This method returns a reference to the Ip6. More... | |
| ThreadNetif & | GetNetif (void) const |
| This method returns a reference to the thread network interface. More... | |
Additional Inherited Members | |
Protected Member Functions inherited from ot::InstanceLocator | |
| InstanceLocator (otInstance &aInstance) | |
| This constructor initializes the object. More... | |
This class implements handling Energy Scan Requests.