|
|
| LinkRaw (otInstance &aInstance) |
| | This constructor initializes the object.
|
| |
|
bool | IsEnabled () |
| | This method returns true if the raw link-layer is enabled.
|
| |
|
void | SetEnabled (bool aEnabled) |
| | This method enables/disables the raw link-layer.
|
| |
|
otRadioCaps | GetCaps () |
| | This method returns the capabilities of the raw link-layer.
|
| |
|
otError | Receive (uint8_t aChannel, otLinkRawReceiveDone aCallback) |
| | This method starts a (recurring) Receive on the link-layer.
|
| |
|
void | InvokeReceiveDone (otRadioFrame *aFrame, otError aError) |
| | This method invokes the mReceiveDoneCallback, if set.
|
| |
|
otError | Transmit (otRadioFrame *aFrame, otLinkRawTransmitDone aCallback) |
| | This method starts a (single) Transmit on the link-layer.
|
| |
|
void | InvokeTransmitDone (otRadioFrame *aFrame, otRadioFrame *aAckFrame, otError aError) |
| | This method invokes the mTransmitDoneCallback, if set.
|
| |
|
otError | EnergyScan (uint8_t aScanChannel, uint16_t aScanDuration, otLinkRawEnergyScanDone aCallback) |
| | This method starts a (single) Enery Scan on the link-layer.
|
| |
|
void | InvokeEnergyScanDone (int8_t aEnergyScanMaxRssi) |
| | This method invokes the mEnergyScanDoneCallback, if set.
|
| |
The documentation for this class was generated from the following file: