0.01.00
meshcop.hpp
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2016, The OpenThread Authors.
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions are met:
7  * 1. Redistributions of source code must retain the above copyright
8  * notice, this list of conditions and the following disclaimer.
9  * 2. Redistributions in binary form must reproduce the above copyright
10  * notice, this list of conditions and the following disclaimer in the
11  * documentation and/or other materials provided with the distribution.
12  * 3. Neither the name of the copyright holder nor the
13  * names of its contributors may be used to endorse or promote products
14  * derived from this software without specific prior written permission.
15  *
16  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
17  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE
18  * IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE
19  * ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT HOLDER OR CONTRIBUTORS BE
20  * LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR
21  * CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF
22  * SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS
23  * INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN
24  * CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE)
25  * ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE
26  * POSSIBILITY OF SUCH DAMAGE.
27  */
28 
35 #ifndef MESHCOP_HPP_
36 #define MESHCOP_HPP_
37 
38 #include "openthread-core-config.h"
39 
40 #include "coap/coap.hpp"
41 #include "common/message.hpp"
42 #include "mac/mac_frame.hpp"
43 
44 namespace ot {
45 namespace MeshCoP {
46 
47 enum
48 {
49  kMeshCoPMessagePriority = Message::kPriorityHigh, // The priority for MeshCoP message
50 };
51 
56 inline Message *NewMeshCoPMessage(Coap::CoapBase &aCoap, const Coap::Header &aHeader)
57 {
58  return aCoap.NewMessage(aHeader, kMeshCoPMessagePriority);
59 }
60 
68 void ComputeJoinerId(const Mac::ExtAddress &aEui64, Mac::ExtAddress &aJoinerId);
69 
70 } // namespace MeshCoP
71 
72 } // namespace ot
73 
74 #endif // MESHCOP_HPP_
Definition: cli.cpp:90
Message * NewMeshCoPMessage(Coap::CoapBase &aCoap, const Coap::Header &aHeader)
This function create Message for MeshCoP.
Definition: meshcop.hpp:56
This file includes definitions for CoAP client and server functionality.
Message * NewMessage(const Header &aHeader, uint8_t aPriority=kDefaultCoapMessagePriority)
This method creates a new message with a CoAP header.
Definition: coap.cpp:144
This class implements CoAP header generation and parsing.
Definition: coap_header.hpp:72
void ComputeJoinerId(const Mac::ExtAddress &aEui64, Mac::ExtAddress &aJoinerId)
This function computes the Joiner ID from a factory-assigned IEEE EUI-64.
Definition: meshcop.cpp:40
This structure represents an IEEE 802.15.4 Extended Address.
Definition: mac_frame.hpp:84
This file includes definitions for generating and processing IEEE 802.15.4 MAC frames.
This class represents a message.
Definition: message.hpp:195
This class implements the common base for CoAP client and server.
Definition: coap.hpp:433
High priority level.
Definition: message.hpp:225
This file includes definitions for the message buffer pool and message buffers.
This file includes compile-time configuration constants for OpenThread.