![]() |
0.01.00
|
This module includes functions for child supervision feature. More...
Functions | |
| uint16_t | otChildSupervisionGetInterval (otInstance *aInstance) |
| Get the child supervision interval (in seconds). More... | |
| void | otChildSupervisionSetInterval (otInstance *aInstance, uint16_t aInterval) |
| Set the child supervision interval (in seconds). More... | |
| uint16_t | otChildSupervisionGetCheckTimeout (otInstance *aInstance) |
| Get the supervision check timeout interval (in seconds). More... | |
| void | otChildSupervisionSetCheckTimeout (otInstance *aInstance, uint16_t aTimeout) |
| Set the supervision check timeout interval (in seconds). More... | |
This module includes functions for child supervision feature.
The functions in this module are available when child supervision feature (OPENTHREAD_ENABLE_CHILD_SUPERVISION) is enabled.
| uint16_t otChildSupervisionGetCheckTimeout | ( | otInstance * | aInstance | ) |
Get the supervision check timeout interval (in seconds).
If the device is a sleepy child and it does not hear from its parent within the specified check timeout, it initiates the re-attach process (MLE Child Update Request/Response exchange with its parent).
| [in] | aInstance | A pointer to an OpenThread instance. |
| uint16_t otChildSupervisionGetInterval | ( | otInstance * | aInstance | ) |
Get the child supervision interval (in seconds).
Child supervision feature provides a mechanism for parent to ensure that a message is sent to each sleepy child within the supervision interval. If there is no transmission to the child within the supervision interval, OpenThread enqueues and sends a supervision message (a data message with empty payload) to the child.
| [in] | aInstance | A pointer to an OpenThread instance. |
| void otChildSupervisionSetCheckTimeout | ( | otInstance * | aInstance, |
| uint16_t | aTimeout | ||
| ) |
Set the supervision check timeout interval (in seconds).
| [in] | aInstance | A pointer to an OpenThread instance. |
| [in] | aTimeout | The check timeout (in seconds). Zero to disable supervision check on the child. |
| void otChildSupervisionSetInterval | ( | otInstance * | aInstance, |
| uint16_t | aInterval | ||
| ) |
Set the child supervision interval (in seconds).
| [in] | aInstance | A pointer to an OpenThread instance. |
| [in] | aInterval | The supervision interval (in seconds). Zero to disable supervision on parent. |