This module includes functions for signal jamming detection feature.
More...
|
| typedef void(* | otJamDetectionCallback) (bool aJamState, void *aContext) |
| | This function pointer is called if signal jam detection is enabled and a jam is detected. More...
|
| |
This module includes functions for signal jamming detection feature.
The functions in this module are available when jam-detection feature (OPENTHREAD_ENABLE_JAM_DETECTION) is enabled.
§ otJamDetectionCallback
| typedef void(* otJamDetectionCallback) (bool aJamState, void *aContext) |
This function pointer is called if signal jam detection is enabled and a jam is detected.
- Parameters
-
| [in] | aJamState | Current jam state (true if jam is detected, false otherwise). |
| [in] | aContext | A pointer to application-specific context. |
§ otJamDetectionGetBusyPeriod()
| uint8_t otJamDetectionGetBusyPeriod |
( |
otInstance * |
aInstance | ) |
|
Get the Jam Detection Busy Period (in seconds)
- Parameters
-
| [in] | aInstance | A pointer to an OpenThread instance. |
- Returns
- The Jam Detection Busy Period
§ otJamDetectionGetHistoryBitmap()
| uint64_t otJamDetectionGetHistoryBitmap |
( |
otInstance * |
aInstance | ) |
|
Get the current history bitmap.
This value provides information about current state of jamming detection module for monitoring/debugging purpose. It returns a 64-bit value where each bit corresponds to one second interval starting with bit 0 for the most recent interval and bit 63 for the oldest intervals (63 sec earlier). The bit is set to 1 if the jamming detection module observed/detected high signal level during the corresponding one second interval.
- Parameters
-
| [in] | aInstance | A pointer to an OpenThread instance. |
- Returns
- The current history bitmap.
§ otJamDetectionGetRssiThreshold()
| int8_t otJamDetectionGetRssiThreshold |
( |
otInstance * |
aInstance | ) |
|
Get the Jam Detection RSSI Threshold (in dBm).
- Parameters
-
| [in] | aInstance | A pointer to an OpenThread instance. |
- Returns
- The Jam Detection RSSI Threshold.
§ otJamDetectionGetState()
| bool otJamDetectionGetState |
( |
otInstance * |
aInstance | ) |
|
Get the Jam Detection State.
- Parameters
-
| [in] | aInstance | A pointer to an OpenThread instance. |
- Returns
- The Jam Detection state (
true jam is detected, `false' otherwise).
§ otJamDetectionGetWindow()
| uint8_t otJamDetectionGetWindow |
( |
otInstance * |
aInstance | ) |
|
Get the Jam Detection Detection Window (in seconds).
- Parameters
-
| [in] | aInstance | A pointer to an OpenThread instance. |
- Returns
- The Jam Detection Window.
§ otJamDetectionIsEnabled()
| bool otJamDetectionIsEnabled |
( |
otInstance * |
aInstance | ) |
|
Get the Jam Detection Status (enabled/disabled)
- Parameters
-
| [in] | aInstance | A pointer to an OpenThread instance. |
- Returns
- The Jam Detection status (true if enabled, false otherwise).
§ otJamDetectionSetBusyPeriod()
Set the Jam Detection Busy Period (in seconds).
The number of aggregate seconds within the detection window where the RSSI must be above threshold to trigger detection.
- Parameters
-
| [in] | aInstance | A pointer to an OpenThread instance. |
| [in] | aBusyPeriod | The Jam Detection busy period (should be non-zero and less than or equal to Jam Detection Window) |
- Return values
-
| OT_ERROR_NONE | Successfully set the window. |
| OT_ERROR_INVALID_ARGS | The given input is not within the valid range. |
§ otJamDetectionSetRssiThreshold()
| otError otJamDetectionSetRssiThreshold |
( |
otInstance * |
aInstance, |
|
|
int8_t |
aRssiThreshold |
|
) |
| |
Set the Jam Detection RSSI Threshold (in dBm).
- Parameters
-
| [in] | aInstance | A pointer to an OpenThread instance. |
| [in] | aRssiThreshold | The RSSI threshold. |
- Return values
-
| OT_ERROR_NONE | Successfully set the threshold. |
§ otJamDetectionSetWindow()
Set the Jam Detection Detection Window (in seconds).
- Parameters
-
| [in] | aInstance | A pointer to an OpenThread instance. |
| [in] | aWindow | The Jam Detection window (valid range is 1 to 63) |
- Return values
-
| OT_ERROR_NONE | Successfully set the window. |
| OT_ERROR_INVALID_ARGS | The given input parameter not within valid range (1-63) |
§ otJamDetectionStart()
Start the jamming detection.
- Parameters
-
| [in] | aInstance | A pointer to an OpenThread instance. |
| [in] | aCallback | A pointer to a function called to notify of jamming state change. |
| [in] | aContext | A pointer to application-specific context. |
- Return values
-
| OT_ERROR_NONE | Successfully started the jamming detection. |
| OT_ERROR_ALREADY | Jam detection has been started before. |
§ otJamDetectionStop()
Stop the jamming detection.
- Parameters
-
| [in] | aInstance | A pointer to an OpenThread instance. |
- Return values
-
| OT_ERROR_NONE | Successfully stopped the jamming detection. |
| OT_ERROR_ALREADY | Jam detection is already stopped. |