This module includes functions that control the Thread stack's execution.
More...
|
| typedef int(* | otCliConsoleOutputCallback) (const char *aBuf, uint16_t aBufLength, void *aContext) |
| | This function pointer is called to notify about Console output. More...
|
| |
This module includes functions that control the Thread stack's execution.
§ otCliConsoleOutputCallback
| typedef int(* otCliConsoleOutputCallback) (const char *aBuf, uint16_t aBufLength, void *aContext) |
This function pointer is called to notify about Console output.
- Parameters
-
| [in] | aBuf | A pointer to a buffer with an output. |
| [in] | aBufLength | A length of the output data stored in the buffer. |
| [out] | aContext | A user context pointer. |
- Returns
- Number of bytes processed by the callback.
§ otCliConsoleInit()
Initialize the CLI CONSOLE module.
- Parameters
-
| [in] | aInstance | The OpenThread instance structure. |
| [in] | aCallback | A callback method called to process console output. |
| [in] | aContext | A user context pointer. |
§ otCliConsoleInputLine()
| void otCliConsoleInputLine |
( |
char * |
aBuf, |
|
|
uint16_t |
aBufLength |
|
) |
| |
This method is called to feed in a console input line.
- Parameters
-
| [in] | aBuf | A pointer to a buffer with an input. |
| [in] | aBufLength | A length of the input data stored in the buffer. |
§ otCliPlatLogv()
Callback to write the OpenThread Log to the CLI console.
- Parameters
-
| [in] | aLogLevel | The log level. |
| [in] | aLogRegion | The log region. |
| [in] | aFormat | A pointer to the format string. |
| [in] | ap | va_list matching aFormat. |
§ otCliUartAppendResult()
| void otCliUartAppendResult |
( |
otError |
aError | ) |
|
Write error code the CLI console.
- Parameters
-
| [in] | aError | Error code value. |
§ otCliUartInit()
Initialize the CLI UART module.
- Parameters
-
| [in] | aInstance | The OpenThread instance structure. |
§ otCliUartOutputBytes()
| void otCliUartOutputBytes |
( |
const uint8_t * |
aBytes, |
|
|
uint8_t |
aLength |
|
) |
| |
Write a number of bytes to the CLI console as a hex string.
- Parameters
-
| [in] | aBytes | A pointer to data which should be printed. |
| [in] | aLength | aBytes length. |
§ otCliUartOutputFormat()
| void otCliUartOutputFormat |
( |
const char * |
aFmt, |
|
|
|
... |
|
) |
| |
Write formatted string the CLI console.
- Parameters
-
| [in] | aFmt | A pointer to the format string. |
| [in] | ... | A matching list of arguments. |
§ otCliUartSetUserCommands()
| void otCliUartSetUserCommands |
( |
const otCliCommand * |
aUserCommands, |
|
|
uint8_t |
aLength |
|
) |
| |
Set a user command table.
- Parameters
-
| [in] | aUserCommands | A pointer to an array with user commands. |
| [in] | aLength | aUserCommands length. |