This module includes functions for the Thread Joiner role.
More...
|
| enum | otJoinerState {
OT_JOINER_STATE_IDLE = 0,
OT_JOINER_STATE_DISCOVER = 1,
OT_JOINER_STATE_CONNECT = 2,
OT_JOINER_STATE_CONNECTED = 3,
OT_JOINER_STATE_ENTRUST = 4,
OT_JOINER_STATE_JOINED = 5
} |
| | This enumeration defines the Joiner State.
|
| |
This module includes functions for the Thread Joiner role.
§ otJoinerCallback
| typedef void(OTCALL * otJoinerCallback) (otError aError, void *aContext) |
This function pointer is called to notify the completion of a join operation.
- Parameters
-
| [in] | aError | OT_ERROR_NONE if the join process succeeded. OT_ERROR_SECURITY if the join process failed due to security credentials. OT_ERROR_NOT_FOUND if no joinable network was discovered. OT_ERROR_RESPONSE_TIMEOUT if a response timed out. |
| [in] | aContext | A pointer to application-specific context. |
§ otJoinerGetId()
Get the Joiner ID.
Joiner ID is the first 64 bits of the result of computing SHA-256 over factory-assigned IEEE EUI-64, which is used as IEEE 802.15.4 Extended Address during commissioning process.
- Parameters
-
| [in] | aInstance | A pointer to the OpenThread instance. |
| [out] | aJoinerId | A pointer to where the Joiner ID is placed. |
- Return values
-
| OT_ERROR_NONE | Successfully retrieved the Joiner ID. |
| OT_ERROR_DISABLED_FEATURE | The Joiner feature is not enabled in this build. |
§ otJoinerGetState()
This function returns the Joiner State.
- Parameters
-
| [in] | aInstance | A pointer to an OpenThread instance. |
- Return values
-
| OT_JOINER_STATE_IDLE | |
| OT_JOINER_STATE_DISCOVER | |
| OT_JOINER_STATE_CONNECT | |
| OT_JOINER_STATE_CONNECTED | |
| OT_JOINER_STATE_ENTRUST | |
| OT_JOINER_STATE_JOINED | |
§ otJoinerStart()
| OTAPI otError OTCALL otJoinerStart |
( |
otInstance * |
aInstance, |
|
|
const char * |
aPSKd, |
|
|
const char * |
aProvisioningUrl, |
|
|
const char * |
aVendorName, |
|
|
const char * |
aVendorModel, |
|
|
const char * |
aVendorSwVersion, |
|
|
const char * |
aVendorData, |
|
|
otJoinerCallback |
aCallback, |
|
|
void * |
aContext |
|
) |
| |
This function enables the Thread Joiner role.
- Parameters
-
| [in] | aInstance | A pointer to an OpenThread instance. |
| [in] | aPSKd | A pointer to the PSKd. |
| [in] | aProvisioningUrl | A pointer to the Provisioning URL (may be NULL). |
| [in] | aVendorName | A pointer to the Vendor Name (must be static). |
| [in] | aVendorModel | A pointer to the Vendor Model (must be static). |
| [in] | aVendorSwVersion | A pointer to the Vendor SW Version (must be static). |
| [in] | aVendorData | A pointer to the Vendor Data (must be static). |
| [in] | aCallback | A pointer to a function that is called when the join operation completes. |
| [in] | aContext | A pointer to application-specific context. |
- Return values
-
| OT_ERROR_NONE | Successfully started the Commissioner role. |
| OT_ERROR_INVALID_ARGS | aPSKd or aProvisioningUrl is invalid. |
| OT_ERROR_DISABLED_FEATURE | The Joiner feature is not enabled in this build. |
§ otJoinerStop()
This function disables the Thread Joiner role.
- Parameters
-
| [in] | aInstance | A pointer to an OpenThread instance. |
- Return values
-
| OT_ERROR_NONE | Successfully disabled the Joiner role. |
| OT_ERROR_DISABLED_FEATURE | The Joiner feature is not enabled in this build. |