![]() |
0.01.00
|
This file includes the platform abstraction for the Thread DHCPv6 client. More...
#include <openthread/types.h>Go to the source code of this file.
Classes | |
| struct | otDhcpAddress |
| This structure represents a DHCPv6 address. More... | |
Typedefs | |
| typedef struct otDhcpAddress | otDhcpAddress |
| This structure represents a DHCPv6 address. | |
Functions | |
| void | otDhcp6ClientUpdate (otInstance *aInstance, otDhcpAddress *aAddresses, uint32_t aNumAddresses, void *aContext) |
| Update all automatically created IPv6 addresses for prefixes from current Network Data with DHCP procedure. More... | |
This file includes the platform abstraction for the Thread DHCPv6 client.