![]() |
0.01.00
|
This file defines the structure of the variables required for all instances of OpenThread API. More...
#include "openthread-core-config.h"#include "utils/wrap_stdint.h"#include "utils/wrap_stdbool.h"#include <openthread/types.h>#include <openthread/platform/logging.h>#include "openthread-single-instance.h"#include "coap/coap.hpp"#include "crypto/heap.hpp"#include "crypto/mbedtls.hpp"#include "net/ip6.hpp"#include "thread/thread_netif.hpp"Go to the source code of this file.
Classes | |
| struct | otInstance |
| This type represents all the static / global variables used by OpenThread allocated in one place. More... | |
Typedefs | |
| typedef struct otInstance | otInstance |
| This type represents all the static / global variables used by OpenThread allocated in one place. | |
This file defines the structure of the variables required for all instances of OpenThread API.