![]() |
0.01.00
|
This module includes the platform abstraction for random number generation. More...
Functions | |
| uint32_t | otPlatRandomGet (void) |
| Get a 32-bit random value. More... | |
| otError | otPlatRandomGetTrue (uint8_t *aOutput, uint16_t aOutputLength) |
| Get true random value sequence. More... | |
This module includes the platform abstraction for random number generation.
| uint32_t otPlatRandomGet | ( | void | ) |
Get a 32-bit random value.
This function may be implemented using a pseudo-random number generator.
| otError otPlatRandomGetTrue | ( | uint8_t * | aOutput, |
| uint16_t | aOutputLength | ||
| ) |
Get true random value sequence.
This function MUST be implemented using a true random number generator (TRNG).
| [out] | aOutput | A pointer to where the true random values are placed. Must not be NULL. |
| [in] | aOutputLength | Size of aBuffer. |
| OT_ERROR_NONE | Successfully filled aBuffer with true random values. |
| OT_ERROR_FAILED | Failed to fill aBuffer with true random values. |
| OT_ERROR_INVALID_ARGS | aBuffer was set to NULL. |