![]() |
0.01.00
|
This file defines the top-level functions for the OpenThread diagnostics library. More...
#include <openthread/types.h>Go to the source code of this file.
Functions | |
| void | otDiagInit (otInstance *aInstance) |
| Initialize the diagnostics module. More... | |
| char * | otDiagProcessCmd (int argc, char *argv[]) |
| This function processes a factory diagnostics command line. More... | |
| char * | otDiagProcessCmdLine (char *aString) |
| This function processes a factory diagnostics command line. More... | |
| bool | otDiagIsEnabled (void) |
| This function indicates whether or not the factory diagnostics mode is enabled. More... | |
This file defines the top-level functions for the OpenThread diagnostics library.