0.01.00
messagepool.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2016, The OpenThread Authors.
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions are met:
7  * 1. Redistributions of source code must retain the above copyright
8  * notice, this list of conditions and the following disclaimer.
9  * 2. Redistributions in binary form must reproduce the above copyright
10  * notice, this list of conditions and the following disclaimer in the
11  * documentation and/or other materials provided with the distribution.
12  * 3. Neither the name of the copyright holder nor the
13  * names of its contributors may be used to endorse or promote products
14  * derived from this software without specific prior written permission.
15  *
16  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
17  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE
18  * IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE
19  * ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT HOLDER OR CONTRIBUTORS BE
20  * LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR
21  * CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF
22  * SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS
23  * INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN
24  * CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE)
25  * ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE
26  * POSSIBILITY OF SUCH DAMAGE.
27  */
28 
35 #ifndef MESSAGEPOOL_H_
36 #define MESSAGEPOOL_H_
37 
38 #include <stdint.h>
39 
40 #include <openthread/message.h>
41 #include <openthread/types.h>
42 
53 #ifdef __cplusplus
54 extern "C" {
55 #endif
56 
65 void otPlatMessagePoolInit(otInstance *aInstance, uint16_t aMinNumFreeBuffers, size_t aBufferSize);
66 
76 
84 void otPlatMessagePoolFree(otInstance *aInstance, otMessage *aBuffer);
85 
94 uint16_t otPlatMessagePoolNumFreeBuffers(otInstance *aInstance);
95 
96 #ifdef __cplusplus
97 } // extern "C"
98 #endif
99 
106 #endif // MESSAGEPOOL_H_
uint16_t otPlatMessagePoolNumFreeBuffers(otInstance *aInstance)
Get the number of free buffers.
This type represents all the static / global variables used by OpenThread allocated in one place...
Definition: openthread-instance.h:59
This file defines the types and structures used in the OpenThread library API.
This file defines the top-level OpenThread APIs related to message buffer and queues.
This type points to an OpenThread message buffer.
Definition: types.h:479
void otPlatMessagePoolInit(otInstance *aInstance, uint16_t aMinNumFreeBuffers, size_t aBufferSize)
Initialize the platform implemented message pool.
otMessage * otPlatMessagePoolNew(otInstance *aInstance)
Allocate a buffer from the platform managed buffer pool.
void otPlatMessagePoolFree(otInstance *aInstance, otMessage *aBuffer)
This function is used to free a Buffer back to the platform managed buffer pool.