![]() |
0.01.00
|
This file implements the OpenThread IPv6 API. More...
#include "openthread-core-config.h"#include <openthread/ip6.h>#include "openthread-instance.h"#include "common/logging.hpp"#include "utils/slaac_address.hpp"Macros | |
| #define | WPP_NAME "ip6_api.tmh" |
Functions | |
| otError | otIp6SetEnabled (otInstance *aInstance, bool aEnabled) |
| This function brings up the IPv6 interface. More... | |
| bool | otIp6IsEnabled (otInstance *aInstance) |
| This function indicates whether or not the IPv6 interface is up. More... | |
| const otNetifAddress * | otIp6GetUnicastAddresses (otInstance *aInstance) |
| Get the list of IPv6 addresses assigned to the Thread interface. More... | |
| otError | otIp6AddUnicastAddress (otInstance *aInstance, const otNetifAddress *address) |
| Add a Network Interface Address to the Thread interface. More... | |
| otError | otIp6RemoveUnicastAddress (otInstance *aInstance, const otIp6Address *address) |
| Remove a Network Interface Address from the Thread interface. More... | |
| const otNetifMulticastAddress * | otIp6GetMulticastAddresses (otInstance *aInstance) |
| Get the list of IPv6 multicast addresses subscribed to the Thread interface. More... | |
| otError | otIp6SubscribeMulticastAddress (otInstance *aInstance, const otIp6Address *aAddress) |
| Subscribe the Thread interface to a Network Interface Multicast Address. More... | |
| otError | otIp6UnsubscribeMulticastAddress (otInstance *aInstance, const otIp6Address *aAddress) |
| Unsubscribe the Thread interface to a Network Interface Multicast Address. More... | |
| bool | otIp6IsMulticastPromiscuousEnabled (otInstance *aInstance) |
| Check if multicast promiscuous mode is enabled on the Thread interface. More... | |
| void | otIp6SetMulticastPromiscuousEnabled (otInstance *aInstance, bool aEnabled) |
| Enable multicast promiscuous mode on the Thread interface. More... | |
| void | otIp6SlaacUpdate (otInstance *aInstance, otNetifAddress *aAddresses, uint32_t aNumAddresses, otIp6SlaacIidCreate aIidCreate, void *aContext) |
| Update all automatically created IPv6 addresses for prefixes from current Network Data with SLAAC procedure. More... | |
| otError | otIp6CreateRandomIid (otInstance *aInstance, otNetifAddress *aAddress, void *aContext) |
| Create random IID for given IPv6 address. More... | |
| otError | otIp6CreateMacIid (otInstance *aInstance, otNetifAddress *aAddress, void *) |
| Create IID for given IPv6 address using extended MAC address. More... | |
| otError | otIp6CreateSemanticallyOpaqueIid (otInstance *aInstance, otNetifAddress *aAddress, void *aContext) |
| Create semantically opaque IID for given IPv6 address. More... | |
| void | otIp6SetReceiveCallback (otInstance *aInstance, otIp6ReceiveCallback aCallback, void *aCallbackContext) |
| This function registers a callback to provide received IPv6 datagrams. More... | |
| bool | otIp6IsReceiveFilterEnabled (otInstance *aInstance) |
| This function indicates whether or not Thread control traffic is filtered out when delivering IPv6 datagrams via the callback specified in otIp6SetReceiveCallback(). More... | |
| void | otIp6SetReceiveFilterEnabled (otInstance *aInstance, bool aEnabled) |
| This function sets whether or not Thread control traffic is filtered out when delivering IPv6 datagrams via the callback specified in otIp6SetReceiveCallback(). More... | |
| otError | otIp6Send (otInstance *aInstance, otMessage *aMessage) |
| This function sends an IPv6 datagram via the Thread interface. More... | |
| otMessage * | otIp6NewMessage (otInstance *aInstance, bool aLinkSecurityEnabled) |
| Allocate a new message buffer for sending an IPv6 message. More... | |
| otError | otIp6AddUnsecurePort (otInstance *aInstance, uint16_t aPort) |
| This function adds a port to the allowed unsecured port list. More... | |
| otError | otIp6RemoveUnsecurePort (otInstance *aInstance, uint16_t aPort) |
| This function removes a port from the allowed unsecure port list. More... | |
| const uint16_t * | otIp6GetUnsecurePorts (otInstance *aInstance, uint8_t *aNumEntries) |
| This function returns a pointer to the unsecure port list. More... | |
| bool | otIp6IsAddressEqual (const otIp6Address *a, const otIp6Address *b) |
| Test if two IPv6 addresses are the same. More... | |
| otError | otIp6AddressFromString (const char *str, otIp6Address *address) |
| Convert a human-readable IPv6 address string into a binary representation. More... | |
| uint8_t | otIp6PrefixMatch (const otIp6Address *aFirst, const otIp6Address *aSecond) |
| This function returns the prefix match length (bits) for two IPv6 addresses. More... | |
This file implements the OpenThread IPv6 API.